PSoC™ Creator & Designer Forum Discussions
hello,every one.
I captured the Cmod voltage wave from CY3280-21x34 at the CY3280-BK1 board,just as below.
While according to 《Cypress’ CapSense Sigma-Delta Algorithm》,the wave should like this.
they are very different.
how to explain the Oscilloscope wave?
Show LessPSoC Programmer gets some information about a connected device and displays it. below the How can I programatically get this information using python? Please post some source code for this. Please see the red circle below for the info I am looking to pull programatically.
Show Less
Hi,
I am new with PSoC.
I need to put code into a default ISR for a PSoC-5LP.
I did not find the macro to reassign it properly (or the related documentation), because all the ISR used are in the GUI, and therefore an API is generated. But what about the default vector? Can I manipulate the link of the interrupt manually? Is it safe given the interactions with PSoC Creator? If so, how can I do it?
I believe it is a silly questions, but I miss whereto look for this info.
Thank you,
Show LessHI Cypress:
when we use miniprog2 in the project, i find that we can donwload the hex but can't use in the Capsense Tuner, it show below:
1、it can download the hex;
2、it can't use in capsense tuner ;
3、it can't use in program:
4、system can' t use it,
Show Less
hi cypress:
some computer we can't install the PSOC Creator, Installation process provides the necessary files to install, but the links provided do not correspond to the system version. For example, I am a 64-bit system, and lack of 32-bit system files for installation. Please help provide the following 32-bit and 64-bit system file links that must be installed.
Show LessHello,
I am writing a program for PSoC 5LP (Prototyping Kit) working with the RGB-sensor VEML6040 by Vishay.
I try to outsource most of the functions and only have the core-code remaining in the file main.c. So i created two files: veml6040.h and veml6040.c and added them to the project (in header and source files).
Extract from veml6040.h
#include "veml6040.c"
#include "main.c"
#include <project.h>
// definitions
// function headers
extract from veml6040.c
#include "veml6040.h"
uint16_t ReadSensor(uint8_t CommandCode)
{
// awesome code
}
// other functions ...
When i do so and i change the files following message appears (translated from german by me):
The file cannot be saved: (The process cannot access file "C:\Users\username\Documents\PSoC Creator\PSoC5LP-VEML6040\PSoC5LP-VEML6040.cydsn\main.c", because another process is accessing it.)
None of the files can be saved (not even main.c). Also the Build ends with the PSoC Creator crashing.
When i remove the files from the project, everything works fine again.
Can someone help me with this problem?
Best regards,
Jeroen
Show LessSorry to ask this simple question here, but I couldn't find a section for questions about PSoC Creator. I want to add schematics to a large project and cannot figure out how to do it. I have searched for many combinations of words add, insert, additional, extra schematic, etc... Nothing useful found. Your help appreciated. Thanks. --Jon
Show LessHello sir
PSoC programmer is very higher cost and no one in India are there who can repair this loader !!!
add some guideline if any problem occurs then what to do !!!
share some guideline of repairing it !!!
and try for some instant solution from your developer only !!! if someone has an issue then try to put their problem in the community and after 2-3 week some try to give some solution and which was also not working so developer feeling very bed in this way
Some things is very best microchip only that why people switch to microchip and stay in microchip b'coz they have best support team and its programmer have lower cost and reparable also so
Show LessHow does one tell which components correspond to which shapes/networks? My project will not build and I have been over this for 3 hours, there is nothing at any zoom level that I can see that is unconnected that shouldn't be. I'm beginning to think there's some kind of infinitessimal line segment that got accidently generated or something...so how do you locate it? The report is telling me the shape number and network number that failed, so how do I use that information to fix the schematic? I can't see anything in properties that correspond to these network/shape numbers.
Show Less