PSoC™ Creator & Designer Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
I'm using Creator v4.2 on a Windows 7 box.
I'm trying to figure out the function of the <project>.cyfit file. It appears in both the main project and codegentemp directories, and whenever I do a git status on my project repository, it has changed - sometimes even if nothing else has changed. It's binary, so looking at the contents or diffing with previous versions is not helpful. I know I can name it in my .gitignore file, but that means changes won't be tracked, and I'm just a tad nervous of doing so without understanding its function.
Can anyone shed any light?
Thanks,
Mike Holmes
MPE Design, Inc.
Show LessI am trying to create multiple clock dividers using the "Frequency Divider" component however I am quickly running out of UDB resources. Is there another way to divide an incoming signal in the KHz to multiple signals in Hz range without running out of space? I am using the CY8CKIT-043
Show LessJust want to report that PSoC-Creator 4.2 crashes (hangs - not responding) with lots of warning/error output.
I worked around it by starting a build and then stopping/cancelling it straight away and see the first few warnings/errors and fixing them. Then do it again, working a few errors at a time. I had many of the same types of warnings/errors so with a few fixes (having to do extra '{' and '}' for struct inits!?), it compiled again.
[2c]
Marc
Show LessThe regex applies to the fine what.
But suppose I wish to replace with more than one line?
How to use fine/replace to replace for example,
ONE
with
ONE
TWO
THREE
Show Lessi want basic projects related to rtos in psoc
PSoC Creator will open, but my project that I am working on will no longer open.
"Unhandled exception has occurred in a component in your application. Object reference not set at an instance of an object."
I have tried restarting PSoC, the PC itself, and moving the project file path directly to the desktop with no improvement.
The full error:
See the end of this message for details on invoking
just-in-time (JIT) debugging instead of this dialog box.
************** Exception Text **************
System.NullReferenceException: Object reference not set to an instance of an object.
at CyDesigner.Common.ProjMgmt.Model.CyPrjMgmtComponentMgr.AreCustomizersAllowed()
at CyDesigner.Common.ProjMgmt.Model.CyPrjMgmtProjectPSoCExe.AreCustomizersAllowed()
at CyDesigner.Common.Db.CyS3Db.CyInst.GetCustomizerProviderImpl(CyCompName compName, CyInstBindContext ctx, String schName)
at CyDesigner.Common.Db.CyS3Db.CyInst.GetCustomizerProvider(CyCompName compName, CyInstBindContext ctx, CyInstCustomizerProvider& custProvider)
at CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetIsDesignWideComponent(CyPrjMgmtProjectPSoCExe proj, CyComponentMaster master, CyCompName compName, CyElabInstBindContext context, Boolean checkLatesetIfDoesNotExist)
at CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetSelectedSupportedComponentsBySource()
at CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetSelectedSupportedComponents()
at CyDesigner.Common.ProjMgmt.DWR.CyDWRMgr.<get_DwInsts>d__a.MoveNext()
at System.Collections.Generic.List`1..ctor(IEnumerable`1 collection)
at CyDesigner.Gde.ComponentUpdateTool.CyCutDocument..ctor(CyPrjMgmtProjectPSoCExe owningPrj)
at CyDesigner.Gde.ComponentUpdateTool.CyCutInputData..ctor(CyDesignerFramework fwk, IEnumerable`1 mgrs)
at CyDesigner.Gde.Common.CyGdePlugin.UpdateCutStatusBarIcon(Boolean writeOutputMsg)
at CyDesigner.Gde.Common.CyGdePlugin.mgr_CurrentWorkspaceChanged(Object sender, EventArgs e)
at System.EventHandler.Invoke(Object sender, EventArgs e)
at CyDesigner.Common.Base.CyBasic.RaiseEvent(EventHandler eventToRaise, Object sender, EventArgs eventArgs)
at CyDesigner.Common.ProjMgmt.CyPrjMgr.OnCurrentWorkspaceChanged(EventArgs e)
at CyDesigner.Common.ProjMgmt.CyPrjMgr.set_CurrentWrkspc(CyPrjMgmtWrkspc value)
at CyDesigner.Common.ProjMgmt.CyPrjMgr.OpenWorkspace(CyPrjMgmtWrkspc workspace)
at CyDesigner.Common.ProjMgmt.CyPrjMgr.CheckandOpenWorkspace(String item)
at CyDesigner.Common.ProjMgmt.CyPrjMgr.OpenItem(String item)
at CyDesigner.Common.ProjMgmt.CyPrjMgr.RecentProjectHandler(Object sender, CyCommandClickedEventArgs e)
at CyDesigner.Common.ProjMgmt.CyPrjMgr.Execute(EventHandler`1 handler, Object sender, CyCommandClickedEventArgs e)
at CyDesigner.Framework.CyDesignerFramework.CommandClicked(Object sender, BarCommandLinkEventArgs e)
at ActiproSoftware.UIStudio.Bar.BarCommandLinkEventHandler.Invoke(Object sender, BarCommandLinkEventArgs e)
at ActiproSoftware.UIStudio.Bar.BarManager.OnCommandClick(BarCommandLinkEventArgs e)
at ActiproSoftware.UIStudio.Bar.BarManager.b(BarCommandLinkEventArgs A_0)
at ActiproSoftware.UIStudio.Bar.BarManager.a(Command A_0, Boolean A_1)
at ActiproSoftware.UIStudio.Bar.BarManager.RaiseCommand(Command command)
at CyDesigner.Common.ProjMgmt.CyPrjMgr.RaiseRecentPrjCmd(String prjCanonicalName)
at CyDesigner.StartPage.CyStartPageControl.OpenRecentProject(String prjCanonicalPath)
at CyDesigner.StartPage.CyStartPageControl.CyClickableStartPageRow`1.PerformClick()
at CyDesigner.StartPage.CyStartPageControl.m_table_MouseClickedTable(Object sender, CyTableViewMouseEventArgs e)
at CyDesigner.Common.Base.Controls.CyTableViewBase.OnMouseClickedTable(CyTableViewMouseEventArgs e)
at CyDesigner.Common.Base.Controls.CyTableViewBase.OnMouseClick(MouseEventArgs e)
at CyDesigner.Common.Base.Controls.CyTableViewBase.control_MouseClick(Object sender, MouseEventArgs e)
at System.Windows.Forms.Control.OnMouseClick(MouseEventArgs e)
at System.Windows.Forms.Control.WmMouseUp(Message& m, MouseButtons button, Int32 clicks)
at System.Windows.Forms.Control.WndProc(Message& m)
at System.Windows.Forms.ScrollableControl.WndProc(Message& m)
at System.Windows.Forms.ContainerControl.WndProc(Message& m)
at System.Windows.Forms.UserControl.WndProc(Message& m)
at System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m)
at System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m)
at System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)
************** Loaded Assemblies **************
mscorlib
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3416.0 built by: NET472REL1LAST_B
CodeBase: file:///C:/Windows/Microsoft.NET/Framework/v4.0.30319/mscorlib.dll
----------------------------------------
psoc_creator
Assembly Version: 4.2.0.641
Win32 Version:
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/psoc_creator.exe
----------------------------------------
cycmbase
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cycmbase.DLL
----------------------------------------
System.Windows.Forms
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3324.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms/v4.0_4.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
----------------------------------------
System
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3416.0 built by: NET472REL1LAST_B
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
cydevicedb
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cydevicedb.DLL
----------------------------------------
System.Drawing
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Drawing/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
----------------------------------------
CyFramework
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/CyFramework.DLL
----------------------------------------
cys3db
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cys3db.DLL
----------------------------------------
CyPrjMgmt
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/CyPrjMgmt.DLL
----------------------------------------
cygde
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cygde.DLL
----------------------------------------
cygdegfxlib
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cygdegfxlib.DLL
----------------------------------------
cydebugger
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cydebugger.DLL
----------------------------------------
cyautomation
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyautomation.DLL
----------------------------------------
System.Core
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3429.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Core/v4.0_4.0.0.0__b77a5c561934e089/System.Core.dll
----------------------------------------
System.Configuration
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3324.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Configuration/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll
----------------------------------------
System.Xml
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
Accessibility
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/Accessibility/v4.0_4.0.0.0__b03f5f7f11d50a3a/Accessibility.dll
----------------------------------------
UIFramework.Product6.WinForms
Assembly Version: 16.1.330.0
Win32 Version: 16.1.330.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/UIFramework.Product6.WinForms.DLL
----------------------------------------
UIFramework.Product2.WinForms
Assembly Version: 16.1.330.0
Win32 Version: 16.1.330.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/UIFramework.Product2.WinForms.DLL
----------------------------------------
UIFramework.Product5.WinForms
Assembly Version: 16.1.330.0
Win32 Version: 16.1.330.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/UIFramework.Product5.WinForms.DLL
----------------------------------------
UIFramework.Product4.WinForms
Assembly Version: 16.1.330.0
Win32 Version: 16.1.330.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/UIFramework.Product4.WinForms.DLL
----------------------------------------
CyShared
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/CyShared.DLL
----------------------------------------
System.Management
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Management/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Management.dll
----------------------------------------
System.Web.Services
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Web.Services/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Web.Services.dll
----------------------------------------
pte21etb
Assembly Version: 4.2.0.641
Win32 Version: 4.7.3416.0 built by: NET472REL1LAST_B
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
cydsextensions
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cydsextensions.DLL
----------------------------------------
cygnuarmshipped
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/import/gnu/arm/cygnuarmshipped.dll
----------------------------------------
cykeilpk51
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/import/keil/pk51/cykeilpk51.dll
----------------------------------------
cyeditors
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyeditors.DLL
----------------------------------------
UIFramework.Product6.Addons.DotNet.WinForms
Assembly Version: 16.1.330.0
Win32 Version: 16.1.330.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/UIFramework.Product6.Addons.DotNet.WinForms.DLL
----------------------------------------
cytransport
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cytransport.DLL
----------------------------------------
cypsocdebugger
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cypsocdebugger.EXE
----------------------------------------
cygdbdebugger
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cygdbdebugger.DLL
----------------------------------------
cyarmdebugger
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyarmdebugger.DLL
----------------------------------------
cyppdeviceio
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyppdeviceio.DLL
----------------------------------------
cywin32deviceio
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cywin32deviceio.DLL
----------------------------------------
bootloader_host
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/bootloader_host.EXE
----------------------------------------
cydsfit
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cydsfit.EXE
----------------------------------------
cyfitter_fm
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyfitter_fm.EXE
----------------------------------------
cyfitlib
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyfitlib.DLL
----------------------------------------
Microsoft.GeneratedCode
Assembly Version: 1.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
ICSharpCode.SharpZipLib
Assembly Version: 0.85.4.369
Win32 Version: 0.85.4.369
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/ICSharpCode.SharpZipLib.DLL
----------------------------------------
System.Drawing.Design
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Drawing.Design/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.Design.dll
----------------------------------------
System.Design
Assembly Version: 4.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Design/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Design.dll
----------------------------------------
UIFramework.Product1.WinForms
Assembly Version: 16.1.330.0
Win32 Version: 16.1.330.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/UIFramework.Product1.WinForms.DLL
----------------------------------------
Microsoft.GeneratedCode
Assembly Version: 1.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
MigraDoc.DocumentObjectModel
Assembly Version: 1.32.3885.0
Win32 Version: 1.32.3885.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/MigraDoc.DocumentObjectModel.DLL
----------------------------------------
cyhextool
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyhextool.EXE
----------------------------------------
cykeilspawner
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cykeilspawner.EXE
----------------------------------------
cytunerextensions
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cytunerextensions.DLL
----------------------------------------
cyclangwrapper
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyclangwrapper.DLL
----------------------------------------
PP_Accessor
Assembly Version: 3.24.1.2235
Win32 Version: 3.24.1.2235
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/PP_Accessor.DLL
----------------------------------------
Microsoft.GeneratedCode
Assembly Version: 1.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
Microsoft.GeneratedCode
Assembly Version: 1.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
Microsoft.GeneratedCode
Assembly Version: 1.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
cyp3fit
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cyp3fit.EXE
----------------------------------------
PP_COM_Wrapper
Assembly Version: 3.27.1.3121
Win32 Version: 3.27.1.3121
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/PP_COM_Wrapper.dll
----------------------------------------
PP_PC_Wrapper
Assembly Version: 3.27.1.3121
Win32 Version: 3.27.1.3121
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/PP_PC_Wrapper.dll
----------------------------------------
ProgrammerLibrary
Assembly Version: 3.27.1.3121
Win32 Version: 3.27.1.3121
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/ProgrammerLibrary.DLL
----------------------------------------
Microsoft.GeneratedCode
Assembly Version: 1.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
AxInterop.SHDocVw
Assembly Version: 1.1.0.0
Win32 Version: 1.1.0.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/AxInterop.SHDocVw.DLL
----------------------------------------
Interop.SHDocVw
Assembly Version: 1.1.0.0
Win32 Version: 1.1.0.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/Interop.SHDocVw.DLL
----------------------------------------
CyComponentLibrary_4a4e926d14044765f0cb43e775349e4581cf8ff1479d6b13ed741b126286ee76
Assembly Version: 0.0.0.0
Win32 Version: 0.0.0.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/psoc/content/cycomponentlibrary/CyComponentLibrary.cylib/CyComponentLibrary.dll
----------------------------------------
cydstoolkit
Assembly Version: 4.2.0.641
Win32 Version: 4.2.0.641
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/bin/cydstoolkit.DLL
----------------------------------------
cyprimitives_ff604bb3e44673643345856367282b88e9cc15b8fdd103f545ecff7c0201f386
Assembly Version: 0.0.0.0
Win32 Version: 0.0.0.0
CodeBase: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.2/PSoC%20Creator/psoc/content/cyprimitives/CyPrimitives.cylib/CyPrimitives.dll
----------------------------------------
Microsoft.GeneratedCode
Assembly Version: 1.0.0.0
Win32 Version: 4.7.3190.0 built by: NET472REL1LAST_C
CodeBase: file:///C:/windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
************** JIT Debugging **************
To enable just-in-time (JIT) debugging, the .config file for this
application or computer (machine.config) must have the
jitDebugging value set in the system.windows.forms section.
The application must also be compiled with debugging
enabled.
For example:
<configuration>
<system.windows.forms jitDebugging="true" />
</configuration>
When JIT debugging is enabled, any unhandled exception
will be sent to the JIT debugger registered on the computer
rather than be handled by this dialog box.
Show LessWhen configuring an item on the PSoC schematic in PSoC Creator, many of the parameters used to configure the item have a "f(x)" button off to the right that seems to be there to allow you to define the value based on other parameters.
Clicking on it brings up a box that allows one to enter an expression, and on the right side there is tree full of sources from which one could pull various constants and operators. For example, I can look at the device information and use that somehow.
However, what I'd really like to do is set a constant parameter somewhere (i.e. perhaps in project settings somewhere) and use that to configure many components. For example, I often end up changing the "Width" parameter on digital components based on whether I want to work with 8 bit, 12 bit, 16 bit values or whatever. I end up having to hunt around my entire schematic and find every digital component and constant and set them all to the same constant value. It seems like I should be somehow able to use this "expression" functionality to set that value in one place and have my design updated.
Is such a thing possible? I've tried to find documentation on how to use these expressions, but I was only able to find this: https://www.cypress.com/file/37371/download
That document only described basic expression syntax, and is written for PSoC Express, not PSoC Creator.
Show LessHello.
When the user name was used by other language.
it occurred follow error.
====================================
arm-none-eabi-gcc.exe: error:
C:\Users\??\Documents\PSoC Creator\4.2\Downloads (
4.2).cylib\BLE_v3_61\Library\gccCyBLEStack_BLE_SOC_PERIPHERAL.a: Invalid
argumentThe command 'arm-none-eabi-gcc.exe' failed with exit code '1'.
===============================
?? is korean name.
Do you know about this problem?
Thanks and Best regards.
Glenn.
Show LessHi,
May I know the syntax or get the cypress documentation for receiving using UART cable. I am using UART for transmitting and receiving the character. I have tried using this syntax Cy_SCB_UART_GetArray(UART_HW,SerialBuffer,1); but failed to receive the data. Am able to read the output of the task but not able to write it to the PSOC6. Trying to send data from PC to PSOC6 using UART cable. May I get a suggestion as which syntax to be used to receive the data in PSOC which is sent by the PC.
Thank you in advance,
Warm regards,
Vivekraj MD
Hello
I am unable to solve this error.I am trying to use interrupts in PSoC 6 project on Main controller for robot through following video instructions from https://www.cypress.com/training/psoc-6-101-chapter-2-introduction-psoc-6-mcu-peripherals .
Kindly help me on this issue
thankyou
Show Less