PSoC™ Creator & Designer Forum Discussions
I'm trying to set the period of the Timer/Counter. Supposedly it has: Range: 0-65535 (for 16 bit resolution) or 0–4294967295 (for 32 bit resolution). But it objects to 4294967295 for 32 bit resolution:
It will, however, accept half that:
Am I doing something wrong?
Show Less(I looked for a thread for this problem - I did not see one.)
I am using a CY8CKIT-062-WiFi-BT PSoC 6 WiFi-BT PioneerKit.
I used the default CE220923_VDAC_Sawtooth demo and it worked fine, despite some "incompatible" errors.
PSoC Creator 4.3 (upgraded from 4.2)
PDLSetup3.0.9 (I think)
I then changed the pin from the original pin9_6 to pin9_0.
I got a message that both pins were used. I got the same output on both pins.
I then rebuilt again, and got the error messages below, and the build failed.
I then replaced the DAC with the same (default?) settings. Recompiled. Same fail.
Then downloaded and ran PDLSetup3.1.2.exe
Recompiled. Same fail.
The "Component Update" keeps saying everything is at the latest rev.
I am compiling with the CM4 core on the PSoC 6.
At this point I am stuck.
Thanks .... bandit
Show Less
Hi,
has anyone succesfully used C++ on PSoC? I want to use a C++ source code. On the first run I want to know if it will fit into a 5LP. I switched to the latest ARM GCC release (9-2020-q2). I replaced the GCC exe file with the G++ exe file.
There was an issue in CyLib.c with the initialization of the SysTick Callbacks regarding the void* 0 pointer. Replacing it with "nullptr" resolved the issue. Now, it seems(!) that it can be linked. As expected, it won't fit into the device on the first run, the error message is:
Build error: <...>/xyz.elf section `.ARM.exidx' will not fit in region `rom'
The bad thing is that the .elf file is deleted directly after the build process - it can be seen shortly in file explorer. Trying to copy it while it exists results in a empty file, unfortunately. I assume the created file is filled with valuable content for checking how much the flash content is in size. Too bad that the output window doesn't show the size in this configuration.
There's also an error "cm3gcc.ld:91: undefined symbol `RomVectors' referenced in expression". I don't know if this is related to the error mentioned above.
So, I've two questions:
1) how to get the information regarding the build size / prevent that the .elf file is deleted
2) how to check what's going on with those RomVectors?
Regards
Show LessHello,
Is there a way to to determine the run time of a function?
Normally I'll toggle a pin at the beginning and end of a function and measure with a scope.
That's obviously not a perfect solution as it includes the time to toggle the pin.
I figured there was a way to do this via Creator or during a debug run.
Thanks
Show LessCould someone please help me out. I cannot get this to synthesize... I just cant. Ive been working and reading for a week...
I was so proud to have a design... Just seems it would be so easy to just pick a GPIO and some UART pins... Uh not for me...
William
Show LessI have an old CY8CKIT-050 kit that I can program with the PSoC Creator 1.0, but when I use 4.2 or 4.3 I get this error:
This device was recognized, but PSoC Creator does not support using it at this time.
Show Less
I'm getting this when I try to step through some of my code:
I have extracted a small sample that reproduces the problem from my application. I tried to simplify it further, but then sometimes it doesn't crash.
I get the crash right about here on line 9:
void my_test() {
RunningStat stats;
RS_init(&stats);
float sum = 0;
for (size_t i = 0; i < N_VIBRATIONS; ++i) {
float v = pT2->vibration;
// Scale and translate:
v -= 0x8000;
v /= 0x8000;
Here is the Output:
--------------- Build Started: 06/16/2020 08:33:40 Project: Turb_Mon, Configuration: ARM GCC 5.4-2016-q2-update Debug ---------------
The code generation step is up to date.
The compile step is up to date, no work needs to be done.
The link step is up to date, no work needs to be done.
arm-none-eabi-gcc.exe -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -mthumb -I..\Lab-Project-FreeRTOS-FAT\include -I..\Lab-Project-FreeRTOS-FAT\portable\common -I.\portable\MCU_PSOC6_M4 -I.\Generated_Source\PSoC6\pdl\middleware\ble -I. -IGenerated_Source\PSoC6 -IGenerated_Source\PSoC6\pdl\cmsis/include/ -IGenerated_Source\PSoC6\pdl\devices/psoc6/include/ -IGenerated_Source\PSoC6\pdl\devices/psoc6/include/ip/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/device/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/dma/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/efuse/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/flash/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/gpio/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/ipc/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/lvd/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/profile/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/prot/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/rtc/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/sar/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/scb/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/sysanalog/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/sysclk/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/sysint/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/syslib/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/syspm/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/systick/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/tcpwm/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/trigmux/ -IGenerated_Source\PSoC6\pdl\drivers/peripheral/wdt/ -IGenerated_Source\PSoC6\pdl\middleware/ -IGenerated_Source\PSoC6\pdl\middleware/emWin/code/drivers/Control/ -IGenerated_Source\PSoC6\pdl\middleware/emWin/code/include/ -IGenerated_Source\PSoC6\pdl\middleware/emWin/code/include/osnts_softfp/ -IGenerated_Source\PSoC6\pdl\rtos/FreeRTOS/10.0.1/Source/include/ -IGenerated_Source\PSoC6\pdl\rtos/FreeRTOS/10.0.1/Source/portable/GCC/CM4F/ -IGenerated_Source\PSoC6\pdl\utilities/ -Wa,-alh=.\CortexM4\ARM_GCC_541\Debug/my_test.lst -g -D DEBUG -D CY_CORE_ID=0 -D CY_PSOC_CREATOR_USED=1 -D CY8C6347BZI_BLD53 -Wall -ffunction-sections -ffat-lto-objects -Og -c my_test.c -o .\CortexM4\ARM_GCC_541\Debug\my_test.o
arm-none-eabi-gcc.exe -Wl,--start-group -o "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon_link.elf" Generated_Source\PSoC6\pdl\middleware\ble\lib\cy_ble_stack_gcc_host_ipc_cm4.a Generated_Source\PSoC6\pdl\middleware\emWin\libs\GCC\libemWin_osnts_gcc.a .\CortexM4\ARM_GCC_541\Debug\startup_psoc6_01_cm4.o .\CortexM4\ARM_GCC_541\Debug\crc.o .\CortexM4\ARM_GCC_541\Debug\spi.o .\CortexM4\ARM_GCC_541\Debug\hw_config.o .\CortexM4\ARM_GCC_541\Debug\sd_spi.o .\CortexM4\ARM_GCC_541\Debug\sd_card.o .\CortexM4\ARM_GCC_541\Debug\ff_sddisk.o .\CortexM4\ARM_GCC_541\Debug\ff_crc.o .\CortexM4\ARM_GCC_541\Debug\ff_dir.o .\CortexM4\ARM_GCC_541\Debug\ff_error.o .\CortexM4\ARM_GCC_541\Debug\ff_fat.o .\CortexM4\ARM_GCC_541\Debug\ff_file.o .\CortexM4\ARM_GCC_541\Debug\ff_format.o .\CortexM4\ARM_GCC_541\Debug\ff_ioman.o .\CortexM4\ARM_GCC_541\Debug\ff_locking.o .\CortexM4\ARM_GCC_541\Debug\ff_memory.o .\CortexM4\ARM_GCC_541\Debug\ff_stdio.o .\CortexM4\ARM_GCC_541\Debug\ff_string.o .\CortexM4\ARM_GCC_541\Debug\ff_sys.o .\CortexM4\ARM_GCC_541\Debug\ff_time.o .\CortexM4\ARM_GCC_541\Debug\FreeRTOS_CLI.o .\CortexM4\ARM_GCC_541\Debug\CLI-commands.o .\CortexM4\ARM_GCC_541\Debug\CreateAndVerifyExampleFiles.o .\CortexM4\ARM_GCC_541\Debug\demo_logging.o .\CortexM4\ARM_GCC_541\Debug\ff_stdio_tests_with_cwd.o .\CortexM4\ARM_GCC_541\Debug\app4-IO_module_function_checker.o .\CortexM4\ARM_GCC_541\Debug\big_file_test.o .\CortexM4\ARM_GCC_541\Debug\File-related-CLI-commands.o .\CortexM4\ARM_GCC_541\Debug\filesystem_test_suite.o .\CortexM4\ARM_GCC_541\Debug\ff_utils.o .\CortexM4\ARM_GCC_541\Debug\GLCD_Driver.o .\CortexM4\ARM_GCC_541\Debug\GUIConf.o .\CortexM4\ARM_GCC_541\Debug\GUI_X_RTOS.o .\CortexM4\ARM_GCC_541\Debug\LCDConf.o .\CortexM4\ARM_GCC_541\Debug\TM_LCD.o .\CortexM4\ARM_GCC_541\Debug\ui_fsm.o .\CortexM4\ARM_GCC_541\Debug\keypad.o .\CortexM4\ARM_GCC_541\Debug\ble_task.o .\CortexM4\ARM_GCC_541\Debug\status_led_task.o .\CortexM4\ARM_GCC_541\Debug\system_psoc6_cm4.o .\CortexM4\ARM_GCC_541\Debug\main_cm4.o .\CortexM4\ARM_GCC_541\Debug\data_logging.o .\CortexM4\ARM_GCC_541\Debug\rtc.o .\CortexM4\ARM_GCC_541\Debug\running_stat.o .\CortexM4\ARM_GCC_541\Debug\data_buffers.o .\CortexM4\ARM_GCC_541\Debug\normal.o .\CortexM4\ARM_GCC_541\Debug\data_collecting.o .\CortexM4\ARM_GCC_541\Debug\my_test.o .\CortexM4\ARM_GCC_541\Debug\uart_cli.o .\CortexM4\ARM_GCC_541\Debug\stdio_user.o .\CortexM4\ARM_GCC_541\Debug\config.o .\CortexM4\ARM_GCC_541\Debug\simuvib.o .\CortexM4\ARM_GCC_541\Debug\Hourglass_1bpp01.o .\CortexM4\ARM_GCC_541\Debug\cyfitter_sysint_cfg.o .\CortexM4\ARM_GCC_541\Debug\cymetadata.o .\CortexM4\ARM_GCC_541\Debug\UART_1.o .\CortexM4\ARM_GCC_541\Debug\GLCD.o .\CortexM4\ARM_GCC_541\Debug\GLCD_PM.o .\CortexM4\ARM_GCC_541\Debug\UserSDCrd_SPI.o .\CortexM4\ARM_GCC_541\Debug\SysSDCrd1_SPI.o .\CortexM4\ARM_GCC_541\Debug\SysSDCrd0_SPI.o .\CortexM4\ARM_GCC_541\Debug\Sys_I2C.o .\CortexM4\ARM_GCC_541\Debug\IO_SPI.o .\CortexM4\ARM_GCC_541\Debug\ADC_1.o .\CortexM4\ARM_GCC_541\Debug\ADC_1_INT.o .\CortexM4\ARM_GCC_541\Debug\ADC_1_INIT.o .\CortexM4\ARM_GCC_541\Debug\ADC_1_PM.o .\CortexM4\ARM_GCC_541\Debug\BLE.o .\CortexM4\ARM_GCC_541\Debug\BLE_config.o .\CortexM4\ARM_GCC_541\Debug\BLE_dis_config.o .\CortexM4\ARM_GCC_541\Debug\BLE_custom_config.o .\CortexM4\ARM_GCC_541\Debug\RTC_1.o .\CortexM4\ARM_GCC_541\Debug\UserSDCrd_rxDma.o .\CortexM4\ARM_GCC_541\Debug\UserSDCrd_txDma.o .\CortexM4\ARM_GCC_541\Debug\SysSDCrd0_rxDma.o .\CortexM4\ARM_GCC_541\Debug\SysSDCrd0_txDma.o .\CortexM4\ARM_GCC_541\Debug\SysSDCrd1_rxDma.o .\CortexM4\ARM_GCC_541\Debug\SysSDCrd1_txDma.o .\CortexM4\ARM_GCC_541\Debug\cy_dma.o .\CortexM4\ARM_GCC_541\Debug\cy_efuse.o .\CortexM4\ARM_GCC_541\Debug\cy_flash.o .\CortexM4\ARM_GCC_541\Debug\cy_gpio.o .\CortexM4\ARM_GCC_541\Debug\cy_ipc_drv.o .\CortexM4\ARM_GCC_541\Debug\cy_ipc_sema.o .\CortexM4\ARM_GCC_541\Debug\cy_ipc_pipe.o .\CortexM4\ARM_GCC_541\Debug\cy_lvd.o .\CortexM4\ARM_GCC_541\Debug\cy_profile.o .\CortexM4\ARM_GCC_541\Debug\cy_prot.o .\CortexM4\ARM_GCC_541\Debug\cy_rtc.o .\CortexM4\ARM_GCC_541\Debug\cy_sar.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_common.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_i2c.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_ezi2c.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_spi.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_uart.o .\CortexM4\ARM_GCC_541\Debug\cy_sysanalog.o .\CortexM4\ARM_GCC_541\Debug\cy_sysclk.o .\CortexM4\ARM_GCC_541\Debug\cy_sysint.o .\CortexM4\ARM_GCC_541\Debug\cy_syslib.o .\CortexM4\ARM_GCC_541\Debug\cy_syslib_gcc.o .\CortexM4\ARM_GCC_541\Debug\cy_syspm.o .\CortexM4\ARM_GCC_541\Debug\cy_systick.o .\CortexM4\ARM_GCC_541\Debug\cy_trigmux.o .\CortexM4\ARM_GCC_541\Debug\cy_wdt.o .\CortexM4\ARM_GCC_541\Debug\cy_device.o .\CortexM4\ARM_GCC_541\Debug\cy_tcpwm_counter.o .\CortexM4\ARM_GCC_541\Debug\cy_tcpwm_pwm.o .\CortexM4\ARM_GCC_541\Debug\cy_tcpwm_quaddec.o .\CortexM4\ARM_GCC_541\Debug\cy_ble.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hal_int.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hal_pvt.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_gap.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_gatt.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_event_handler.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ancs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ans.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_aios.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bas.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bcs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bls.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bms.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bts.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_cgms.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_cps.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_cscs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_cts.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_custom.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_dis.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ess.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_gls.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hids.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hps.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hrs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hts.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ias.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ips.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_lls.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_lns.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ndcs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_plxs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_pass.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_rscs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_rtus.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_scps.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_tps.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_uds.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_wpts.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_wss.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_clk.o .\CortexM4\ARM_GCC_541\Debug\GUIDRV_Control.o .\CortexM4\ARM_GCC_541\Debug\croutine.o .\CortexM4\ARM_GCC_541\Debug\event_groups.o .\CortexM4\ARM_GCC_541\Debug\list.o .\CortexM4\ARM_GCC_541\Debug\queue.o .\CortexM4\ARM_GCC_541\Debug\tasks.o .\CortexM4\ARM_GCC_541\Debug\timers.o .\CortexM4\ARM_GCC_541\Debug\stream_buffer.o .\CortexM4\ARM_GCC_541\Debug\port.o .\CortexM4\ARM_GCC_541\Debug\heap_4.o .\CortexM4\ARM_GCC_541\Debug\retarget.o .\CortexM4\ARM_GCC_541\Debug\Counter_1.o -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -mthumb -L Generated_Source\PSoC6 -Wl,-Map,.\CortexM4\ARM_GCC_541\Debug/Turb_Mon.map -T cy8c6xx7_cm4_dual.ld -Wl,--gc-sections -g -ffunction-sections -Og -ffat-lto-objects -Wl,--end-group
"C:\Program Files (x86)\Cypress\PDL\3.1.2\tools\win\elf\cymcuelftool.exe" --sign "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon_link.elf" --output "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon_signed.elf" --hex "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon_signed.hex"
No ELF section .cychecksum found, creating one
Application checksum calculated and stored in ELF section .cychecksum
Checksum calculated and stored in ELF section .cymeta
"C:\Program Files (x86)\Cypress\PDL\3.1.2\tools\win\elf\cymcuelftool.exe" --merge "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon_signed.elf" "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM0p\ARM_GCC_541\Debug\Turb_Mon.elf" --output "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon.elf" --hex "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon.hex"
Application checksum calculated and stored in ELF section .cychecksum
Checksum calculated and stored in ELF section .cymeta
"C:\Program Files (x86)\Cypress\PDL\3.1.2\tools\win\elf\cymcuelftool.exe" -A "C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon.elf"
code:607436 sram:137040
--------------- Build Succeeded: 06/16/2020 08:33:45 ---------------
Programming device 'PSoC 63 CY8C6347BZI-BLD53 (CM4)' with file 'C:\Users\carlk\Documents\PSoC Creator\Turbmon.cydsn\Turb_Mon.cydsn\CortexM4\ARM_GCC_541\Debug\Turb_Mon.hex'.
Device ID Check
Erasing of Main Flash...
Erasing of WFlash...
Programming of Flash Starting...
Protecting...
Verify Checksum...
Finished Programming
Device 'PSoC 63 CY8C6347BZI-BLD53 (CM4)' was successfully programmed at 06/16/2020 08:34:11.
Continuing target program
The target program has stopped at: file: main_cm4.c line: 181 function: main address: 0x1008FADC
Continuing target program
The target program has stopped at: file: my_test.c line: 66 function: my_test address: 0x1009302C
Continuing target program
The target program has stopped at: file: my_test.c line: 68 function: my_test address: 0x10093030
Continuing target program
The target program has stopped at: file: my_test.c line: 70 function: my_test address: 0x10093036
Continuing target program
The target program has stopped at: file: my_test.c line: 71 function: my_test address: 0x1009303A
Continuing target program
The target program has stopped at: file: my_test.c line: 73 function: my_test address: 0x10093048
Continuing target program
The target program has stopped at: file: my_test.c line: 75 function: my_test address: 0x10093050
~"/home/build/work/GCC-5-0-build/src/gdb/gdb/regcache.c:176: internal-error: register_size: Assertion `regnum >= 0 && regnum < (gdbarch_num_regs (gdbarch) + gdbarch_num_pseudo_regs (gdbarch))' failed.\nA problem internal to GDB has been detected,\nfurther debugging may prove unreliable.\nQuit this debugging session? "
~"/home/build/work/GCC-5-0-build/src/gdb/gdb/regcache.c:176: internal-error: register_size: Assertion `regnum >= 0 && regnum < (gdbarch_num_regs (gdbarch) + gdbarch_num_pseudo_regs (gdbarch))' failed.\nA problem internal to GDB has been detected,\nfurther debugging may prove unreliable.\nCreate a core file of GDB? "
Error: dbg.M0015: Debugger exited unexpectedly during run. Encountered error (GDB encountered an error and had to close. See output window for more information. See output window for more information.)
CANCEL
Error: dbg.M0015: Debugger exited unexpectedly during run. Encountered error (GDB encountered an error and had to close. See output window for more information. See output window for more information.)
CANCEL
Show LessHi All
PSoC 4.3 is unable to open any existing project or to create a new one.
I uninstalled all the old PSoC version, I purge all I found about Cypress, I installed (and reinstalled) several time 4.3 version, but no way: it does not work.
The log file I get when I try to open an existing project is here reported.
Should I come back to 4.2 version or is there something I can try to do for make it working?
Thanks for your help.
Best Regards
Vittorio
Le informazioni su come richiamare il debug JIT (Just-In-Time) anziché questa finestra
sono riportate in fondo al messaggio.
************** Testo dell'eccezione **************
System.NullReferenceException: Riferimento a un oggetto non impostato su un'istanza di oggetto.
in CyDesigner.Common.ProjMgmt.Model.CyPrjMgmtComponentMgr.AreCustomizersAllowed()
in CyDesigner.Common.ProjMgmt.Model.CyPrjMgmtProjectPSoCExe.AreCustomizersAllowed()
in CyDesigner.Common.Db.CyS3Db.CyInst.GetCustomizerProviderImpl(CyCompName compName, CyInstBindContext ctx, String schName)
in CyDesigner.Common.Db.CyS3Db.CyInst.GetCustomizerProvider(CyCompName compName, CyInstBindContext ctx, CyInstCustomizerProvider& custProvider)
in CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetIsDesignWideComponent(CyPrjMgmtProjectPSoCExe proj, CyComponentMaster master, CyCompName compName, CyElabInstBindContext context, Boolean checkLatesetIfDoesNotExist)
in CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetSelectedSupportedComponentsBySource()
in CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetSelectedSupportedComponents()
in CyDesigner.Common.ProjMgmt.DWR.CyDWRMgr.<get_DwInsts>d__a.MoveNext()
in System.Collections.Generic.List`1..ctor(IEnumerable`1 collection)
in CyDesigner.Gde.ComponentUpdateTool.CyCutDocument..ctor(CyPrjMgmtProjectPSoCExe owningPrj)
in CyDesigner.Gde.ComponentUpdateTool.CyCutInputData..ctor(CyDesignerFramework fwk, IEnumerable`1 mgrs)
in CyDesigner.Gde.Common.CyGdePlugin.UpdateCutStatusBarIcon(Boolean writeOutputMsg)
in CyDesigner.Gde.Common.CyGdePlugin.mgr_CurrentWorkspaceChanged(Object sender, EventArgs e)
in System.EventHandler.Invoke(Object sender, EventArgs e)
in CyDesigner.Common.Base.CyBasic.RaiseEvent(EventHandler eventToRaise, Object sender, EventArgs eventArgs)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.OnCurrentWorkspaceChanged(EventArgs e)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.set_CurrentWrkspc(CyPrjMgmtWrkspc value)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.OpenWorkspace(CyPrjMgmtWrkspc workspace)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.CheckandOpenWorkspace(String item)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.OpenItem(String item)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.RecentProjectHandler(Object sender, CyCommandClickedEventArgs e)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.Execute(EventHandler`1 handler, Object sender, CyCommandClickedEventArgs e)
in CyDesigner.Framework.CyDesignerFramework.CommandClicked(Object sender, BarCommandLinkEventArgs e)
in ActiproSoftware.UIStudio.Bar.BarCommandLinkEventHandler.Invoke(Object sender, BarCommandLinkEventArgs e)
in ActiproSoftware.UIStudio.Bar.BarManager.OnCommandClick(BarCommandLinkEventArgs e)
in ActiproSoftware.UIStudio.Bar.BarManager.b(BarCommandLinkEventArgs A_0)
in ActiproSoftware.UIStudio.Bar.BarManager.a(Command A_0, Boolean A_1)
in ActiproSoftware.UIStudio.Bar.BarManager.RaiseCommand(Command command)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.RaiseRecentPrjCmd(String prjCanonicalName)
in CyDesigner.StartPage.CyStartPageControl.OpenRecentProject(String prjCanonicalPath)
in CyDesigner.StartPage.CyStartPageControl.CyClickableStartPageRow`1.PerformClick()
in CyDesigner.StartPage.CyStartPageControl.m_table_MouseClickedTable(Object sender, CyTableViewMouseEventArgs e)
in CyDesigner.Common.Base.Controls.CyTableViewBase.OnMouseClickedTable(CyTableViewMouseEventArgs e)
in CyDesigner.Common.Base.Controls.CyTableViewBase.OnMouseClick(MouseEventArgs e)
in CyDesigner.Common.Base.Controls.CyTableViewBase.control_MouseClick(Object sender, MouseEventArgs e)
in System.Windows.Forms.Control.OnMouseClick(MouseEventArgs e)
in System.Windows.Forms.Control.WmMouseUp(Message& m, MouseButtons button, Int32 clicks)
in System.Windows.Forms.Control.WndProc(Message& m)
in System.Windows.Forms.ScrollableControl.WndProc(Message& m)
in System.Windows.Forms.ContainerControl.WndProc(Message& m)
in System.Windows.Forms.UserControl.WndProc(Message& m)
in System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m)
in System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m)
in System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)
************** Assembly caricati **************
mscorlib
Versione assembly: 4.0.0.0
Versione Win32: 4.8.4180.0 built by: NET48REL1LAST_B
Base di codice: file:///C:/Windows/Microsoft.NET/Framework/v4.0.30319/mscorlib.dll
----------------------------------------
psoc_creator
Versione assembly: 4.3.0.1445
Versione Win32:
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/psoc_creator.exe
----------------------------------------
cycmbase
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cycmbase.DLL
----------------------------------------
System.Windows.Forms
Versione assembly: 4.0.0.0
Versione Win32: 4.8.4150.0 built by: NET48REL1LAST_C
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms/v4.0_4.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
----------------------------------------
System
Versione assembly: 4.0.0.0
Versione Win32: 4.8.4001.0 built by: NET48REL1LAST_C
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
System.Drawing
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Drawing/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
----------------------------------------
cydevicedb
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydevicedb.DLL
----------------------------------------
CyFramework
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/CyFramework.DLL
----------------------------------------
cys3db
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cys3db.DLL
----------------------------------------
CyPrjMgmt
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/CyPrjMgmt.DLL
----------------------------------------
cygde
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cygde.DLL
----------------------------------------
cygdegfxlib
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cygdegfxlib.DLL
----------------------------------------
cydebugger
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydebugger.DLL
----------------------------------------
cyautomation
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyautomation.DLL
----------------------------------------
System.Core
Versione assembly: 4.0.0.0
Versione Win32: 4.8.4180.0 built by: NET48REL1LAST_B
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Core/v4.0_4.0.0.0__b77a5c561934e089/System.Core.dll
----------------------------------------
System.Configuration
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Configuration/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll
----------------------------------------
System.Xml
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
UIFramework.Product6.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product6.WinForms.DLL
----------------------------------------
UIFramework.Product2.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product2.WinForms.DLL
----------------------------------------
UIFramework.Product5.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product5.WinForms.DLL
----------------------------------------
UIFramework.Product4.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product4.WinForms.DLL
----------------------------------------
CyShared
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/CyShared.DLL
----------------------------------------
System.Management
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Management/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Management.dll
----------------------------------------
System.Web.Services
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Web.Services/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Web.Services.dll
----------------------------------------
dyw2mpla
Versione assembly: 4.3.0.1445
Versione Win32: 4.8.4001.0 built by: NET48REL1LAST_C
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
cydsextensions
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydsextensions.DLL
----------------------------------------
cygnuarmshipped
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/import/gnu/arm/cygnuarmshipped.dll
----------------------------------------
cykeilpk51
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/import/keil/pk51/cykeilpk51.dll
----------------------------------------
cyeditors
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyeditors.DLL
----------------------------------------
UIFramework.Product6.Addons.DotNet.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product6.Addons.DotNet.WinForms.DLL
----------------------------------------
cytransport
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cytransport.DLL
----------------------------------------
cypsocdebugger
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cypsocdebugger.EXE
----------------------------------------
cygdbdebugger
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cygdbdebugger.DLL
----------------------------------------
cyarmdebugger
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyarmdebugger.DLL
----------------------------------------
cyppdeviceio
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyppdeviceio.DLL
----------------------------------------
cywin32deviceio
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cywin32deviceio.DLL
----------------------------------------
bootloader_host
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/bootloader_host.EXE
----------------------------------------
cydsfit
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydsfit.EXE
----------------------------------------
cyfitter_fm
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyfitter_fm.EXE
----------------------------------------
cyfitlib
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyfitlib.DLL
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
ICSharpCode.SharpZipLib
Versione assembly: 0.85.4.369
Versione Win32: 0.85.4.369
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/ICSharpCode.SharpZipLib.DLL
----------------------------------------
System.Drawing.Design
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Drawing.Design/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.Design.dll
----------------------------------------
System.Design
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Design/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Design.dll
----------------------------------------
UIFramework.Product1.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product1.WinForms.DLL
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
MigraDoc.DocumentObjectModel
Versione assembly: 1.32.3885.0
Versione Win32: 1.32.3885.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/MigraDoc.DocumentObjectModel.DLL
----------------------------------------
cyhextool
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyhextool.EXE
----------------------------------------
cykeilspawner
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cykeilspawner.EXE
----------------------------------------
cytunerextensions
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cytunerextensions.DLL
----------------------------------------
cyclangwrapper
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyclangwrapper.DLL
----------------------------------------
PP_Accessor
Versione assembly: 3.24.1.2235
Versione Win32: 3.24.1.2235
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/PP_Accessor.DLL
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
PP_COM_Wrapper
Versione assembly: 3.28.6.4409
Versione Win32: 3.28.6.4409
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/PP_COM_Wrapper.dll
----------------------------------------
PP_PC_Wrapper
Versione assembly: 3.28.6.4409
Versione Win32: 3.28.6.4409
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/PP_PC_Wrapper.dll
----------------------------------------
ProgrammerLibrary
Versione assembly: 3.28.6.4409
Versione Win32: 3.28.6.4409
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/ProgrammerLibrary.DLL
----------------------------------------
Accessibility
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/Accessibility/v4.0_4.0.0.0__b03f5f7f11d50a3a/Accessibility.dll
----------------------------------------
cyp3fit
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyp3fit.EXE
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
AxInterop.SHDocVw
Versione assembly: 1.1.0.0
Versione Win32: 1.1.0.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/AxInterop.SHDocVw.DLL
----------------------------------------
Interop.SHDocVw
Versione assembly: 1.1.0.0
Versione Win32: 1.1.0.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/Interop.SHDocVw.DLL
----------------------------------------
mscorlib.resources
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/mscorlib.resources/v4.0_4.0.0.0_it_b77a5c561934e089/mscorlib.resources.dll
----------------------------------------
System.Windows.Forms.resources
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms.resources/v4.0_4.0.0.0_it_b77a5c561934e089/System.Windows.Forms.resources.dll
----------------------------------------
Microsoft.mshtml
Versione assembly: 7.0.3300.0
Versione Win32: 7.0.3300.0
Base di codice: file:///C:/WINDOWS/assembly/GAC/Microsoft.mshtml/7.0.3300.0__b03f5f7f11d50a3a/Microsoft.mshtml.dll
----------------------------------------
CyComponentLibrary_65fe1f8a6cd32b6e353a8ad0ef05ea46002fba85ebbbd6d3ef946952d7cc7c85
Versione assembly: 0.0.0.0
Versione Win32: 0.0.0.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/psoc/content/cycomponentlibrary/CyComponentLibrary.cylib/CyComponentLibrary.dll
----------------------------------------
cydstoolkit
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydstoolkit.DLL
----------------------------------------
cyprimitives_51970e599dc9fe71dc823be05afcec24d44b6e0795d948dda179790f16769558
Versione assembly: 0.0.0.0
Versione Win32: 0.0.0.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/psoc/content/CyPrimitives/CyPrimitives.cylib/CyPrimitives.dll
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
BLE_PDL_v2_20
Versione assembly: 1.0.0.0
Versione Win32: 1.0.0.0
Base di codice: file:///C:/Users/vitto/Documents/PSoC%20Creator/4.3/Downloads%20(%204.3).cylib/BLE_PDL_v2_20/BLE_PDL_v2_20.dll
----------------------------------------
BLE_v3_65
Versione assembly: 1.0.0.0
Versione Win32: 1.0.0.0
Base di codice: file:///C:/Users/vitto/Documents/PSoC%20Creator/4.3/Downloads%20(%204.3).cylib/BLE_v3_65/BLE_v3_65.dll
----------------------------------------
************** Debug JIT **************
Per abilitare il debug JIT, è necessario impostare il valore
jitDebugging nella sezione system.windows.forms del file di configurazione
dell'applicazione o del computer (machine.config).
L'applicazione inoltre deve essere compilata con il debug
abilitato.
Ad esempio:
<configuration>
<system.windows.forms jitDebugging="true" />
</configuration>
Quando il debug JIT è abilitato, tutte le eccezioni non gestite
vengono inviate al debugger JIT registrato nel computer,
anziché essere gestite da questa finestra di dialogo.
Hi All
PSoC 4.3 is unable to open any project or to create a new one.
I uninstalled all the old PSoC version, I purge all I found about Cypress, I installed (and reinstalled) several time 4.3 version, but no way; it does not work.
The log file I get when I try to open an existing project is here reported.
Should I come back to 4.2 version or Is there something I can do for make it working?
Thanks
Best Regards
Vittorio
Le informazioni su come richiamare il debug JIT (Just-In-Time) anziché questa finestra
sono riportate in fondo al messaggio.
************** Testo dell'eccezione **************
System.NullReferenceException: Riferimento a un oggetto non impostato su un'istanza di oggetto.
in CyDesigner.Common.ProjMgmt.Model.CyPrjMgmtComponentMgr.AreCustomizersAllowed()
in CyDesigner.Common.ProjMgmt.Model.CyPrjMgmtProjectPSoCExe.AreCustomizersAllowed()
in CyDesigner.Common.Db.CyS3Db.CyInst.GetCustomizerProviderImpl(CyCompName compName, CyInstBindContext ctx, String schName)
in CyDesigner.Common.Db.CyS3Db.CyInst.GetCustomizerProvider(CyCompName compName, CyInstBindContext ctx, CyInstCustomizerProvider& custProvider)
in CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetIsDesignWideComponent(CyPrjMgmtProjectPSoCExe proj, CyComponentMaster master, CyCompName compName, CyElabInstBindContext context, Boolean checkLatesetIfDoesNotExist)
in CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetSelectedSupportedComponentsBySource()
in CyDesigner.Device.FitLib.DesignWideResources.Components.CyComponentsModel.GetSelectedSupportedComponents()
in CyDesigner.Common.ProjMgmt.DWR.CyDWRMgr.<get_DwInsts>d__a.MoveNext()
in System.Collections.Generic.List`1..ctor(IEnumerable`1 collection)
in CyDesigner.Gde.ComponentUpdateTool.CyCutDocument..ctor(CyPrjMgmtProjectPSoCExe owningPrj)
in CyDesigner.Gde.ComponentUpdateTool.CyCutInputData..ctor(CyDesignerFramework fwk, IEnumerable`1 mgrs)
in CyDesigner.Gde.Common.CyGdePlugin.UpdateCutStatusBarIcon(Boolean writeOutputMsg)
in CyDesigner.Gde.Common.CyGdePlugin.mgr_CurrentWorkspaceChanged(Object sender, EventArgs e)
in System.EventHandler.Invoke(Object sender, EventArgs e)
in CyDesigner.Common.Base.CyBasic.RaiseEvent(EventHandler eventToRaise, Object sender, EventArgs eventArgs)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.OnCurrentWorkspaceChanged(EventArgs e)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.set_CurrentWrkspc(CyPrjMgmtWrkspc value)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.OpenWorkspace(CyPrjMgmtWrkspc workspace)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.CheckandOpenWorkspace(String item)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.OpenItem(String item)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.RecentProjectHandler(Object sender, CyCommandClickedEventArgs e)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.Execute(EventHandler`1 handler, Object sender, CyCommandClickedEventArgs e)
in CyDesigner.Framework.CyDesignerFramework.CommandClicked(Object sender, BarCommandLinkEventArgs e)
in ActiproSoftware.UIStudio.Bar.BarCommandLinkEventHandler.Invoke(Object sender, BarCommandLinkEventArgs e)
in ActiproSoftware.UIStudio.Bar.BarManager.OnCommandClick(BarCommandLinkEventArgs e)
in ActiproSoftware.UIStudio.Bar.BarManager.b(BarCommandLinkEventArgs A_0)
in ActiproSoftware.UIStudio.Bar.BarManager.a(Command A_0, Boolean A_1)
in ActiproSoftware.UIStudio.Bar.BarManager.RaiseCommand(Command command)
in CyDesigner.Common.ProjMgmt.CyPrjMgr.RaiseRecentPrjCmd(String prjCanonicalName)
in CyDesigner.StartPage.CyStartPageControl.OpenRecentProject(String prjCanonicalPath)
in CyDesigner.StartPage.CyStartPageControl.CyClickableStartPageRow`1.PerformClick()
in CyDesigner.StartPage.CyStartPageControl.m_table_MouseClickedTable(Object sender, CyTableViewMouseEventArgs e)
in CyDesigner.Common.Base.Controls.CyTableViewBase.OnMouseClickedTable(CyTableViewMouseEventArgs e)
in CyDesigner.Common.Base.Controls.CyTableViewBase.OnMouseClick(MouseEventArgs e)
in CyDesigner.Common.Base.Controls.CyTableViewBase.control_MouseClick(Object sender, MouseEventArgs e)
in System.Windows.Forms.Control.OnMouseClick(MouseEventArgs e)
in System.Windows.Forms.Control.WmMouseUp(Message& m, MouseButtons button, Int32 clicks)
in System.Windows.Forms.Control.WndProc(Message& m)
in System.Windows.Forms.ScrollableControl.WndProc(Message& m)
in System.Windows.Forms.ContainerControl.WndProc(Message& m)
in System.Windows.Forms.UserControl.WndProc(Message& m)
in System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m)
in System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m)
in System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)
************** Assembly caricati **************
mscorlib
Versione assembly: 4.0.0.0
Versione Win32: 4.8.4180.0 built by: NET48REL1LAST_B
Base di codice: file:///C:/Windows/Microsoft.NET/Framework/v4.0.30319/mscorlib.dll
----------------------------------------
psoc_creator
Versione assembly: 4.3.0.1445
Versione Win32:
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/psoc_creator.exe
----------------------------------------
cycmbase
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cycmbase.DLL
----------------------------------------
System.Windows.Forms
Versione assembly: 4.0.0.0
Versione Win32: 4.8.4150.0 built by: NET48REL1LAST_C
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms/v4.0_4.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
----------------------------------------
System
Versione assembly: 4.0.0.0
Versione Win32: 4.8.4001.0 built by: NET48REL1LAST_C
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
System.Drawing
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Drawing/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
----------------------------------------
cydevicedb
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydevicedb.DLL
----------------------------------------
CyFramework
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/CyFramework.DLL
----------------------------------------
cys3db
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cys3db.DLL
----------------------------------------
CyPrjMgmt
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/CyPrjMgmt.DLL
----------------------------------------
cygde
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cygde.DLL
----------------------------------------
cygdegfxlib
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cygdegfxlib.DLL
----------------------------------------
cydebugger
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydebugger.DLL
----------------------------------------
cyautomation
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyautomation.DLL
----------------------------------------
System.Core
Versione assembly: 4.0.0.0
Versione Win32: 4.8.4180.0 built by: NET48REL1LAST_B
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Core/v4.0_4.0.0.0__b77a5c561934e089/System.Core.dll
----------------------------------------
System.Configuration
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Configuration/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll
----------------------------------------
System.Xml
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
UIFramework.Product6.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product6.WinForms.DLL
----------------------------------------
UIFramework.Product2.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product2.WinForms.DLL
----------------------------------------
UIFramework.Product5.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product5.WinForms.DLL
----------------------------------------
UIFramework.Product4.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product4.WinForms.DLL
----------------------------------------
CyShared
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/CyShared.DLL
----------------------------------------
System.Management
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Management/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Management.dll
----------------------------------------
System.Web.Services
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Web.Services/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Web.Services.dll
----------------------------------------
dyw2mpla
Versione assembly: 4.3.0.1445
Versione Win32: 4.8.4001.0 built by: NET48REL1LAST_C
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
cydsextensions
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydsextensions.DLL
----------------------------------------
cygnuarmshipped
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/import/gnu/arm/cygnuarmshipped.dll
----------------------------------------
cykeilpk51
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/import/keil/pk51/cykeilpk51.dll
----------------------------------------
cyeditors
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyeditors.DLL
----------------------------------------
UIFramework.Product6.Addons.DotNet.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product6.Addons.DotNet.WinForms.DLL
----------------------------------------
cytransport
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cytransport.DLL
----------------------------------------
cypsocdebugger
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cypsocdebugger.EXE
----------------------------------------
cygdbdebugger
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cygdbdebugger.DLL
----------------------------------------
cyarmdebugger
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyarmdebugger.DLL
----------------------------------------
cyppdeviceio
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyppdeviceio.DLL
----------------------------------------
cywin32deviceio
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cywin32deviceio.DLL
----------------------------------------
bootloader_host
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/bootloader_host.EXE
----------------------------------------
cydsfit
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydsfit.EXE
----------------------------------------
cyfitter_fm
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyfitter_fm.EXE
----------------------------------------
cyfitlib
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyfitlib.DLL
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
ICSharpCode.SharpZipLib
Versione assembly: 0.85.4.369
Versione Win32: 0.85.4.369
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/ICSharpCode.SharpZipLib.DLL
----------------------------------------
System.Drawing.Design
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Drawing.Design/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.Design.dll
----------------------------------------
System.Design
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Design/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Design.dll
----------------------------------------
UIFramework.Product1.WinForms
Versione assembly: 16.1.330.0
Versione Win32: 16.1.330.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/UIFramework.Product1.WinForms.DLL
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
MigraDoc.DocumentObjectModel
Versione assembly: 1.32.3885.0
Versione Win32: 1.32.3885.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/MigraDoc.DocumentObjectModel.DLL
----------------------------------------
cyhextool
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyhextool.EXE
----------------------------------------
cykeilspawner
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cykeilspawner.EXE
----------------------------------------
cytunerextensions
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cytunerextensions.DLL
----------------------------------------
cyclangwrapper
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyclangwrapper.DLL
----------------------------------------
PP_Accessor
Versione assembly: 3.24.1.2235
Versione Win32: 3.24.1.2235
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/PP_Accessor.DLL
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
PP_COM_Wrapper
Versione assembly: 3.28.6.4409
Versione Win32: 3.28.6.4409
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/PP_COM_Wrapper.dll
----------------------------------------
PP_PC_Wrapper
Versione assembly: 3.28.6.4409
Versione Win32: 3.28.6.4409
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/PP_PC_Wrapper.dll
----------------------------------------
ProgrammerLibrary
Versione assembly: 3.28.6.4409
Versione Win32: 3.28.6.4409
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/Programmer/ProgrammerLibrary.DLL
----------------------------------------
Accessibility
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/Accessibility/v4.0_4.0.0.0__b03f5f7f11d50a3a/Accessibility.dll
----------------------------------------
cyp3fit
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cyp3fit.EXE
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
AxInterop.SHDocVw
Versione assembly: 1.1.0.0
Versione Win32: 1.1.0.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/AxInterop.SHDocVw.DLL
----------------------------------------
Interop.SHDocVw
Versione assembly: 1.1.0.0
Versione Win32: 1.1.0.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/Interop.SHDocVw.DLL
----------------------------------------
mscorlib.resources
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/mscorlib.resources/v4.0_4.0.0.0_it_b77a5c561934e089/mscorlib.resources.dll
----------------------------------------
System.Windows.Forms.resources
Versione assembly: 4.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms.resources/v4.0_4.0.0.0_it_b77a5c561934e089/System.Windows.Forms.resources.dll
----------------------------------------
Microsoft.mshtml
Versione assembly: 7.0.3300.0
Versione Win32: 7.0.3300.0
Base di codice: file:///C:/WINDOWS/assembly/GAC/Microsoft.mshtml/7.0.3300.0__b03f5f7f11d50a3a/Microsoft.mshtml.dll
----------------------------------------
CyComponentLibrary_65fe1f8a6cd32b6e353a8ad0ef05ea46002fba85ebbbd6d3ef946952d7cc7c85
Versione assembly: 0.0.0.0
Versione Win32: 0.0.0.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/psoc/content/cycomponentlibrary/CyComponentLibrary.cylib/CyComponentLibrary.dll
----------------------------------------
cydstoolkit
Versione assembly: 4.3.0.1445
Versione Win32: 4.3.0.1445
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/bin/cydstoolkit.DLL
----------------------------------------
cyprimitives_51970e599dc9fe71dc823be05afcec24d44b6e0795d948dda179790f16769558
Versione assembly: 0.0.0.0
Versione Win32: 0.0.0.0
Base di codice: file:///C:/Program%20Files%20(x86)/Cypress/PSoC%20Creator/4.3/PSoC%20Creator/psoc/content/CyPrimitives/CyPrimitives.cylib/CyPrimitives.dll
----------------------------------------
Microsoft.GeneratedCode
Versione assembly: 1.0.0.0
Versione Win32: 4.8.3752.0 built by: NET48REL1
Base di codice: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
BLE_PDL_v2_20
Versione assembly: 1.0.0.0
Versione Win32: 1.0.0.0
Base di codice: file:///C:/Users/vitto/Documents/PSoC%20Creator/4.3/Downloads%20(%204.3).cylib/BLE_PDL_v2_20/BLE_PDL_v2_20.dll
----------------------------------------
BLE_v3_65
Versione assembly: 1.0.0.0
Versione Win32: 1.0.0.0
Base di codice: file:///C:/Users/vitto/Documents/PSoC%20Creator/4.3/Downloads%20(%204.3).cylib/BLE_v3_65/BLE_v3_65.dll
----------------------------------------
************** Debug JIT **************
Per abilitare il debug JIT, è necessario impostare il valore
jitDebugging nella sezione system.windows.forms del file di configurazione
dell'applicazione o del computer (machine.config).
L'applicazione inoltre deve essere compilata con il debug
abilitato.
Ad esempio:
<configuration>
<system.windows.forms jitDebugging="true" />
</configuration>
Quando il debug JIT è abilitato, tutte le eccezioni non gestite
vengono inviate al debugger JIT registrato nel computer,
anziché essere gestite da questa finestra di dialogo.
Show Less
Hi,
I wanted to export a PSOC creator project to an IDE, Is there any documentation or video on how to do that.
- How to export a PSOC project to an IDE?
- After exporting how to open it in the IDE ( Like what is the top level file )? How to run it.
By IDE I mean I wanted to export it to IAR.
Show Less