PSoC™ Creator & Designer Forum Discussions
I am making the “proximity” project with the PSoC CYCKIT040and shield CYC024, and I want to know the capacitance by the formula. But I get trouble with sense clock frequency Fsw and the current Icomp/Imod, could anyone help me ?thanks.
Show LessHello together,
under Build Setting in PSOC Creator I can only find the GCC and MDK under Toolchain. Is there a possibility to add IAR toolchain to this menu?
Thanks and Regards
Show LessI'm using CYBLE-416045-02 in a custom application. I am trying to configure a switch as a sleep/wake-up button. I am able to use the interrupt to wake up from 'sleep', but not from 'deep sleep'.
I followed the suggestion from this thread, but without success:
Re: GPIO Interrupt won't wake from DeepSleep
I am using a Global Signal to generate the interrupt:
And I am initializing the interrupt like this:
On the first button press, the interrupt is generated, and the MCU goes to deep sleep. But subsequent button presses do not wake the system up from deep sleep.
Additionally, the code worked on the Psoc 6 development kit, but is not working for my custom PCB. Are there any suggestions for what I may be missing?
Thank you!
Show Lesshello there i'm in Psoc creattor 4.2 and i'm working code exemple i didn't change anything in the project i tried to build but i have this error "Unable to open file from disk: (A window with the key 'K:\Documents\PSoC Creator\project adress\CYPD3175-24LQXQ_pa_direct_fb.cydsn\Generated_Source\PSoC4\project.h' is already being managed by the dock manager. Create a unique key to add the window.)" i generated folder i can see the project.h with "?" symbol what does that means how i can i fix the problem ?
Show LessThe device is developed using PSOC5 (PSoc Creator 4.3) on CY8C5888AXI-LP096.
The compiler uses "ARM GCC 5.4-2016-q2-update".
The upper part of the following if statement is normal, but the lower part gives a compile error.
Please tell me the cause.
prj.M0120:Build error: region RAM overflowed with stack
Show Less
int KaDIM[2][5] ={0};
const KaDIM_ini[2][5] = { {1,2,3,4,5} ,{7,8,9,10,11}};
#if 0
KaDIM[0][0] = KaDIM_ini[0][0];
KaDIM[0][1] = KaDIM_ini[0][1];
KaDIM[0][2] = KaDIM_ini[0][2];
KaDIM[0][3] = KaDIM_ini[0][3];
KaDIM[0][4] = KaDIM_ini[0][4];
KaDIM[1][0] = KaDIM_ini[1][0];
KaDIM[1][1] = KaDIM_ini[1][1];
KaDIM[1][2] = KaDIM_ini[1][2];
KaDIM[1][3] = KaDIM_ini[1][3];
KaDIM[1][4] = KaDIM_ini[1][4];
#else
for(int i=0;i<2;i++)
{
for(int j=0;j<5;j++)
{
KaDIM
= KaDIM_ini ; }
}
#endif
Hello,
i am using Cy8c4125lqi-483 and cy8c4146lqi-s433 both, i want to connect 2 GPIO pins internally (i want to short them each other). Are these chips allow this process? If not, which chip i can use with the similar pin outs? Thank you for replies.
Show Lessin PSoC creator, is there a way to save the user input files, such as main.c, topdesign, pins, that have the user input, and not save generated files?
do the user input file names indicate that they are user input files?
do the generated file names indicate that they are generated?
Show LessI work with PSoC Creator 4.3 but need to export the projects for compilation with IAR.
In cy8c6xx7_cm4_dual.icf (a linker file for the IAR compiler), the definition of /* Supervisory FLASH - User Data */ states:
define symbol __ICFEDIT_region_IROM3_start__ = 0x16000800;
define symbol __ICFEDIT_region_IROM3_end__ = 0x160007FF;
which places the end before the before the start. Looking at the other linker files it probably must be:
define symbol __ICFEDIT_region_IROM3_end__ = 0x16000FFF;
or am I missing something?
Show LessDear Cypress/Infineon team,
Please see a wishlist for basic feature requests for PSoC Creator 4.4
- Make it more git friendly.
- Make it possible to remove the binary project file and only use the xml based one.
- Do not touch/modify project files that is not changed (today they get modified by just viewing the project)
- Generate a list of ALL auto-generated files to make .gitignore creation more clear.
- Make it possible to script or import items to the schematic editor
- We use tools that export a control-file based on the schematic-software (altium) Netlist, this is great to modify the pins mapping in Creator, very useful when pin-swapping during layout.
- But you still need to first create and name all the pins in Creator, it would be great if we could create these 'pins' placeholders programmatically.
- Offer a standard netlist export for the schematic created in Creator.
- This could also be any easy to parse file-format such as a .json or .xml
- i.e. peripheral type, names, pin-config etc.
- A headless compiler that can be run command-line on Linux & Mac
- If you use 'DotNet Runtime', porting it should be very straight forward.
Thanks David
Show LessHello,
I have a MiniProg4 which is recognized by the Cypress Programmer 3.0 just fine. However, the MiniProg4 isn't recognized by either PSoC creator 4.2 or PSoC Programmer 3.28.07.
I'm running Windows 10 x64. I have a second machine with the same version of PSoC Creator, PSoC Programmer, and Cypress Programmer and the same MiniProg4 is recognized on this machine by all 3.
I've verified the device shows up on Device Manager and appear to be functioning properly according to Windows 10. Any ideas?
Show Less