PSoC™ Creator & Designer Forum Discussions
text.format{('custom.tabs.no.results')}
I have a question regarding the following issue.
I have opened a project from an existing folder/directory. I am seeing the following two issues and saw the suggestion to reach out to customer support as shown in the screenshot below:
- Cannot find CapSense component.
Here is the screenshot of the schematic
Here is the screenshot of the error in Output window:
Please let me know how to resolve these issues so that I can build my project and debug.
Looking forward to your response.
Thank you,
Arshiya Tabassum !PSoC Creator
Show LessHello,
Does anyone know if there are published system requirements for PSOC programmer such as OS and cpu/memory? I just need it for documentation purposes but have not really found anything in Cypress' documentation.
Show LessHello,
I'm using sw CySmart 1.3 and I often restart it. Each time I have to make the same settings according to my needs, and I don't see the option of saving the Master Settings. Is there such a thing? Maybe it is obvious, but for me not
Show LessI have about 800 Mb of files saved under directory PSoC Creator on my local drive.
I want to move all of it to the company server (sort of server - it is actually dropbox) .
windows 10 will let me drag and drop said files, but i am concerned that
whatever links and relationships there are between them, produced by PSoC Creator,
will disappear with the net result that all will be lost and unre-coveable
is there a procedure to move said files and not lose the (presumed) links and relationships,
so that the files behave the same, open the same, and save as when they are local?
Show LessWhen i Try to Use the feature "Find All Active References" in PSoC Creator I get this error:
Unhandled Exception has occurred in a component in your Application. ..... File format is not valid.
************** Exception Text **************
System.ArgumentException: File format is not valid.
at System.Windows.Forms.RichTextBox.StreamIn(Stream data, Int32 flags)
at System.Windows.Forms.RichTextBox.StreamIn(String str, Int32 flags)
at System.Windows.Forms.RichTextBox.set_Rtf(String value)
at CyDesigner.Framework.FindReplace.CyFindResultsToolWindow.UpdateDisplay(Boolean scrollToEnd)
at CyDesigner.Framework.FindReplace.CyFindResultsToolWindow.ForceDisplay(Boolean scrollToEnd)
at CyDesigner.Common.Editors.CyFileEditor.FindAllReferencesDoneCallback(CyRsltOrErr`1 result)
at CyDesigner.Common.Editors.ClangDetail.CyClangRequest`1.<>c__DisplayClass2`1.<CallbackInvoker>b__0(Object obj)
This fail is present both in version 4.3 and 4.4
The rest of the details are attached.
Show LessWe intend to use Cypress PSoC Creator 4.3 and CYBLE-214015-01 in a medical device development according to IEC 62304 and FDA guidances.
The medical device has moderate level of concern (FDA) and software safety class B (IEC 62304).
- Do you have a validated/certified PSoC Creator according to IEC 62304 and FDA guidances?
- Do you have a basic documentation for the sources generated by PSoC Creator?
- Do you have a basic documentation for the standard library functions like memcpy, etc.
A basic documentation means an answer to the following questions:
- Identification of the OTS / SOUP Software
- Title
- Manufacturer and Country of Origin
- Version Level
- Release Date
- Patch Number
- Upgrade Designation
- Retrieved from
- Digital Signature or Checksum
- Reference Documentation
- Known Bugs
- Availability as Source Code
- Access to Updates
- Hardware and Software Requirements
- Actions Required by End Users
- License Information
- Copyright Information
- Expected Design Limitations
- Description of the OTS / SOUP Functions
Hi all, I hope this is OK for me to post and is the correct place to post this question.
I have a HOTAS PC joystick game controller (Hand On Throttle And Stick) which uses a Cypress CY8C24894. Unfortunately, the throttle stopped being recognised by windows via USB. Apparently this is very common and sourcing a repolacement PCB direct from Thrustmaster is the fix. I've contacted Thrustmaster and hopefully I'll get a replacement PCB soon.
However, being somewhat of a electronics hobbiest, I started to wonder how easy it would be to source a new chip. I've soldered many small SMD packages before. So I ordered a couple of CY8C24894 chips and I've since replaced the defective chip with a new one.
Now, obviously this chip is brand new and has nothing on it. Obviously the proprietary Thrustmaster firmware updater app doesn't recognise it. I'm assuming I need to get a bootloader onto the chip via the I2C interface? But, even then, will the Thrustmaster updater app recognise it?
Anyway, no great shakes if I can't do anything. Hopefully a replacement PCB will arrive from TM soon. I was just curious, I like a challenge and I'm always up for learning something new.
If anyone can provide any information on how to get the TM firmware onto the new cyrpess chip, I would be very grateful to you.
Many thanks in advance.
Show LessHi, i have gotten some problems when i try to start on my psoc creator 4.4, because it doesn't begin and windows show up a compatibility problem, i have been using psoc creator since july with out problems, but on the last week appeare the problem.
I appreciate any help or advice, thanks.
Show Less
Greetings,
My project has a warning (see below) saying that the clock accuracy is not within the specified tolerance range. What are the implications of this warning? Any suggestions on how to fix it?
Thanks in advance!
Show Less