Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ Creator & Designer Forum Discussions

Sort by:
hayc_4840776
PSoC™ Creator & Designer

i want program cy8c27443 ,make a project , but i can not find it ,in the PSoCCreator4.4

tisc_4786871
PSoC™ Creator & Designer
I'm integrating class B library from Cypress/Inf and I come across a weird problem with PSoC Creator when I build with the flash self test included in... Show More
WiFl_1166056
PSoC™ Creator & Designer
I have a project that runs fine.  I committed it to SVN. Then I added an RTC component and committed the project update to SVN, except I forgot to add... Show More
ETRO_SSN583
PSoC™ Creator & Designer
I downloaded both the ISO and the basic install file from you site, they both error on installon a cab file being corrupted.psoc_creator_3.3_cp3_b9648... Show More
FrSt_4749731
PSoC™ Creator & Designer
Hello to all,I am using BLE v3.30 and am testing authentication fail situations. One of them is also to enter wrong pin code.I also read Bluetooth Low... Show More
ReMa_3807036
PSoC™ Creator & Designer
Hi, I'm using PSoC Creator 4.3 with device PSOC4100S  CY8C4125AXI-S433, in my design I'm using Flash to emulate EEprom and I'm following the relative ... Show More
ErJa_4614451
PSoC™ Creator & Designer
I'm using PSoC creator 4.3In the Workspace Explorer window, when I create a folder in my source files folder, I would like that folder to also be crea... Show More
KrDe_284951
PSoC™ Creator & Designer
Hi,We installed Psoc Creator 4.4 on a brand new Windows 10 machine. We copied an existing old working PSoC3 project (using the same Keil version C51 c... Show More
MaMo_1429561
PSoC™ Creator & Designer
Hello Community,I am currently evaluating RTC backup time after POR in PSoC6 BLE PIONEER KIT. As mentioned in the schematic there is a supercapacitor ... Show More
StKr_1203736
PSoC™ Creator & Designer
I have 7 calls to an external function within one source file. ONLY FOUR generate this error. I have tried copying one of the "good ones" over the bad... Show More