PSoC™ Creator & Designer Forum Discussions
I am having issues with PSoC designer while compiling a project. Up till yesterday everything was working fine however since this morning compling a project is taking anywhere from 5 to 10 minutes. This used to take about 20 seconds. I have tried restarting the computer and also i uninstalled the designer and reinstalled it again. The problem still exists.
I also noticed that everytime i try to restart or shut off the computer i get and error: CMXPD - System can not end this program because it is waiting for a response from you.
Not sure what is going ond and why it is taking this long to compile a project.
Any help would be greatly appreciated.
Thanks,
Arun
I recently ran into a problem when trying to share a project with a co-worker here that I thought might be easily resolvable if I could get the feature added to next release of Creator.
Specifically the "Additional Include Directories" under the Compiler configuration doesn't currently allow for relative paths to be used. I even tried manually editing the .cyprj file to force this (which caused Creator to crash during compilation) to no avail.
Would it be possible to add the ability to use relative paths for these include directories? Trying to use any Creator project between more than one person becomes quite difficult, especially so when the code is stored in a revisioning system(i.e., CVS/SVN and the like), as every time someone different wants to use the project they must update the include directories to reflect their PCs file system.
Thanks, hopefully this is a relatively minor change...(horrible pun)
Regards,
Joe
Show LessIs there an expected release date yet for PSoC Creator Beta 5? I am specifically interested in the source code for creating a custom Bootloader-type project that is supposed to be included with Beta 5. We need to be able to receive Bootloadable code via a WirelessUSB radio link and program it to Flash. This means the Bootloader will need to include radio driver code as well as be able to program Flash without an externally connected I2C host.
Show LessIs there anyone interested in a lighter version of PSoc Designer? A version which could work on a low performance machine.
Post a reply if interested.
Show LessHas anyone had biuld errors when using the CSD property module ans CSd buttons? I get a cant find the CSDpropertyConst file error. I never had this issue with the previous version of Designer, so maybe some new bug.
Stephen
Show LessHallo everybody.
I'm new to Psoc so i'm starting with the latest tool, the Psoc Creator. After searching and searching the question remains: how is possible to integrate a simple IIR filter in my project using the DFB - DSP capabilities of the psoc3 (or psoc5) ?
in Psoc Creator only a FIR filter element is available by now , (and seems not suitable for filtering out the 50 hz hum from the adc output)
I know that a simple and effective filtering could be done writing a filter in C language and letting the MCU execute the task, but the MCU has something else to do, and is a perfect job for the DFB - DSP block, anyway.
So, can anybody suggest a way , and possibly were to find the relative documentation? I tougth that maybe was possible to take some DSP code and create a new library component or maybe link some external code as a library but found no hints.
Thanks in advance for any suggestion
Show LessHi,
I noticed PSoC Creator gives an error when I disable the debug property at both the bootloader project and the main project.
ADD: pft.M0047: error: The 'Enable' property of the System DWR for the Bootloader and Loadable projects must match but don't. Bootloader ('Bootload01') has value 'False' and Loadable ('UMR01_T_01a35') has value 'True'.
This error is issued false because the Loadable (UMR01...) has the debug enable property set to false. I'll attach a screenshot. Funny thing is the project finally builds well 🙂
There are also problems with the debug port selection, setting them both to 'none' also gives an error.
Does PSoC Creator take the corresponding build configuration (debug/release) for the bootloader also, or does it always take the one in the 'debug' folder?
At last, it would be nice if the DWR settings would automatically switch when switching from 'debug' to 'release' and vice versa.
Thanks!
Rolf
I have installed the psoc designer 5 sp5 and also tryed the sp5.5 but no sdcard modules.
With the previous psoc designer 5 sp4a there was the sdcard modules.
Please help to find the sdcard user module.
using cy8c29466 in the project.
Thank you
Luigi Palumbo.
Show Less
I do like the way these graphic editors look, but I don't think they are so easy to handle when it comes to zooming and panning throughout the pages - though they aren't really big.
As I am an Altium Designer user, I think it'd be quite handy to go about their solution, which is:
Zoom in : Ctrl + mouse wheel forward / keystroke(configurable)
Zoom out : Ctrl + mouse wheel backward / keystroke(configurable)
Pan left: Shift + mouse wheel forward / left arrow key (configurable) / 2D mouse wheel left
Pan right: Shift + mouse wheel backward / right arrow key (configurable) / 2D mouse wheel right
Pan up: mouse wheel forward / up arrow key (configurable)
Pan down: mouse wheel backward / down arrow key (configurable)
Dragging: Hold right button on the mouse and move the cursor.
With the help of mice equiped with configurable buttons, many people (including me) are getting used to navigating graphic GUI with only one hand. It'd make us a lot more efficient if such enhancement was introuduced. Thanks.
Show LessFor instance, suppose you're designing a modem to be used over simplex radio. (Simplex is where you take turns transmitting and receiving, as compared to full-duplex where you transmit and receive at the same time.)
Can you use all the op-amps on the chip to receive audio and decode it to digital data and then re-wire some of the op-amps to generate audio from your digital data when you switch to transmit? Show Less