PSoC™ Creator & Designer

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
EthanHQaQ
PSoC™ Creator & Designer
Hello, Recently I tried to use StripLights component from WS281xLib on the CY8C4146AXI-S455, while I met the error seen as attached.  Is that because ... Show More
Etry
PSoC™ Creator & Designer
I am using PSoC Creator 4.3 and my team uses git for version control. On my projects, whenever I "add existing item" or "remove from 'project_name'" t... Show More
willrow
PSoC™ Creator & Designer
Hello, Recently I have been playing with the CapSense block in PSoC 4.3 with the specific aim of trying to maximise the rate at which I can poll the e... Show More
PascalS
PSoC™ Creator & Designer
Hello, I'm using a CYBLE-416045-02 Controller and want to read out some registers from an external I2C sensor. I followed Infineon's instructions how ... Show More
alexr
PSoC™ Creator & Designer
Since PSoC Creator still requires Windows, I've been trying to get it to run on a Windows 11 on ARM64 installation. I've tried a variety of systems, b... Show More
pbedesign34
PSoC™ Creator & Designer
I have a product that uses a CY8C29556, but due to the chip shortage it is not available. For a temporary sub, I've found the CY8C28533, which might w... Show More
Praba
PSoC™ Creator & Designer
I am Using the Controller CY8C29466-24SXI . In that Just Configuring the Port Pin to Turn ON And OFF the LED . But Controller Not responding its Point... Show More
yuna_4671381
PSoC™ Creator & Designer
The device is developed using PSOC5 (PSoc Creator 4.3) on CY8C5888AXI-LP096.Although cyPm.h is generated by the code generation at compile time, the f... Show More
Len_CONSULTRON
PSoC™ Creator & Designer
Hi, I'm hoping someone can provide some wisdom to officially solve a compiler/linker issue that I'm encountering with Keil. I'm a seasoned programmer ... Show More
BellMan
PSoC™ Creator & Designer
Hello, I bought a CY8CKIT-046 and working on a project that requires audio file from SD card to be played back. Do you have an example project for the... Show More
Forum Information

PSoC™ Creator & Designer

Discussion forum regarding PSoC Creator & Designer Software topics.
Top liked authors