PSoC™ Creator & Designer Forum Discussions
text.format{('custom.tabs.no.results')}
I would like to see more options in the device selector.
Especially, I would like to be able to filter results on the availability of Fixed Dunction Blocks, such as USB. So for example I could just see all the PSoC3 devices which have USB ability. (Or any of the other fixed function blocks, like I2C, I2S etc).
Show LessApparently the LED module refers to the need for the user to
use Shadow Registers, but datasheet does not convey the module
takes care of this for the user. Eg,. user does not have to place
a separate Shadow Register module to use the LED Module.
See thread http://www.cypress.com/?app=forum&id=1573&rID=67778
Regards, Dana.
Show LessThe nomenclature on plots is confusing.
"Nominal" should be changed to "desired" or "ideal"
"Expected" should be changed to "PSOC actual" or "PSOC result".
Regards, Dana.
Show LessWould be nice if right clicking in either of these views a .bmp or .jpg picture of
just that part of the desktop view could be saved. Including when veiw is magnified.
Regards, Dana.
Show LessHow do I send you a direct email ? On the topic of Rewards Points and
Wireless kits I posted earlier. http://www.cypress.com/?app=forum&id=2492&rID=68285
Regards, Dana.
Show LessI tried hard to understand the "Component Author Guide" but some things are not quite clear to me:
When I want to design a component that uses several I/O pins and the number of pins should be parameterized in the configuration dialog
1st. How to generate in Verilog (or is there a better/easier way?) the pins
2nd. How to set the properties of the pins (even if they are all the same)
Regards, Bob
Show LessI found a very minor bug in PSoC Creator 2.1.0.607
It may not even be a bug - what do you think?
If you have multiple files open and you select one by clickin on it's tab.
The you right click on a different tab and select 'Close all but this' then it is the selected tab that stays open, not the one you right-clicked on.
Show Less