PSoC™ Creator & Designer Forum Discussions
Any thought given to upgrading this utility to handle upgraded current version of Imagecraft compiler ?
http://www.psocdeveloper.com/forums/viewtopic.php?f=3&t=9&p=10&hilit=stackwalk#p10
Very useful for working in C with small RAM based parts, a problem I am having now.
Regards, Dana.
Show Lessthis is my program
#include <m8c.h> // part specific constants and macros
#include "PSoCAPI.h" // PSoC API definitions for all User Modules
void main(void)
{
// M8C_EnableGInt ; // Uncomment this line to enable Global Interrupts
// Insert your main routine code here.
PGA_SetGain(PGA_1_G8_00);
PGA_Start(PGA_1_MEDPOWER);
}
and this is my errors
!W C:\Users\hai\DOCUME~1\PSOCDE~1.3PR\PDPROJ~4\PDPROJ~1\main.c(14):[warning] [MISRA 2200]calling an undeclared function may cause unexpected behavior if the function
takes or returns values other than int
!W C:\Users\hai\DOCUME~1\PSOCDE~1.3PR\PDPROJ~4\PDPROJ~1\main.c(14):[warning] [MISRA 2714]calling a function without prototype may cause unexpected behavior if the function
takes or returns values other than int
!W C:\Users\hai\DOCUME~1\PSOCDE~1.3PR\PDPROJ~4\PDPROJ~1\main.c(15):[warning] [MISRA 2200]calling an undeclared function may cause unexpected behavior if the function
takes or returns values other than int
!W C:\Users\hai\DOCUME~1\PSOCDE~1.3PR\PDPROJ~4\PDPROJ~1\main.c(15):[warning] [MISRA 2714]calling a function without prototype may cause unexpected behavior if the function
takes or returns values other than int
./boot.asm
Linking..
LMM info: area 'virtual_registers' uses 2 bytes in SRAM page 0
!ERROR {linker} file 'main.o': undefined symbol '_PGA_SetGain'
!ERROR {linker} file 'main.o': undefined symbol '_PGA_Start'
make: *** [output/PDProject4.rom] Error -1
Show LessSince installing PSoC Creator 2.1 I have noticed that it is less responsive then previous versions.
The mouse doesn't move about the screen smoothly, keyboard entry is a bit 'glitchy' with a noticeable stutter.
When Creator 2.1 is actually idle - the IDE open, a project loaded, but doing nothing at all it consumes between 4 and 10% of CPU time. What on earth is Creator doing?
The system I'm running on is usually a fast and responsive machine. It is a Dell Lattitude with 8 GB of ram. It has 8 CPU cores and is normally a very responsive machine.
Anyone else seeing this?
Show LessAttached is a library of three DACs that provide alternatives to acheive more than the native 8-bits of resolution found in the PSoC3 and PSoC5LP devices. These DACs provide resolution with reasonable INL and DNL to 10 or 11 bits. More information and example projects can be found in the application note AN64275.
Mark
Show LessIn the example projects, specifically the ADCINC and ADC10 projects,
you use floating point math to display the voltage read on the LCD.
I would like to suggest you do these in integer math, because of the cost
of the float library in code space, especially in light of the the ADC10 project
using a CY21xxx part. Do the calcs in mV and then display as a float repre-
sentation by acting/formatting on the ltoa() or itoa() output appropriately.
Regards, Dana.
Show LessWould be great if there was a Wireless Forum category.
SCD Enahncements -
1) Allow simultaneous graphing and datalogging.
2) When data logging, cache the data with a number of entries before writing to
disk. For those PC systems on low power, like disk sleep, not to have to
continuously write disk at the sampling rate.
Regards, Dana.
Show LessHi,
I'd like to connect a port pin and pass it's state to a datapath register(d0 or d1) and do alu. Can anybody tell me how can I wire a port pin to a datapath register? Thank You.
TJ
Show LessHello All,
When I boot up the Cypress Update Manager software and click "Check for updates", I see a "No Updates Availible" message. i have PSoC Creator 2.1 component pack 4, and I understand that Service pack 1 is now availible. What do I have to do to get this to work?
Thanks,
DiodeDan
Show LessOne Cypress emplyee mentioned a problem with PSoC5 compiler issue.
Could Cypress engineer confirm this?
http://www.cypress.com/?app=forum&id=2233&rID=70185&message=posted
Show LessPlease, i have 4 PCB ready to programmed for end-use.
What software versions / kits do i need to program / debug firemware for CY7C63743 MCUs?
Thanks!
Show Less