PSoC™ Creator & Designer

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
GiLi
PSoC™ Creator & Designer
Hi Cypress, I recently looking into the 4700S series, but i found that there are not much code example for this series, only 8 of them.  I tried to f... Show More
alex4
PSoC™ Creator & Designer
hello used PSoc 4.2. i defined a uint8 XXX variable. in another file, by mistake,  this variable defined as: extern uint32 XXX; there was no warning. ... Show More
alexr
PSoC™ Creator & Designer
Since PSoC Creator still requires Windows, I've been trying to get it to run on a Windows 11 on ARM64 installation. I've tried a variety of systems, b... Show More
trtr_1961036
PSoC™ Creator & Designer
I have a compilation error on psoc creator 4.4 between break point and no break point Environment:PSoC Creator 4.4 (4.4.0.80)Culture: English (United ... Show More
RuGl_1600761
PSoC™ Creator & Designer
Using PSOC Creator 4.4 on a win7 x64 system I get the following error message: after clean and build I get: prj.M0120:Build error: The command 'arm-n... Show More
adamelli
PSoC™ Creator & Designer
So I have this main.c program that was made long ago (by another employee). It was made for CY8C4245PVI-482. I'm trying to understand the program, but... Show More
Anonymous
PSoC™ Creator & Designer
I got introduced to the PSoC 5 chip by the freeSOC project on Kickstarter (and smARtDUINO, which is compatible with it). They are part of the Arduino ... Show More
akrupaa
PSoC™ Creator & Designer
Hello,  I am searching for a solution or guide, how to setup PsoC Creator (or other IDE or VSCode) on Windows 10 and OpenOCD/GDB running on Linux. I h... Show More
cadi_1014291
PSoC™ Creator & Designer
Hi,Are there plans to improve the code editor in PSoC Creator? Here a little list of points i would like to see improved:- Working bookmarks.- Dark co... Show More
ricardoquesada
PSoC™ Creator & Designer
Hi, I'm using PSoC Creator 4.4. In case it helps I'm targeting PSoC 5LP. And I can compile my project from IDE without any problem.   But I want to in... Show More
Board Information

PSoC™ Creator & Designer

Discussion forum regarding PSoC Creator & Designer Software topics.
Top liked authors