PSoC™ Creator & Designer Forum Discussions
Hey Bob, seems like its you and me recently.
I apologise if this has been asked hundres of times but I have looked at the examples and data sheet and I did see a simple tutorial a while ago and cannot remember where I saw it.
I am wanting to use USB UART to connect my project to PC. I dropped the component on the worksheet and based a simple application based on the example in Creator (receives USB data and sends back to PC, I remobed the LCD portion).
When I plug into my PC, I see USB UART appear under ports in devices dialog with the yellow warning.
I downloaded a driver for windows and found Windows 8 dll and ran the install for the driver but still does not install the driver.
I am sure there is some obvious step I have glossed over setting up the component or installing the driver. If I can set it up as HID device then maybe I don't need to install specific driver, would be good if it uses windows standard drivers.
Thanks
Show LessHi,
I am developing a setup using PSoC 5 and KIT-001. i want to control the activity from my system. so i initiated the USB communication using CYUSB in my VB. using this i can successfully ,communicate to the KIT and i am able to read also.
i need to know how can i read the data whenever the bulkIN is not empty. that means, whenever i want to send some data to my PC, my tool in PC must be able t o detect it display that.
Thanks
Vinay
Show LessMy list of components is empty.
I receive a message that there is a problem with any cryptographic algorithm (FIPS?) In Windows 8.1 Home.
Hello,
i can read out Chipid and BUTTON_STAT from CY8CMBR3101 over I2C and can write Register GPO_OUTPUT_STATE.
But changing GPO_CFG and PWM_DUTYCYCLE_CFG0 has no effect. Whats the problem?
Günter
Show LessHi, I'm wondering if there is any ability to connect PSoC creator to an external gdb server. I understand that Cypress only supports the miniProg debugger (which is understandable) but I know that it uses gdb as it's underlying debug system. My question is if it would be possible to modify the configuration files to redirect to an external server such as a JLink system.
Currently I've been exporting my projects to Eclipse for code development, but since I usually end up tweaking the hardware configuration multiple times during the debug process it would be nice to be able to perform everything within a single environment.
Ideally, it would be awesome if we could define custom tools within PSoC creator that could launch/pass commands to other programs. (similar to Eclipse)
If anyone here doesn't know a way to connect an external gdb server, I'll experiment on the system myself and post any solutions that I find.
Show LessI have an application that is polling a remote device for data. The polling device needs to be able to determine when the remote unit is responding or not.
At the moment I have an error count that increments each time the poll is not responded to and when count is exceeded the operator gets a warning. If the remote unit starts to respond again then operator gets indication that remote unit is ok.
During testing, I remove the cable to remote unit and get the warning. However, when reconnecting Somethings the system detects the device available and gives notice but often it does not and the code appears to stop responding. As the "Pause" function does not work when this happens, I cannot look at the call stack to see where it s.
What I am doing after loss of remote reposnse is to stop and restart the UART component. I don't think this is the best approach and cannot find a clear tutorial regarding recovering from UART errors.
Is there a status I can read and reset the flags after error detected so the UART can recover after hardware fault (serial lines being disconnected and reconnected)
Thanks
Show LessWhen I halt the debugger (Attached to MiniProg 3), the code continues to run. To get it to stop running, I again run the debugger to start of code and then stop.
Is there a button or something I can click that stops the code in the MiniProg 3 from running?
Show LessHi,
I am currently using a PSOC Creator 3.0 for creating a simple psoc 4 application and I am looking for a way to add version number to the hex file properties.
I tried googling for a way to this but had no luck so far.
Any help regarding this is highly appreciated.
Thanks and Regards,
Balu Ramamurthy
Show LessCould you solve this?
I want to open sample projects, but pass error occures.
Psoc tells:
Unable to save the workspace's user data file "C:\Program Files\Cypress\example\SCB_Bootloader_42xx\SCB_Bootloader.cywrk.usernamexxx": (pass 'C:\Program Files\Cypress\example\SCB_Bootloader_42xx\SCB_Bootloader.cywrk.usernamexxx' denied access to). Address the error in order to save the user info.
Thank you .
Show LessHello everyone,
1. I Have a 4 BTNS available to me for my slider.
2. The slider consists of 4 stage operation.
3. I do not hold an extra BTN for the ON-OFF control.
4. How would I get the slider working ok if the conditions are-
a> #1 BTN = #1 LED ON & slider ON; rest LEDs OFF
b> #2 BTN = #2 LED ON; rest LEDs OFF
c> #3 BTN = #1 & #2 both LEDs ON; rest LEDs OFF
d> #4 BTN = # 4 LED ON; rest LEDs OFF
e> when I return (touch) to #1 BTN while slider is ON, slider should turn OFF
f> Then repeat the ( a> to e> ) steps.
5. When I again press the #1 BTN (even time touch @#1 BTN should turn OFF (power Off) the slider & odd time touch @#1 BTN should turn ON (power On) the slider) it should turn off the slider, i.e. power Off.
6. At any point of operation for the even touch slider is off.
7. At any point of operation for the odd touch slider is on.
8. When #1 BTN is off i.e. slider is off no other segment of slider is in operation.
Can i do this in the abov specified circumstances, guide on the same.
Thanks & Regards-
Amit
Show Less