PSoC™ Creator & Designer Forum Discussions
text.format{('custom.tabs.no.results')}
I am just trying Creator 3.1 for the first time (3.1 (3.1.0.1570)) ( and a later version as well) and I cannot build any project that uses any part of the gcc toolchain on a computer running windows vista.
The error messages are
'arm-none-eabi-gcc.exe: error: CreateProcess: No such file or directory'
'arm-none-eabi-gcc.exe' failed with exit code '1'
The same two versions of creator installed on a windows7 virtual machine running on linux work perfectly ok with no changes to the default installation and they also work fine on a native win7 install on another machine.
Is there a problem running the software on a windows vista machine?
Show LessI have attached an image of the error I get everytime I 'step over' or 'step into' a statement in Debug mode. This is the case for both PSoC Creator 3.0 & 3.1. Has anyone come across this issue recently? Any pointers on how I could go about resolving this?
Much appreciated,
V
Show LessPretty consitently I get the below error when trying to upload zip file
using explorer, firefox, chrome -
struct | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Detail | The value of the attribute destination, which is currently C:\inetpub\wwwroot\Cypress.com\files\, is invalid. | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Message | Attribute validation error for tag CFFILE. | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
StackTrace | coldfusion.tagext.InvalidTagAttributeException: Attribute validation error for tag CFFILE. at coldfusion.tagext.io.FileUtils.determineDest(FileUtils.java:591) at coldfusion.tagext.io.FileTag.upload(FileTag.java:652) at coldfusion.tagext.io.FileTag.doStartTag(FileTag.java:268) at coldfusion.runtime.CfJspPage._emptyTcfTag(CfJspPage.java:2722) at cfForum2ecfc672310569$funcEDITPOST._factor5(\\121019-admin\s$\com\cypress\services\Forum.cfc:987) at cfForum2ecfc672310569$funcEDITPOST._factor6(\\121019-admin\s$\com\cypress\services\Forum.cfc:982) at cfForum2ecfc672310569$funcEDITPOST._factor7(\\121019-admin\s$\com\cypress\services\Forum.cfc:980) at cfForum2ecfc672310569$funcEDITPOST.runFunction(\\121019-admin\s$\com\cypress\services\Forum.cfc:976) at coldfusion.runtime.UDFMethod.invoke(UDFMethod.java:472) at coldfusion.runtime.UDFMethod$ReturnTypeFilter.invoke(UDFMethod.java:405) at coldfusion.runtime.UDFMethod$ArgumentCollectionFilter.invoke(UDFMethod.java:368) at coldfusion.filter.FunctionAccessFilter.invoke(FunctionAccessFilter.java:55) at coldfusion.runtime.UDFMethod.runFilterChain(UDFMethod.java:321) at coldfusion.runtime.UDFMethod.invoke(UDFMethod.java:220) at coldfusion.runtime.TemplateProxy.invoke(TemplateProxy.java:490) at coldfusion.runtime.TemplateProxy.invoke(TemplateProxy.java:336) at coldfusion.runtime.CfJspPage._invoke(CfJspPage.java:2360) at cfeditpost2ecfm1427110115.runPage(\\121019-admin\s$\Cypress.com\3.0\modules\forum\editpost.cfm:4) at coldfusion.runtime.CfJspPage.invoke(CfJspPage.java:231) at coldfusion.tagext.lang.IncludeTag.doStartTag(IncludeTag.java:416) at coldfusion.runtime.CfJspPage._emptyTcfTag(CfJspPage.java:2722) at cfforum2ecfm1574266689.runPage(\\121019-admin\s$\Cypress.com\3.0\apps\forum.cfm:119) at coldfusion.runtime.CfJspPage.invoke(CfJspPage.java:231) at coldfusion.tagext.lang.IncludeTag.doStartTag(IncludeTag.java:416) at coldfusion.runtime.CfJspPage._emptyTcfTag(CfJspPage.java:2722) at cfindex2ecfm2051812796._factor1(\\121019-admin\s$\Cypress.com\3.0\index.cfm:29) at cfindex2ecfm2051812796._factor18(\\121019-admin\s$\Cypress.com\3.0\index.cfm:10) at cfindex2ecfm2051812796.runPage(\\121019-admin\s$\Cypress.com\3.0\index.cfm:1) at coldfusion.runtime.CfJspPage.invoke(CfJspPage.java:231) at coldfusion.tagext.lang.IncludeTag.doStartTag(IncludeTag.java:416) at coldfusion.filter.CfincludeFilter.invoke(CfincludeFilter.java:65) at coldfusion.filter.ApplicationFilter.invoke(ApplicationFilter.java:348) at coldfusion.filter.RequestMonitorFilter.invoke(RequestMonitorFilter.java:48) at coldfusion.filter.MonitoringFilter.invoke(MonitoringFilter.java:40) at coldfusion.filter.PathFilter.invoke(PathFilter.java:87) at coldfusion.filter.ExceptionFilter.invoke(ExceptionFilter.java:70) at coldfusion.filter.ClientScopePersistenceFilter.invoke(ClientScopePersistenceFilter.java:28) at coldfusion.filter.BrowserFilter.invoke(BrowserFilter.java:38) at coldfusion.filter.NoCacheFilter.invoke(NoCacheFilter.java:46) at coldfusion.filter.GlobalsFilter.invoke(GlobalsFilter.java:38) at coldfusion.filter.DatasourceFilter.invoke(DatasourceFilter.java:22) at coldfusion.filter.CachingFilter.invoke(CachingFilter.java:53) at coldfusion.filter.RequestThrottleFilter.invoke(RequestThrottleFilter.java:126) at coldfusion.CfmServlet.service(CfmServlet.java:201) at coldfusion.bootstrap.BootstrapServlet.service(BootstrapServlet.java:89) at jrun.servlet.FilterChain.doFilter(FilterChain.java:86) at coldfusion.monitor.event.MonitoringServletFilter.doFilter(MonitoringServletFilter.java:42) at coldfusion.bootstrap.BootstrapFilter.doFilter(BootstrapFilter.java:46) at jrun.servlet.FilterChain.doFilter(FilterChain.java:94) at jrun.servlet.FilterChain.service(FilterChain.java:101) at jrun.servlet.ServletInvoker.invoke(ServletInvoker.java:106) at jrun.servlet.JRunInvokerChain.invokeNext(JRunInvokerChain.java:42) at jrun.servlet.JRunRequestDispatcher.invoke(JRunRequestDispatcher.java:286) at jrun.servlet.ServletEngineService.dispatch(ServletEngineService.java:543) at jrun.servlet.jrpp.JRunProxyService.invokeRunnable(JRunProxyService.java:203) at jrunx.scheduler.ThreadPool$ThreadThrottle.invokeRunnable(ThreadPool.java:428) at jrunx.scheduler.WorkerThread.run(WorkerThread.java:66) | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
TagContext |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Type | Application | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
name | destination | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
tagName | CFFILE | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
value | C:\inetpub\wwwroot\Cypress.com\files\ |
Hi,
Now, I'm using psoc creator with psoc5lp device.
My projects consist of bootloader and bootloadable.
And P1[3] of PSoC5 LP is connected to led.
Debug Select options were swd. and i could change both of them.
There was no problem before upgrade psoc creator today.
After that, debug select option in bootloadable project is changed to inherit the value from associated bootloader.
I can't find the way to inherit bootloader value in bootloadable project.
Show LessHi to all,
I'm using PSoC Creator v3.1 and I'm facing with a strange problem; when I copy a selection in the editor, the Creator seems blocking for few seconds, before I can paste...I really don't know where is the problem. Please, could anyone help me ?
Regards
Show LessHi, newbie here. I am trying to get the examples installed from Lesson 4 of the $4 PSoC board. I downloaded the installer trhough the Akamai (why?) DM. It won't install and ends up with below InstallShield error. When I click Yes, it ends up here again. FYI: I did install the whole PSoC Creator IDE without any complaints.
Any ideas for a newbie and windows 7 in virtualbox user?
Arthur
Show LessHello everyone,
how can the current measurement be done with PSOC 5? Under paragaph 8.12.2 First Order Modulator-SC Mode, there is written, that applications such as current measurement can be done.
In the case, which it is possible, what is the theoretical sensitivity? I would like to measure current arround 20A (the voltage is 800mV)
Thanks for your help
Regards
Rosine
Show LessHi,
I need to access individual bit values of ControlReg and StatusReg. For that I typically do:
Bit_0 = (StatusReg_1_Status) & 0x01;
Bit_1 = (StatusReg_1_Status >>1) & 0x01;
Bit_2 = (StatusReg_1_Status >>2) & 0x01;
....
Is there any better way to directly read/set individual bits in Status / Control registers?
regards,
odissey1
Show Less