PSoC™ Creator & Designer Forum Discussions
Hello EveryBody,
I am using PSOC 5LP Kit and i want to implement instrumentation amplifier having high CMRR and Gain. How i can do this?
Looking forward for your suggestions.
Regards
Awais
Show LessHello,
I receive the following error every time I shutdown PSOC Creator 3.2 (I've already uninstalled / reinstalled )
PSoC Creator has encountered a problem and must close. The requested operation cannot be performed on a file with a user-mapped section open.
Here is the error log:
System.IO.IOException: The requested operation cannot be performed on a file with a user-mapped section open.
at System.IO.__Error.WinIOError(Int32 errorCode, String maybeFullPath)
at System.IO.FileStream.SetLengthCore(Int64 value)
at System.IO.FileStream.SetLength(Int64 value)
at CyDesigner.Common.Base.CyLocalFileSettingsProvider.SaveToStream(XmlDocument doc, Stream stream)
at CyDesigner.Common.Base.CyLocalFileSettingsProvider.SetPropertyValues(SettingsContext context, SettingsPropertyValueCollection collection)
at System.Configuration.SettingsBase.SaveCore()
at System.Configuration.SettingsBase.Save()
at System.Configuration.ApplicationSettingsBase.Save()
at CyDesigner.Common.Base.CyApplicationSettingsBase.app_AppExit(Object sender, EventArgs e)
at System.EventHandler.Invoke(Object sender, EventArgs e)
at CyDesigner.Common.Base.CyApp.OnAppExit(EventArgs e)
at CyDesigner.Common.Base.CyApp.CheckRaiseAppExit()
at CyDesigner.Common.Base.CyApp.Application_ApplicationExit(Object sender, EventArgs e)
at System.EventHandler.Invoke(Object sender, EventArgs e)
at System.Windows.Forms.Application.RaiseExit()
at System.Windows.Forms.Application.ThreadContext.Dispose(Boolean postQuit)
at System.Windows.Forms.Application.ThreadContext.RunMessageLoopInner(Int32 reason, ApplicationContext context)
at System.Windows.Forms.Application.ThreadContext.RunMessageLoop(Int32 reason, ApplicationContext context)
at System.Windows.Forms.Application.Run(Form mainForm)
at CyDesigner.Framework.Run.Main(String[] args)
Show LessAfter initial debugging of my 8051 code, I have a "syntax error near '8'" error on line 99 of EZI2C.h. This being a PSoC Creator generated file, I don't know what could be causing this, the code looks fine above line 99. On a possible unrelated note, I #included project.h to my main file and the uintxx data types were failing to be recognized. This problem is resolved now.
I've attached my project archive bundle to this post as well. Thanks in advance for any assisstance.
Show LessHello Every Body,
I want to implement a balanced modulator/demodulator that can do the operation more closely like (AD630 "See attachment for data sheet").
If Yes, then please give me some source or reference that i can follow.
Looking forward for your suggestions.
regards
Awais
Show LessHi PSoC community,
I am a PSoC beginner and i am currently learning the ropes of PSoC and the Creator software.
I am a student and as some first steps i tried to get a sine wave out of my PSoC 3. I work with Creator 2.0 and used the ´Sine
Wave Generator with DAC´ document. The steps are well explained but I have no idea how to import or create the look up table for the values for the sine wave.
I searched the cypress page and other sources but got no idea, so now I am counting on you.
Thank you for your comments.
StudentA
Show LessHow do you access the component parameters in the component API for a custom component? I have been looking for this for about an hour now, but I can't find any documentation on it. Even the tutorial videos don't seem to talk about this.
Show LessI'm trying to create a new project in PSoC Creator, and I want to use the CTBLE-022001-00 device.
However, I don't get this device as an option when I create a new project. the only option I'm allowed to choose is the CYBL10563-56LQXI
The CYBLE-022001-00 should show up in this list of devices to select. I'm working with an application engineer, and he has the correct option on his system, but he doesn't know how I can get the option.
Does anyone know how I can update my PSoC Creator to provide the CTBLE-022001-00 option when I create a new project?
Thank you!
Show LessHello,
As a sanity check we would like to switch from 9.03 to 8.16a and try to mimic the exact production environment that we inherited code from. We downloaded 8.16a and went to Tools-->Options-->Project Management-->Generic Toolchains and set the binary path to the DP8051 of version 8.16a but the options to switch to it in Build Settings/Build Configuration does not show up. Any thoughts what we may be doing wrong? The only option is still for the newer 9.03 compiler.
Thanks,
Wess
Show LessHi All.
I am probably going to ask the stupidist question here ever.
What is the meaning of the icons next to the component in the component libary. See attached pic.
Regards
Matt
Show Less