PSoC™ Creator & Designer Forum Discussions
Hi,
Is there any specification to program efficiently in Psoc Creator using C language ? I have found it low efficient when I saw the assembly language in .lst file.
Thanks.
Show LessI'm trying to use the macro callbacks feature described in the I2C component datasheet, but the auto-generated I2C API does not include cyapicallbacks.h like the datasheet suggests that it should. I see the #ifdefs and the compiled-out callback functions in the source file, but the source file does not include the macro callbacks header file.
I'm using I2C Slave component v3.50. What am I missing??
Show LessHi.
I am trying to create multiple components with different values of D0 register using UDB editor. The value of the D0 register is set so that it can be changed by the parameter of the component.
However, when multiple components are placed in the schematic and the parameters are changed, all the components are set to the value of one of the parameters.
For example, if you set the value of component A to 100 and the value of component B to 200, the value of all components will be set to 200.
How do you set the parameters of each component to the correct values?
Show Lesswell, what looks unclear to me - if I can decide at one point, that there will be two devices with different logic, schematic, etc, but both are derivatives of what I have for a moment.
I can't just copy a project to a different directory - some paths will be broken then. I have to copypaste schematics and code. even worse when it's user library in use...
what if there is a button in the menus, which brings me my project with the name and path of choice? or a button to 'recover' brocken links in the already copied project?
Show LessI want to add a composite device(USB Audio and USB UART).
I could use a USB Audio Device, but can't add a USB UART Device.
How to add a USB UART Device. Is there a sample project file?
Show LessI see a very big difference in memory footprint for PSoC3 and PSoC5
( I changed only Project-> Device selector-> select chip )
What is the reason for this difference and whether it is possible to reduce.
I have a Creator 4.0 project written from PRoC. Now I need to change it to use the Keil MDK compiler. I found that in the old project, in the Linker option it included a "m" library in the "additional library" field. What is that and do I also need to include it in the MDK tool chain?
Thank you.
Show LessFor some reasons I need to use ADC_SAR v 2.0 in project under Creator 4.
Trying to import ADC_SAR v 2.0 from CyComponentLibrary.cywrk (v 3.3) I got error messages concerning another legacy components such as:
The instance 'theACLK', of component cy_clock_v2_0, contains an error. Unable to locate and customize component 'cy_clock_v2_0' used in schematic 'C:\Cypress\PSoC.
Till now I have to use Creator 3.3.
The question is:
How to correctly make such import procedure.
Thanks in advance,
Vladimir
Show Less