Recent discussions
Rolf Nooteboom helped develop a technique for writing and compiling firmware for PSOC5 on Linux and Macintosh (and Windows). The overall system uses the free VSCode from Microsoft, the ARM compiler from ARM itself, some of the Modus Toolbox work Cypress put into previous versions of ModusToolbox(tm).
The upside to his work is the entire project's build finishes in seconds on Mac or Linux vs. minutes natively. (The minutes is when building under Windows using Creator). I was able to take his work and stumble into modifying it for using a KitProg (as well as kitprog 2 or 3). The pattern for the project directory was also changed, making it easy to use as a template for future projects, and with FreeRTOS. (Yes, a complete FreeRTOS rebuild takes seconds on a Mac.)
I wrote several blog posts on this at socmaker.com. My guide for coding/compiling on Linux (which is built on the previous blogs) is at https://socmaker.com/?p=1119 . You have to create the schematic with PSOC Creator first. (I use a virtual machine running windows 7, 64 bit to accomplish this.) Then finish with the firmware development on your native O.S.
Previous posts at socmaker.com cover the Macintosh side. Enjoy
Show LessHello,
I have been using PSoC Creator 4.4 for some time now and have been unable to download the example code for some weeks now.
When I select Code Example from the File menu in PSoC Creator, all that appears is code that has already been downloaded.
I think this is probably the same cause of this problem. Please fix it ASAP.
Regards,
Shimamura
Show LessBLE component is missing from Communications component of PSoC Creator 4.4
Hello,
I've just downloaded the PSoC Creator 4.4 and I'm trying to build an exisiting project. However, I can't do it as PSoC Creator can't update it's components to the required versions:
My project needs cy_boot to be version 6.10, but only 6.0 is available. Also, it need cy_isr to be 1.71, but only 1.70 is available.
According to Help -> Update Manager, everything is up to date:
Here is some information about my environment, installed products etc, Help -> About:
Environment:
PSoC Creator 4.4 (4.4.0.80)
Culture: English (United States)
OS Version: Microsoft Windows NT 10.0.19043.0
CLR Version: 4.0.30319.42000
Installed CyInstaller Products:
Peripheral Driver Library 3.1.1
Peripheral Driver Library 3.1.3
Peripheral Driver Library 3.1.5
PSoC Programmer 3.29.1
PSoC Creator 4.4
Loaded Plugins:
Name: Customizer Loader
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Loads component customizers.
Name: Addin Discovery
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Discovers PSoC Creator addins (kits, language packs, etc)
Name: Device Catalog
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Device Catalog Plugin
Name: Documentation
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Adds the topics available in the documentation.
Name: Start Page
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Adds a start page to the framework.
Name: Output Window Plugin
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Adds the output window
Name: SCC Manager
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: The Source Code Control Manager is the central class used for SCC actions within PSoC Creator.
Name: Symbol, Schematic and SchMacro Factory
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: The Symbol and Schematic Factory is used to load, cache, and retrieve symbols and schematics.
Name: Project Manager Plugin
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Adds project management related functionality.
Name: GDE Plugin
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Loads the Symbol and Schematic editors
Name: Language Plugin
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Supports user files in multiple languages
Name: Workspace Factory
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: The Workspace Factory is used to retrieve instances of PSoC Creator workspaces.
Name: Project Factory
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: The Project Factory is used to retrieve instances of PSoC Creator projects.
Name: Toolchain Manager
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: PSoC Creator Toolchain Manager
Name: ARM GCC Generic
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: ARM GNU Generic
Name: ARM MDK Generic
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: ARM MDK Generic
Name: ARM IAR Generic
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: ARM IAR Generic
Name: DP8051 Keil Generic
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: DP8051 Keil Generic
Name: Device Selector
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Adds a dialog that allows the user to select a device.
Name: File Editor Factory Plugin
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Add file editors to the framework.
Name: Transport Framework
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Provides a generic device communication framework for use by other plugins.
Name: Debugger Core
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: The Core Debugger provides an architecture independent framework for the common debug features.
Name: PSoC Debugger
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Provides debugging support for the different PSoC families through a GDB back end.
Name: FM Debugger
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Provides debugging support for FM device families
Name: Device IO Transport
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Provides device IO support for Cypress devices though PSoC Programmer APIs.
Name: Serial Transport
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Provides basic serial device support for the rest of the tool.
Name: Bootloader Host
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Provides a host tool to perform bootloading operations.
Name: Background Elaborator
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: PSoC Creator Background Elaborator.
Name: TypeCache Factory
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: The TypeCache Factory is used to retrieve instances of TypeCaches.
Name: PSoC Fitter
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: PSoC Fitter Plugin
Name: FM Fitter
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: FM Fitter Plugin
Name: DWR Plugin
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Registers resource editors with devices.
Name: DMA Wizard
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Enables quick and correct development of applications that use DMA.
Name: Tuner Plugin
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: Manages custom component tuner executables
Name: Notice Window
Version: 4.4.0.80
Company: Cypress Semiconductor
Description: The Notice Window displays notices (status messages / errors with managed lifetimes).
I've already tried a lot of things to solve this problem. Probably the only thing I didn't do is to reinstall the OS 🙂
I have a feeling that PSoC Creator is not able to download these required components from some remote server(s). This guess is also supported by what I found in the PSoC Creator logs (C:\Users\<user>\AppData\Local\Temp\PSoC Creator-000.log):
Unable to download latest online manifest: The underlying connection was closed: Could not establish trust relationship for the SSL/TLS secure channel.
It should also be mentioned that this problem is observed for different computers located on different networks. That is why I think the problem is related to some server, and not to the computer.
Show LessDear Community Members,
I found a strange behaviour of nested void functions (void functions under other void functions),
I would like to ask community members : is it a feature/expected behaviour or bug ?
let me show you:
background info:
PSoC Creator 4.4 (4.4.0.80) with latest updates, CY8CKIT-059 PSoC 5LP Prototyping Kit 1.0 Rev.*A
setup: from desktop C# I communicate with PSoC firmware by USBFS sending commands to PSOC (DMA auto management) to call different functions, like :
under main for(;;)
{
// Is there any new Out transaction..
// Data parsing ...
// call correspoding function, e.g.:
Beep_VERY_Short_Nx( 3u); // 3x Beep by toggling pins of a buzzer and led
// important1: beep function takes time to run down
// important2: every line in beep function are void functions -see later
}
my Beep function:
void Beep_VERY_Short_Nx (uint32_t Nx ) // N times
{
Pin_BUZZER_Write(1u); // BUZZER default (POR) off: silent
for (uint32_t i = 0; i < Nx; i++)
{
Pin_BUZZER_Write(0u); // pull down => beep
CyDelay(25);
Pin_BUZZER_Write(1u); // pull UP => silent
CyDelay(25);
}
}
So far everything is fine, as expected, nothing special.
First case:
If I call this beep function It return immediately. I mean the function runs fine from start to end, but in line in time (the order in which events occur) is:
1.) call Beep function,
2.) Beep function returns immediately (I see it as my firmware reply to desktop program by USBFS), this is my real quation.
3.) hear the beeps as expected but after point 2, not before point 2.
(beep runs like as async / non-blocking function in PSoC 5lp)
let me emphasize: all functions in the body of beep function are voids:
as void Pin... Write(); and void CyDelay(); functions are void functions.
If I rewrite the beep function method signature to non-void and call it, like:
uint8 result = Beep_VERY_Short_Nx( 3u );
The order is:
1.) call Beep function
2.) beeps as expected
3.) Beep function return in the end of the process.
So, in this second case the code running as expected.
So, my question is: is it (immediately return of an 'all void function') a feature/expected behaviour (e.g. from compiler optimization) or bug ?
Thanks for your kind reply,
Best Regards,
Péter
Show Less
I am an end user and some years ago my developer installed PSOC on my computer so I could go into control C and adjust various parameters
My computer has died and I want to install creator back on my new laptop so that I can open the programs I have saved and edit them again
I just need a bit of direction on which version to install and get it setup, Would I just be able to use the latest version?
Show Less
Hi All,
I've been playing with Cypress products for years but I'm predominantly a Linux user. Because of this, I have recently built a new Windows machine specifically for development work. Normally I would avoid using Cypress for my designs but I think the PSoC 4 will suit my project design requirements nicely.
Has Infineon considered creating a development suite for the Linux developers out there?
Have the developers in this community had any measure of success in running PSoC creator on Ubuntu / Debian systems?
All the best,
KVN
I am using PSoC Creator 4.4, and I am unable to text search .ld files. I'm wondering if there is a setting somewhere (which I have been unable to find) that will fix this. Anybody able to text search .ld files through PSoC Creator?
The only text search settings I have been able to find are Tools/Options/Text Editor/Find and Replace and there is nothing relevant there.
Show LessCant seem to find the project archive anywhere ?
Would be grateful for a link.
Regards, Dana.
Dear Community Member,
(as I didn't find a solution here, I've written one and share it)
Please, find my attached sample code for NO polling, interrupt based Martix 4x4 keypad.
Background: most of our projects the the focus is on analog and real-time processing, so I would always feel uncomfortable if a device used in a very small time slot -like a 4x4 matrix keyboard- used up valuable CPU time.
This sample code is interrupt based (the key pad pins is only 'watching', no CPU time needed at this stage).
The user key press event give a trigger for this watching state to CPU start working.
Very simple logic behind of that:
1.)
-matrix keypad COLUMN (input digital) pins setted to HIGH,
-matrix keypad ROW (input digital) pins setted to resistive pull-down mode, pluss a rising edge interrupt service routine attached to row pins.
This is the watcher / idle state.
2.) if any key pressed, the rising edge interrupt service routine TRIGGERED by row pins.
3.) After an adjustable debouncing periode the columns and correcponding row pins are scanned: the pushed key found.
Tested with the following 4x4 matrix membran keypad:
https://www.hestore.hu/prod_10041773.html
with CyKit-059.
All the other other information: see main.c comments
(how to use math library and special SWD pins)
Thanks for the feedback,
Have nice day,
Péter
Show Less