- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Why do I get this message when I try to do a DMA Wizard on DMA_1 ? The build file is attached. Where should I actually paste these lines? I have tried various places and they get optimized out of existence when I do a Clean and Build.
I am trying to use the sequencing SAR to put analog data into the FIR filter where I will do a time-align on the two input channels. A secondary question is: how do I be sure that the next ADC starts with ADC_SAR input 0? I have to keep them time aligned. But this is a secondary question. Go back up to the first paragraph for my primary question. Why do I get the message below from the DMA Wizard and what do I do with it? My Workspace bundle is attached.
/* Variable declarations for DMA_1 */
/* Move these variable declarations to the top of the function */
uint8 DMA_1_Chan;
uint8 DMA_1_TD[2];
/* DMA Configuration for DMA_1 */
#define DMA_1_BYTES_PER_BURST 2
#define DMA_1_REQUEST_PER_BURST 1
#define DMA_1_SRC_BASE (CYDEV_PERIPH_BASE)
#define DMA_1_DST_BASE (CYDEV_PERIPH_BASE)
DMA_1_Chan = DMA_1_DmaInitialize(DMA_1_BYTES_PER_BURST, DMA_1_REQUEST_PER_BURST,
HI16(DMA_1_SRC_BASE), HI16(DMA_1_DST_BASE));
DMA_1_TD[0] = CyDmaTdAllocate();
DMA_1_TD[1] = CyDmaTdAllocate();
CyDmaTdSetConfiguration(DMA_1_TD[0], 2, DMA_1_TD[1], DMA_1__TD_TERMOUT_EN | TD_INC_DST_ADR | TD_AUTO_EXEC_NEXT);
CyDmaTdSetConfiguration(DMA_1_TD[1], 2, DMA_1_TD[0], DMA_1__TD_TERMOUT_EN | TD_INC_DST_ADR);
CyDmaTdSetAddress(DMA_1_TD[0], LO16((uint32)ADC_SAR_Seq_SAR_SAR_WRK0_PTR), LO16((uint32)Filter_STAGEA_PTR));
CyDmaTdSetAddress(DMA_1_TD[1], LO16((uint32)ADC_SAR_Seq_SAR_SAR_WRK0_PTR), LO16((uint32)Filter_STAGEB_PTR));
CyDmaChSetInitialTd(DMA_1_Chan, DMA_1_TD[0]);
CyDmaChEnable(DMA_1_Chan, 1);
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Its setup code, with globals, or you can use it in a startup function.
http://www.cypress.com/?rID=37793 AN52705 Getting Started with DMA
http://www.cypress.com/?rID=82680 AN84810 PSoC® 3 and PSoC 5LP Advanced DMA Topics
http://www.cypress.com/?rID=44335 AN61102 PSoC® 3 and PSoC 5LP - ADC Data Buffering Using DMA
http://video.cypress.com/video-library/search/dma/ Videos on DMA
https://www.youtube.com/results?search_query=dma+psoc Videos on DMA (some overlap)
From AN52705