Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer Forum Discussions

JeCo_264681
Level 5
Level 5
100 replies posted 50 replies posted 25 replies posted

Why do I get this message when I try to do a DMA Wizard on DMA_1 ? The build file is attached. Where should I actually paste these lines?  I have tried various places and they get optimized out of existence when I do a Clean and Build.

   

I am trying to use the sequencing SAR to put analog data into the FIR filter where I will do a time-align on the two input channels. A secondary question is: how do I be sure that the next ADC starts with ADC_SAR input 0?  I have to keep them time aligned.  But this is a secondary question. Go back up to the first paragraph for my primary question. Why do I get the message below from the DMA Wizard and what do I do with it?  My Workspace bundle is attached.

   

/* Variable declarations for DMA_1 */

   

/* Move these variable declarations to the top of the function */

   

uint8 DMA_1_Chan;

   

uint8 DMA_1_TD[2];

   

 

   

/* DMA Configuration for DMA_1 */

   

#define DMA_1_BYTES_PER_BURST 2

   

#define DMA_1_REQUEST_PER_BURST 1

   

#define DMA_1_SRC_BASE (CYDEV_PERIPH_BASE)

   

#define DMA_1_DST_BASE (CYDEV_PERIPH_BASE)

   

DMA_1_Chan = DMA_1_DmaInitialize(DMA_1_BYTES_PER_BURST, DMA_1_REQUEST_PER_BURST, 

   

    HI16(DMA_1_SRC_BASE), HI16(DMA_1_DST_BASE));

   

DMA_1_TD[0] = CyDmaTdAllocate();

   

DMA_1_TD[1] = CyDmaTdAllocate();

   

CyDmaTdSetConfiguration(DMA_1_TD[0], 2, DMA_1_TD[1], DMA_1__TD_TERMOUT_EN | TD_INC_DST_ADR | TD_AUTO_EXEC_NEXT);

   

CyDmaTdSetConfiguration(DMA_1_TD[1], 2, DMA_1_TD[0], DMA_1__TD_TERMOUT_EN | TD_INC_DST_ADR);

   

CyDmaTdSetAddress(DMA_1_TD[0], LO16((uint32)ADC_SAR_Seq_SAR_SAR_WRK0_PTR), LO16((uint32)Filter_STAGEA_PTR));

   

CyDmaTdSetAddress(DMA_1_TD[1], LO16((uint32)ADC_SAR_Seq_SAR_SAR_WRK0_PTR), LO16((uint32)Filter_STAGEB_PTR));

   

CyDmaChSetInitialTd(DMA_1_Chan, DMA_1_TD[0]);

   

CyDmaChEnable(DMA_1_Chan, 1);

   
        
0 Likes
1 Solution
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Its setup code, with globals, or you can use it in a startup function.

   

 

   

    

   

          

   

http://www.cypress.com/?rID=37793     AN52705     Getting Started with DMA

   

http://www.cypress.com/?rID=82680     AN84810     PSoC® 3 and PSoC 5LP Advanced DMA Topics

   

http://www.cypress.com/?rID=44335     AN61102 PSoC® 3 and PSoC 5LP - ADC Data Buffering Using DMA

   

http://video.cypress.com/video-library/search/dma/     Videos on DMA

   

https://www.youtube.com/results?search_query=dma+psoc Videos on DMA (some overlap)

   

 

   

 

   

From AN52705

View solution in original post

0 Likes
4 Replies
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Its setup code, with globals, or you can use it in a startup function.

   

 

   

    

   

          

   

http://www.cypress.com/?rID=37793     AN52705     Getting Started with DMA

   

http://www.cypress.com/?rID=82680     AN84810     PSoC® 3 and PSoC 5LP Advanced DMA Topics

   

http://www.cypress.com/?rID=44335     AN61102 PSoC® 3 and PSoC 5LP - ADC Data Buffering Using DMA

   

http://video.cypress.com/video-library/search/dma/     Videos on DMA

   

https://www.youtube.com/results?search_query=dma+psoc Videos on DMA (some overlap)

   

 

   

 

   

From AN52705

0 Likes
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

The below image did not paste in last post. See attached.

   

 

   

Note your mic interface should eliminate coupling cap, that will

   

allow bias source to bias up the PGA into ~ center of CM range.

   

2.5 V would have nailed it.

JeCo_264681
Level 5
Level 5
100 replies posted 50 replies posted 25 replies posted

 Ah, yes, danaknight. I found the answer there in AN52705 on page 7 and Appendix A.  I paste the wizard code into main.c. Page 7 explains that the wizard does not support all peripherals so we have to do some editing to define the parameters. Thanks.

0 Likes
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Glad to have been of assistance.

   

 

   

Regards, Dana.

0 Likes