Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
loop_y0u
Level 4
Level 4
25 replies posted 50 sign-ins 10 questions asked

Hi Community, Im working on Touch switch Application based on CY8C4246LTI-M445. I have previously used CY8C4245-AXI and in its Capsense Component I was able to tune every single button's "Finger Threshold, Noise Threshold and so on", But with this one or Project, Im not able to Tune every single button. 

I'll be attaching screenshot regarding this.

Additionally I have seen two different CapSense Components. 

1. CapSense[v7.10]

2. CapSense CSD[v2.60]

 

If I drag 1st Component, It won't allow me to Set Finger Threshold for Each Button. It sets the value of Fing. Thre. Default to every button.

 

If I drag 2nd Component, It will allow me to select Finger Threshold to each button

 

Assistance is required for this. I hope the issue which I've posted is simple to understand. Let me know if you have some quries. 

 

Thanks and Regards,

Pankaj

0 Likes
1 Solution
PandaS
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 5 likes given

Hi @loop_y0u ,

Please confirm the settings of the Basic Tab in CapSense Component v7.10.

1. Is it One Button Widget with Multiple Sensing Elements :

PandaS_0-1695205200200.png

2. Or is it Two or More Separate Button widgets:

PandaS_1-1695205496628.png

Hardware and Software Parameters configuration is common to a widget and its sensing elements. You should have separate widgets for setting different tuning parameters in your case.

I would suggest using CapSense v7.1 over CapSensev2.6 component. Create separate button widgets and you should be able to set the tuning parameters for each widget separately.

I hope this answers your query, let us know if this helps.

 

Thanks and regards,

Sobhit

View solution in original post

3 Replies
PandaS
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 5 likes given

Hi @loop_y0u ,

Please confirm the settings of the Basic Tab in CapSense Component v7.10.

1. Is it One Button Widget with Multiple Sensing Elements :

PandaS_0-1695205200200.png

2. Or is it Two or More Separate Button widgets:

PandaS_1-1695205496628.png

Hardware and Software Parameters configuration is common to a widget and its sensing elements. You should have separate widgets for setting different tuning parameters in your case.

I would suggest using CapSense v7.1 over CapSensev2.6 component. Create separate button widgets and you should be able to set the tuning parameters for each widget separately.

I hope this answers your query, let us know if this helps.

 

Thanks and regards,

Sobhit

Hi @PandaS ,

 

Thank You, I'm happy that my issue got resolved within a day. Love your helping hands.

 

Thanks and Regards,

Pankaj Singh

 

0 Likes
PandaS
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 5 likes given

Hi @icstock ,

I did not get you. Could you please elaborate.

Thankyou

0 Likes