- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have a custom board with PSoC5 using USBUART. In the past, I got this board version working and enumerating just fine. Today, I pulled out a second board made at the same time as the first one. I programmed the PSoC5. I inserted the USB plug into my PC, and things aren't behaving.
Specifically, in Device Manager I see the board identified as "Unknown Device". I tried to update the driver, providing my ...Generated_Source\PSoC5 folder name. Windows told me the driver was up-to-date. Nevertheless, it's not installed properly. The driver is from Microsoft, date 6/21/2006, version 6.1.7601.18328.
Meanwhile, I still have the original board that works. I plug its USB cable into my PC and it comes up just fine as COM9 in the Device Manager. It says it's using a driver from Cypress, date 3/5/2007, version 2.0.0.0.
What step did I forget? How do I force windows to use the Cypress driver?
I'm using Win7 SP1, 64-bit, 32GB ram, Intel I7-2600 3.4GHz