- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Attaching the host UART PC application which is designed in VC++ with this post.
AN68272 (PSoC 3, PSoC 4 and PSoC 5LP UART Bootloader) available at link http://www.cypress.com/?rID=50230 has an application designed in VC#. This application cannot be used with Windows CE.
I am attaching the same application designed in VC++ which you can compile with Windows CE compiler to make it work. Currenlty, this application is working on Windows XP, Vista, 7 and 8. Source code of application is allso attached with this post.
Regards,
--Rave
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
thank you was looking for.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
najac,
Hi. I've tried compiling your C++ project in VS 2019. No luck.
Here are the errors I receive:
1>------ Build started: Project: UARTBootloaderHost, Configuration: Debug x64 ------
1>AssemblyInfo.cpp
1>C:\Users\lpoma\Desktop\UART Bootlaoder\Source code in VC++\UARTBootloaderHost\UARTBootloaderHost\AssemblyInfo.cpp(40,29): warning C4947: 'System::Security::Permissions::SecurityAction::RequestMinimum': marked as obsolete
1>C:\Users\lpoma\Desktop\UART Bootlaoder\Source code in VC++\UARTBootloaderHost\UARTBootloaderHost\AssemblyInfo.cpp(40,29): message : Message: 'Assembly level declarative security is obsolete and is no longer enforced by the CLR by default. See http://go.microsoft.com/fwlink/?LinkID=155570 for more information.'
1>stdafx.cpp
1>UARTBootloaderHost.cpp
1>C:\Users\lpoma\Desktop\UART Bootlaoder\Source code in VC++\UARTBootloaderHost\UARTBootloaderHost\BootloadFunctions.h(84): warning C4091: 'static ': ignored on left of 'Bootload_Functions::Bootload_Utils::CyBtldr_CommunicationsData' when no variable is declared
1>C:\Users\lpoma\Desktop\UART Bootlaoder\Source code in VC++\UARTBootloaderHost\UARTBootloaderHost\Form1.h(332,23): warning C4101: 'Ex': unreferenced local variable
1>C:\Users\lpoma\Desktop\UART Bootlaoder\Source code in VC++\UARTBootloaderHost\UARTBootloaderHost\Form1.h(341,23): warning C4101: 'Exc': unreferenced local variable
1>C:\Users\lpoma\Desktop\UART Bootlaoder\Source code in VC++\UARTBootloaderHost\UARTBootloaderHost\Form1.h(379,1): warning C4817: 'System::Array::Length': illegal use of '.' to access this member; compiler replaced with '->'
1>C:\Users\lpoma\Desktop\UART Bootlaoder\Source code in VC++\UARTBootloaderHost\UARTBootloaderHost\Form1.h(498,35): warning C4101: 'ex': unreferenced local variable
1>C:\Users\lpoma\Desktop\UART Bootlaoder\Source code in VC++\UARTBootloaderHost\UARTBootloaderHost\Form1.h(505): warning C4700: uninitialized local variable 'status' used
1>.NETFramework,Version=v4.0.AssemblyAttributes.cpp
1>LINK : fatal error LNK1104: cannot open file 'C:\Users\namn\Documents\Visual Studio 2010\Projects\BootLoad_Utils_dll\Debug\BootLoad_Utils.lib'
1>C:\Program Files (x86)\Microsoft Visual Studio\2019\Community\MSBuild\Microsoft\VC\v160\Microsoft.CppCommon.targets(847,5): error MSB6006: "link.exe" exited with code 1104.
1>Done building project "UARTBootloaderHost.vcxproj" -- FAILED.
========== Build: 0 succeeded, 1 failed, 0 up-to-date, 0 skipped ==========
In effect, it aborts the build due to not finding the file 'C:\Users\namn\Documents\Visual Studio 2010\Projects\BootLoad_Utils_dll\Debug\BootLoad_Utils.lib'
Len
"Engineering is an Art. The Art of Compromise."