Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

NiNa_4043086
Level 3
Level 3
First like received

Hello,

I am using PSOC creator for PSOC 5LP and I need to connect analog inputs to two components but I am getting errors from the compiler.

How do I overcome this?

1 Solution

Errormessage says that this combination is not possible. Use two analog input pins and connect them externally.

Bob

View solution in original post

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Can you please post your complete project so that we all can have a look at all of your settings. To do so, use

Creator->File->Create Workspace Bundle (minimal)

and attach the resulting file.

Bob

0 Likes

I will give more details. I am trying to connect analog input to two components at the same time: scanning comparator mux input and power monitor voltage input.

The compiler gives the following error: "AmuxHW only supports controlled analog connections to GPIOs. Please make sure all the controlled analog connections are connected to GPIOs."

0 Likes

Errormessage says that this combination is not possible. Use two analog input pins and connect them externally.

Bob

0 Likes