Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer

Anonymous
Not applicable

 Testing SPI on Psoc 5LP, and need to monitor pin values during debugging. The variables are "out of scope". Please advice the best way to monitor pin values during debugging.

0 Likes
5 Replies
ETRO_SSN583
Level 9
5 likes given 1000 replies posted 750 replies posted
Level 9

A simple way would be to assign the port value to a variable

   

and monitor the variable via a register read of port at the point of interest

   

in the code. Or temporarily use simple LCD to display port register. You would

   

insert at key points a register read of the port.

   

 

   

Port register naming can be found in the cypins.h

   

 

   

Regards, Dana.

0 Likes
ETRO_SSN583
Level 9
5 likes given 1000 replies posted 750 replies posted
Level 9

If you need to monitor SPI pins during SPI activity a logic analyzer

   

would be needed. Here is a cheap one that I have used and works

   

pretty good with decoding for serial protocols -

   

 

   

    

   

          

   

http://www.ebay.com/itm/Logic-Analyzer-24MHz-8CH-USB-Logic-Analyzer-/121300301611?pt=LH_DefaultDomai...

   

 https://www.saleae.com/ Software

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

So i looked in cypins.h *before* posting, and did not find. What is the address/name of P[0].6 pin 78.

   

Please show me where in cypins.h i find this info. I have attached the file below

   

-----------

   

/*******************************************************************************

   

* File Name: cypins.h

   

* Version 4.10

   

*

   

*  Description:

   

*   This file contains the function prototypes and constants used for a port/pin

   

*   in access and control.

   

*

   

*  Note:

   

*   Documentation of the API's in this file is located in the

   

*   System Reference Guide provided with PSoC Creator.

   

*

   

********************************************************************************

   

* Copyright 2008-2014, Cypress Semiconductor Corporation.  All rights reserved.

   

* You may use this file only in accordance with the license, terms, conditions,

   

* disclaimers, and limitations in the end user license agreement accompanying

   

* the software package with which this file was provided.

   

*******************************************************************************/

   

 

   

#if !defined(CY_BOOT_CYPINS_H)

   

#define CY_BOOT_CYPINS_H

   

 

   

#include "cyfitter.h"

   

#include "cytypes.h"

   

 

   

 

   

/**************************************

   

*        API Parameter Constants

   

**************************************/

   

 

   

#define CY_PINS_PC_DRIVE_MODE_SHIFT (0x01u)

   

#define CY_PINS_PC_DRIVE_MODE_MASK  ((uint8)(0x07u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

#define CY_PINS_PC_DRIVE_MODE_0     ((uint8)(0x00u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

#define CY_PINS_PC_DRIVE_MODE_1     ((uint8)(0x01u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

#define CY_PINS_PC_DRIVE_MODE_2     ((uint8)(0x02u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

#define CY_PINS_PC_DRIVE_MODE_3     ((uint8)(0x03u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

#define CY_PINS_PC_DRIVE_MODE_4     ((uint8)(0x04u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

#define CY_PINS_PC_DRIVE_MODE_5     ((uint8)(0x05u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

#define CY_PINS_PC_DRIVE_MODE_6     ((uint8)(0x06u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

#define CY_PINS_PC_DRIVE_MODE_7     ((uint8)(0x07u << CY_PINS_PC_DRIVE_MODE_SHIFT))

   

 

   

 

   

/*  SetPinDriveMode */

   

#define CY_PINS_DM_ALG_HIZ          (CY_PINS_PC_DRIVE_MODE_0)

   

#define CY_PINS_DM_DIG_HIZ          (CY_PINS_PC_DRIVE_MODE_1)

   

#define CY_PINS_DM_RES_UP           (CY_PINS_PC_DRIVE_MODE_2)

   

#define CY_PINS_DM_RES_DWN          (CY_PINS_PC_DRIVE_MODE_3)

   

#define CY_PINS_DM_OD_LO            (CY_PINS_PC_DRIVE_MODE_4)

   

#define CY_PINS_DM_OD_HI            (CY_PINS_PC_DRIVE_MODE_5)

   

#define CY_PINS_DM_STRONG           (CY_PINS_PC_DRIVE_MODE_6)

   

#define CY_PINS_DM_RES_UPDWN        (CY_PINS_PC_DRIVE_MODE_7)

   

 

   

 

   

/**************************************

   

*       Register Constants

   

**************************************/

   

 

   

/* Port Pin Configuration Register */

   

#define CY_PINS_PC_DATAOUT          (0x01u)

   

#define CY_PINS_PC_PIN_FASTSLEW     (0xBFu)

   

#define CY_PINS_PC_PIN_SLOWSLEW     (0x40u)

   

#define CY_PINS_PC_PIN_STATE        (0x10u)

   

#define CY_PINS_PC_BIDIR_EN         (0x20u)

   

#define CY_PINS_PC_SLEW             (0x40u)

   

#define CY_PINS_PC_BYPASS           (0x80u)

   

 

   

 

   

/**************************************

   

*       Pin API Macros

   

**************************************/

   

 

   

/*******************************************************************************

   

* Macro Name: CyPins_ReadPin

   

********************************************************************************

   

*

   

* Summary:

   

*  Reads the current value on the pin (pin state, PS).

   

*

   

* Parameters:

   

*   pinPC: Port pin configuration register (uint16).

   

*   #defines for each pin on a chip are provided in the cydevice_trm.h file

   

*   in the form:

   

*       CYREG_PRTx_PCy

   

*

   

*   where x is a port number 0 - 15 and y is a pin number 0 - 7

   

*

   

* Return:

   

*   Pin state

   

*    0: Logic low value

   

*    Non-0: Logic high value

   

*

   

*******************************************************************************/

   

#define CyPins_ReadPin(pinPC)    ( *(reg8 *)(pinPC) & CY_PINS_PC_PIN_STATE )

   

 

   

 

   

/*******************************************************************************

   

* Macro Name: CyPins_SetPin

   

********************************************************************************

   

*

   

* Summary:

   

*  Set the output value for the pin (data register, DR) to a logic high.

   

*

   

*  Note that this only has an effect for pins configured as software pins that

   

*  are not driven by hardware.

   

*

   

* Parameters:

   

*   pinPC: Port pin configuration register (uint16).

   

*   #defines for each pin on a chip are provided in the cydevice_trm.h file

   

*   in the form:

   

*       CYREG_PRTx_PCy

   

*

   

*   where x is a port number 0 - 15 and y is a pin number 0 - 7

   

*

   

* Return:

   

*   None

   

*

   

*******************************************************************************/

   

#define CyPins_SetPin(pinPC)     ( *(reg8 *)(pinPC) |= CY_PINS_PC_DATAOUT)

   

 

   

 

   

/*******************************************************************************

   

* Macro Name: CyPins_ClearPin

   

********************************************************************************

   

*

   

* Summary:

   

*  This macro sets the state of the specified pin to 0

   

*

   

* Parameters:

   

*   pinPC: address of a Pin Configuration register.

   

*   #defines for each pin on a chip are provided in the cydevice_trm.h file

   

*   in the form:

   

*       CYREG_PRTx_PCy

   

*

   

*   where x is a port number 0 - 15 and y is a pin number 0 - 7

   

*

   

* Return:

   

*   None

   

*

   

*******************************************************************************/

   

#define CyPins_ClearPin(pinPC)   ( *(reg8 *)(pinPC) &= ((uint8)(~CY_PINS_PC_DATAOUT)))

   

 

   

 

   

/*******************************************************************************

   

* Macro Name: CyPins_SetPinDriveMode

   

********************************************************************************

   

*

   

* Summary:

   

*  Sets the drive mode for the pin (DM).

   

*

   

* Parameters:

   

*   pinPC: Port pin configuration register (uint16)

   

*   #defines for each pin on a chip are provided in the cydevice_trm.h file

   

*   in the form:

   

*       CYREG_PRTx_PCy

   

*

   

*   where x is a port number 0 - 15 and y is a pin number 0 - 7

   

*

   

*   mode: Desired drive mode

   

*

   

*   Define                Source

   

*   PIN_DM_ALG_HIZ        Analog HiZ

   

*   PIN_DM_DIG_HIZ        Digital HiZ

   

*   PIN_DM_RES_UP        Resistive pull up

   

*   PIN_DM_RES_DWN        Resistive pull down

   

*   PIN_DM_OD_LO        Open drain - drive low

   

*   PIN_DM_OD_HI        Open drain - drive high

   

*   PIN_DM_STRONG        Strong CMOS Output

   

*   PIN_DM_RES_UPDWN    Resistive pull up/down

   

*

   

* Return:

   

*   None

   

*

   

*******************************************************************************/

   

#define CyPins_SetPinDriveMode(pinPC, mode) \

   

            ( *(reg8 *)(pinPC) = (*(reg8 *)(pinPC) & ((uint8)(~CY_PINS_PC_DRIVE_MODE_MASK))) | \

   

            ((mode) & CY_PINS_PC_DRIVE_MODE_MASK))

   

 

   

 

   

/*******************************************************************************

   

* Macro Name: CyPins_ReadPinDriveMode

   

********************************************************************************

   

*

   

* Summary:

   

*  Reads the drive mode for the pin (DM).

   

*

   

* Parameters:

   

*   pinPC: Port pin configuration register (uint16)

   

*   #defines for each pin on a chip are provided in the cydevice_trm.h file

   

*   in the form:

   

*       CYREG_PRTx_PCy

   

*

   

*   where x is a port number 0 - 15 and y is a pin number 0 - 7

   

*

   

*

   

* Return:

   

*   mode:  The current drive mode for the pin

   

*

   

*   Define                Source

   

*   PIN_DM_ALG_HIZ        Analog HiZ

   

*   PIN_DM_DIG_HIZ        Digital HiZ

   

*   PIN_DM_RES_UP        Resistive pull up

   

*   PIN_DM_RES_DWN        Resistive pull down

   

*   PIN_DM_OD_LO        Open drain - drive low

   

*   PIN_DM_OD_HI        Open drain - drive high

   

*   PIN_DM_STRONG        Strong CMOS Output

   

*   PIN_DM_RES_UPDWN    Resistive pull up/down

   

*

   

*******************************************************************************/

   

#define CyPins_ReadPinDriveMode(pinPC)      (*(reg8 *)(pinPC) & CY_PINS_PC_DRIVE_MODE_MASK)

   

 

   

 

   

/*******************************************************************************

   

* Macro Name: CyPins_FastSlew

   

********************************************************************************

   

*

   

* Summary:

   

*  Set the slew rate for the pin to fast the edge rate.

   

*  Note that this only applies for pins in strong output drive modes,

   

*  not to resistive drive modes.

   

*

   

* Parameters:

   

*   pinPC: address of a Pin Configuration register.

   

*   #defines for each pin on a chip are provided in the cydevice_trm.h file

   

*   in the form:

   

*       CYREG_PRTx_PCy

   

*

   

*   where x is a port number 0 - 15 and y is a pin number 0 - 7

   

*

   

*

   

* Return:

   

*   None

   

*

   

*******************************************************************************/

   

#define CyPins_FastSlew(pinPC)      (*(reg8 *)(pinPC) = (*(reg8 *)(pinPC) & CY_PINS_PC_PIN_FASTSLEW))

   

 

   

 

   

/*******************************************************************************

   

* Macro Name: CyPins_SlowSlew

   

********************************************************************************

   

*

   

* Summary:

   

*  Set the slew rate for the pin to slow the edge rate.

   

*  Note that this only applies for pins in strong output drive modes,

   

*  not to resistive drive modes.

   

*

   

* Parameters:

   

*   pinPC: address of a Pin Configuration register.

   

*   #defines for each pin on a chip are provided in the cydevice_trm.h file

   

*   in the form:

   

*       CYREG_PRTx_PCy

   

*

   

*   where x is a port number 0 - 15 and y is a pin number 0 - 7

   

*

   

* Return:

   

*   None

   

*

   

*******************************************************************************/

   

#define CyPins_SlowSlew(pinPC)      (*(reg8 *)(pinPC) = (*(reg8 *)(pinPC) | CY_PINS_PC_PIN_SLOWSLEW))

   

 

   

 

   

/*******************************************************************************

   

* The following code is OBSOLETE and must not be used.

   

*

   

* If the obsoleted macro definitions intended for use in the application use the

   

* following scheme, redefine your own versions of these definitions:

   

*    #ifdef <OBSOLETED_DEFINE>

   

*        #undef  <OBSOLETED_DEFINE>

   

*        #define <OBSOLETED_DEFINE>      (<New Value>)

   

*    #endif

   

*

   

* Note: Redefine obsoleted macro definitions with caution. They might still be

   

*       used in the application and their modification might lead to unexpected

   

*       consequences.

   

*******************************************************************************/

   

#define PC_DRIVE_MODE_SHIFT (CY_PINS_PC_DRIVE_MODE_SHIFT)

   

#define PC_DRIVE_MODE_MASK  (CY_PINS_PC_DRIVE_MODE_MASK)

   

#define PC_DRIVE_MODE_0     (CY_PINS_PC_DRIVE_MODE_0)

   

#define PC_DRIVE_MODE_1     (CY_PINS_PC_DRIVE_MODE_1)

   

#define PC_DRIVE_MODE_2     (CY_PINS_PC_DRIVE_MODE_2)

   

#define PC_DRIVE_MODE_3     (CY_PINS_PC_DRIVE_MODE_3)

   

#define PC_DRIVE_MODE_4     (CY_PINS_PC_DRIVE_MODE_4)

   

#define PC_DRIVE_MODE_5     (CY_PINS_PC_DRIVE_MODE_5)

   

#define PC_DRIVE_MODE_6     (CY_PINS_PC_DRIVE_MODE_6)

   

#define PC_DRIVE_MODE_7     (CY_PINS_PC_DRIVE_MODE_7)

   

 

   

#define PIN_DM_ALG_HIZ      (CY_PINS_DM_ALG_HIZ)

   

#define PIN_DM_DIG_HIZ      (CY_PINS_DM_DIG_HIZ)

   

#define PIN_DM_RES_UP       (CY_PINS_DM_RES_UP)

   

#define PIN_DM_RES_DWN      (CY_PINS_DM_RES_DWN)

   

#define PIN_DM_OD_LO        (CY_PINS_DM_OD_LO)

   

#define PIN_DM_OD_HI        (CY_PINS_DM_OD_HI)

   

#define PIN_DM_STRONG       (CY_PINS_DM_STRONG)

   

#define PIN_DM_RES_UPDWN    (CY_PINS_DM_RES_UPDWN)

   

 

   

#define PC_DATAOUT          (CY_PINS_PC_DATAOUT)

   

#define PC_PIN_FASTSLEW     (CY_PINS_PC_PIN_FASTSLEW)

   

#define PC_PIN_SLOWSLEW     (CY_PINS_PC_PIN_SLOWSLEW)

   

#define PC_PIN_STATE        (CY_PINS_PC_PIN_STATE)

   

#define PC_BIDIR_EN         (CY_PINS_PC_BIDIR_EN)

   

#define PC_SLEW             (CY_PINS_PC_SLEW)

   

#define PC_BYPASS           (CY_PINS_PC_BYPASS)

   

 

   

#endif /* (CY_BOOT_CYPINS_H) */

   

 

   

 

   

/* [] END OF FILE */

   
        
0 Likes
ETRO_SSN583
Level 9
5 likes given 1000 replies posted 750 replies posted
Level 9

My cypins.h file, a portion, the DR register is the Data Register for the port.

   

 

   

/**************************************
*        Compatibility Macros
**************************************/

#if(CY_PSOC4A)
    #define CYREG_GPIO_PRT0_DR                (CYREG_PRT0_DR)
    #define CYREG_GPIO_PRT0_PS                (CYREG_PRT0_PS)
    #define CYREG_GPIO_PRT0_PC                (CYREG_PRT0_PC)

    #define CYREG_GPIO_PRT1_DR                (CYREG_PRT1_DR)
    #define CYREG_GPIO_PRT1_PS                (CYREG_PRT1_PS)
    #define CYREG_GPIO_PRT1_PC                (CYREG_PRT1_PC)

    #define CYREG_GPIO_PRT2_DR                (CYREG_PRT2_DR)
    #define CYREG_GPIO_PRT2_PS                (CYREG_PRT2_PS)
    #define CYREG_GPIO_PRT2_PC                (CYREG_PRT2_PC)

    #define CYREG_GPIO_PRT3_DR                (CYREG_PRT3_DR)
    #define CYREG_GPIO_PRT3_PS                (CYREG_PRT3_PS)
    #define CYREG_GPIO_PRT3_PC                (CYREG_PRT3_PC)

    #define CYREG_GPIO_PRT4_DR                (CYREG_PRT4_DR)
    #define CYREG_GPIO_PRT4_PS                (CYREG_PRT4_PS)
    #define CYREG_GPIO_PRT4_PC                (CYREG_PRT4_PC)
#else
    #define CYREG_PRT0_DR                     (CYREG_GPIO_PRT0_DR)
    #define CYREG_PRT0_PS                     (CYREG_GPIO_PRT0_PS)
    #define CYREG_PRT0_PC                     (CYREG_GPIO_PRT0_PC)

    #define CYREG_PRT1_DR                     (CYREG_GPIO_PRT1_DR)
    #define CYREG_PRT1_PS                     (CYREG_GPIO_PRT1_PS)
    #define CYREG_PRT1_PC                     (CYREG_GPIO_PRT1_PC)

    #define CYREG_PRT2_DR                     (CYREG_GPIO_PRT2_DR)
    #define CYREG_PRT2_PS                     (CYREG_GPIO_PRT2_PS)
    #define CYREG_PRT2_PC                     (CYREG_GPIO_PRT2_PC)

    #define CYREG_PRT3_DR                     (CYREG_GPIO_PRT3_DR)
    #define CYREG_PRT3_PS                     (CYREG_GPIO_PRT3_PS)
    #define CYREG_PRT3_PC                     (CYREG_GPIO_PRT3_PC)

    #define CYREG_PRT4_DR                     (CYREG_GPIO_PRT4_DR)
    #define CYREG_PRT4_PS                     (CYREG_GPIO_PRT4_PS)
    #define CYREG_PRT4_PC                     (CYREG_GPIO_PRT4_PC)

    #define CYREG_PRT5_DR                     (CYREG_GPIO_PRT5_DR)
    #define CYREG_PRT5_PS                     (CYREG_GPIO_PRT5_PS)
    #define CYREG_PRT5_PC                     (CYREG_GPIO_PRT5_PC)

    #define CYREG_PRT6_DR                     (CYREG_GPIO_PRT6_DR)
    #define CYREG_PRT6_PS                     (CYREG_GPIO_PRT6_PS)
    #define CYREG_PRT6_PC                     (CYREG_GPIO_PRT6_PC)

    #define CYREG_PRT7_DR                     (CYREG_GPIO_PRT7_DR)
    #define CYREG_PRT7_PS                     (CYREG_GPIO_PRT7_PS)
    #define CYREG_PRT7_PC                     (CYREG_GPIO_PRT7_PC)

    #define CYREG_PRT8_DR                     (CYREG_GPIO_PRT8_DR)
    #define CYREG_PRT8_PS                     (CYREG_GPIO_PRT8_PS)
    #define CYREG_PRT8_PC                     (CYREG_GPIO_PRT8_PC)

    #define CYREG_PRT9_DR                     (CYREG_GPIO_PRT9_DR)
    #define CYREG_PRT9_PS                     (CYREG_GPIO_PRT9_PS)
    #define CYREG_PRT9_PC                     (CYREG_GPIO_PRT9_PC)

    #define CYREG_PRT10_DR                    (CYREG_GPIO_PRT10_DR)
    #define CYREG_PRT10_PS                    (CYREG_GPIO_PRT10_PS)
    #define CYREG_PRT10_PC                    (CYREG_GPIO_PRT10_PC)

    #define CYREG_PRT11_DR                    (CYREG_GPIO_PRT11_DR)
    #define CYREG_PRT11_PS                    (CYREG_GPIO_PRT11_PS)
    #define CYREG_PRT11_PC                    (CYREG_GPIO_PRT11_PC)

    #define CYREG_PRT12_DR                    (CYREG_GPIO_PRT12_DR)
    #define CYREG_PRT12_PS                    (CYREG_GPIO_PRT12_PS)
    #define CYREG_PRT12_PC                    (CYREG_GPIO_PRT12_PC)

    #define CYREG_PRT13_DR                    (CYREG_GPIO_PRT13_DR)
    #define CYREG_PRT13_PS                    (CYREG_GPIO_PRT13_PS)
    #define CYREG_PRT13_PC                    (CYREG_GPIO_PRT13_PC)

    #define CYREG_PRT14_DR                    (CYREG_GPIO_PRT14_DR)
    #define CYREG_PRT14_PS                    (CYREG_GPIO_PRT14_PS)
    #define CYREG_PRT14_PC                    (CYREG_GPIO_PRT14_PC)

    #define CYREG_PRT15_DR                    (CYREG_GPIO_PRT15_DR)
    #define CYREG_PRT15_PS                    (CYREG_GPIO_PRT15_PS)
    #define CYREG_PRT15_PC                    (CYREG_GPIO_PRT15_PC)
#endif

0 Likes
ETRO_SSN583
Level 9
5 likes given 1000 replies posted 750 replies posted
Level 9

If you go to help, System Reference, System Reference Guide, chapter 6,

   

there is a section on pin addressing.

   

 

   

Regards, Dana.

0 Likes