Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
deonc_3697476
Level 2
Level 2
First like given

I am trying to get code that turns a LED on in Psoc Creator to work but I'm getting the following errors on the bottom image. I checked the configuration of the LED and don't think that's the cause of the issue. Any suggestions?

image (3).png

image (1).png

image (2).png

image.png

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Hi,

Since you un-checked the HW box, in the schematic there should not be a wire left.

So the schematic will look like...

001-schematic.JPG

My pin configuration is like yours, but please note I set "Initial drive state" to "High(1)"

so that the LED is off when the program starts.

000-pin-LEDG.JPG

Then I assign LEDG to pin P2[6] for CY8CKIT-044, (change the pin according to your board.)

002-Pins.JPG

Then after generating application, edit main.c something like below.

Note, I define LED_ON as 0u.

003-Source.JPG

Then when I select debug and run, my CY8CKIT-044 blinks Green LED on and off.

Attached is my test project.

Meantime, I strongly recommend you to watch the "PSoC 101 Video Tutorial Series"

they are worth for the time and save you a lot of time later.

http://www.cypress.com/training/psoc-101-video-tutorial-series-how-use-arm-cortex-m0-based-psoc-4

moto

View solution in original post

6 Replies
Owen_Zhang123
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 250 sign-ins

Please uncheck the "HW connection" box as you don't connect the pin to anywhere.

Hi I unchecked the HW box and the errors below still occur.

image.png

0 Likes
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Hi,

Since you un-checked the HW box, in the schematic there should not be a wire left.

So the schematic will look like...

001-schematic.JPG

My pin configuration is like yours, but please note I set "Initial drive state" to "High(1)"

so that the LED is off when the program starts.

000-pin-LEDG.JPG

Then I assign LEDG to pin P2[6] for CY8CKIT-044, (change the pin according to your board.)

002-Pins.JPG

Then after generating application, edit main.c something like below.

Note, I define LED_ON as 0u.

003-Source.JPG

Then when I select debug and run, my CY8CKIT-044 blinks Green LED on and off.

Attached is my test project.

Meantime, I strongly recommend you to watch the "PSoC 101 Video Tutorial Series"

they are worth for the time and save you a lot of time later.

http://www.cypress.com/training/psoc-101-video-tutorial-series-how-use-arm-cortex-m0-based-psoc-4

moto

lock attach
Attachments are accessible only for community members.

Hi Motoo,

Thanks for your help! I got the LEDs to work, but now am encountering issues getting the code in the C file attached to work in my board. My PCB is using a PSoC 4000S and I managed to compile and flash the code onto the board, but the LED is not blinking when activating the sensor at the pin designated 'VELO' .

After I tried activating the sensor a few times the PCB became unresponsive to my KitProg programmer and the PSoc software. I will solder a new board, but do you have any suggestions as to why the PSoC ADC isn't behaving as it should with the flashed code?

image (1).png

image.png

0 Likes
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Hi,

> Thanks for your help!

> I got the LEDs to work,

I'm glad hearing that!

I'd appreciate it if you mark my reply as correct answer.

> but now am encountering issues getting the code

> in the C file attached to work in my board.

Now you are asking a very different question from the original question.

Especially question(s) about CapSense is, IMHO, not a trivial one,

Then I'd strongly ask you to post a new question with an appropriate title,

so that those "CapSense Experts" can help you.

Having written that, although I'm not very familiar with CapSense,

if I were you, I would modify the main.c something like below.

My points are

(1) check if the CapSense_ADC is busy or not by using

        if (CapSense_ADC_NOT_BUSY == CapSense_ADC_IsBusy()) {

(2) move CapSense_ADC_ScanAllWidgets() inside the loop at the end of the loop,

since you have already called one just before the loop.

(3) I would separate process between STATE_ADC and STATE_CAPSENSE

==============================

int main (void)

{

    CyGlobalIntEnable; // Enable global interrupts

   //modified from the example program (CE210311 http://www.cypress.com/file/230881/download) )

   /* Start CapSense_ADC component */

   CapSense_ADC_Start();

   CapSense_ADC_ScanAllWidgets();

   scanState = STATE_ADC;

// move this to the begining of main()   CyGlobalIntEnable; // Enable global interrupts

   VELO_Write(1);

   while(1) {

        if (CapSense_ADC_NOT_BUSY == CapSense_ADC_IsBusy()) {

            if (scanState == STATE_ADC) {

               CapSense_ADC_RunTuner();

//               CapSense_ADC_ScanAllWidgets();

                mVolts = CapSense_ADC_AdcGetResult_mVolts(CapSense_ADC_AdcCHANNEL_0);

                CapSense_ADC_AdcStartConvert(CapSense_ADC_AdcCHANNEL_0);

//                CapSense_ADC_ProcessAllWidgets();

                scanState = STATE_CAPSENSE;

     

            //quick test of ADC - indicate whether the ADC detects something less than a threshold

            //when sensor at VELO pin detects < 400u mVolts the green LED at LEDG will blink

                if(mVolts < 400u){

                    LEDG_Write(1);

                    CyDelay(500);

                    LEDG_Write(0);

                }

     

            //else the green LED will not blink

     

                else{

                    LEDG_Write(0);

                }

            } else if (scanState == STATE_CAPSENSE) {

                CapSense_ADC_ProcessAllWidgets() ;

                if (CapSense_ADC_IsAnyWidgetActive()) {

                    mVolts = CapSense_ADC_AdcGetResult_mVolts(CapSense_ADC_AdcCHANNEL_0);  

                    /* do process for STATE_CAPSENSE, here */

                }

            }

            CapSense_ADC_ScanAllWidgets() ;

        }

    }

}

==============================

I'm not sure if this solve you the problem,

and you probably need to get help from those experts CapSense.

moto

0 Likes
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Hi,

In many evaluation boards, the logic of LED is negative,

which means you must write '0' to turn it on.

Anyway to give a try, how about doing?

====================

while(1) {

     LEDG_Write(1) ;

     CyDelay(500) ;

     LEDG_Write(0) ;

     CyDelay(500) ;

}

====================

moto