Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

miki_4426356
Level 1
Level 1

Hello

I don't know if this is the correct place to ask, but I will do so anyway.

I looked at the project.h header file today and saw that there were no #pragma once or #ifndef in the file. I have programmed a bit in C/C++ and thought this was a standard and a must-have.

Am I wrong about this? In the case I am - can anyone tell me why?

Many thanks

1 Solution
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
Beta tester First comment on KBA 1000 replies posted

Hi,

That is a very good question!

I have never thought of that, actually I'm lazy enough so I've never explored the Project.h.

So I opened one of my project's "Project.h", I skipped the comments.

Then there were only "#include" statements.

And each ".h" file included by this statement had #ifndef ~ #endif,

so  even if "Project.h" will be included more than twice,

it will not cause problem.

But anyway, thanks for your question, I learned 😉

Project.h

======================

#include "cyfitter_cfg.h"

#include "cydevice_trm.h"

#include "cyfitter.h"

#include "cydisabledsheets.h"

#include "UART.h"

#include "UART_SPI_UART.h"

#include "UART_PINS.h"

#include "UART_SPI_UART_PVT.h"

#include "UART_PVT.h"

#include "UART_BOOT.h"

#include "UART2.h"

#include "UART2_SPI_UART.h"

#include "UART2_PINS.h"

#include "UART2_SPI_UART_PVT.h"

#include "UART2_PVT.h"

#include "UART2_BOOT.h"

#include "uart_rx_int.h"

#include "uart2_rx_int.h"

#include "UART_SCBCLK.h"

#include "UART_tx.h"

#include "UART_tx_aliases.h"

#include "UART_rx.h"

#include "UART_rx_aliases.h"

#include "UART2_SCBCLK.h"

#include "UART2_tx.h"

#include "UART2_tx_aliases.h"

#include "UART2_rx.h"

#include "UART2_rx_aliases.h"

#include "cy_em_eeprom.h"

#include "core_cm0_psoc4.h"

#include "CyFlash.h"

#include "CyLib.h"

#include "cyPm.h"

#include "cytypes.h"

#include "cypins.h"

#include "CyDMA.h"

#include "CyLFClk.h"

======================

moto

View solution in original post

0 Likes
1 Reply
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
Beta tester First comment on KBA 1000 replies posted

Hi,

That is a very good question!

I have never thought of that, actually I'm lazy enough so I've never explored the Project.h.

So I opened one of my project's "Project.h", I skipped the comments.

Then there were only "#include" statements.

And each ".h" file included by this statement had #ifndef ~ #endif,

so  even if "Project.h" will be included more than twice,

it will not cause problem.

But anyway, thanks for your question, I learned 😉

Project.h

======================

#include "cyfitter_cfg.h"

#include "cydevice_trm.h"

#include "cyfitter.h"

#include "cydisabledsheets.h"

#include "UART.h"

#include "UART_SPI_UART.h"

#include "UART_PINS.h"

#include "UART_SPI_UART_PVT.h"

#include "UART_PVT.h"

#include "UART_BOOT.h"

#include "UART2.h"

#include "UART2_SPI_UART.h"

#include "UART2_PINS.h"

#include "UART2_SPI_UART_PVT.h"

#include "UART2_PVT.h"

#include "UART2_BOOT.h"

#include "uart_rx_int.h"

#include "uart2_rx_int.h"

#include "UART_SCBCLK.h"

#include "UART_tx.h"

#include "UART_tx_aliases.h"

#include "UART_rx.h"

#include "UART_rx_aliases.h"

#include "UART2_SCBCLK.h"

#include "UART2_tx.h"

#include "UART2_tx_aliases.h"

#include "UART2_rx.h"

#include "UART2_rx_aliases.h"

#include "cy_em_eeprom.h"

#include "core_cm0_psoc4.h"

#include "CyFlash.h"

#include "CyLib.h"

#include "cyPm.h"

#include "cytypes.h"

#include "cypins.h"

#include "CyDMA.h"

#include "CyLFClk.h"

======================

moto

0 Likes