Pin assignment window automatically closing

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
dari_292216
Level 2
Level 2
First like received First like given

On Creator 4.0 (4.0.0.432), in the Pins resource page, when I try to select a pin to assign a port the pull-down menu closes on me automatically, so I cannot select the pin.  

I checked the keyboard/mouse is Ok.

   

No other applications are showing the problem. 

Here is a short movie showing the issue -- https://vimeo.com/192566258

   

Perhaps related, upon opening the project, the status line on the bottom right shows a blinking "Ln 1 Col 1 INS" as if it being continuously updated.

   

Any clues what this is all about?

   

Thanks for any help!

0 Likes
1 Solution
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

Hello,

   

Close all the unnecessary tabs on which you are not working in PC4.0.

   

"Ln 1 Col 1 INS" blinking because  the code is stuck at a certain line no. in certain opened file in a tab.

View solution in original post

0 Likes
3 Replies
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

I suggest you to check if any key or button is stuck on Keyboard or mouse.

   

Meanwhile,you can provide us with your project to see if this is any generic issue with PC4.0

0 Likes
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

Hello,

   

Close all the unnecessary tabs on which you are not working in PC4.0.

   

"Ln 1 Col 1 INS" blinking because  the code is stuck at a certain line no. in certain opened file in a tab.

0 Likes
CaFi_1682016
Level 1
Level 1
First like received

I resolved this issue by going to the PSoC exe file properties and setting the "Compatibility" to "Windows 8".

0 Likes