Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hello everyone,

   

While reading about the PSoC Creator, I found it mentioned in the doc that PSoC Creator differs from that of the IDE's; so please tell me whats the difference between the PSoC Creator & IDE?

   

How its advantageous?

   

Will that be ok for ones like me, who are switching from PSoC1?

   

Thanks & Regards-

   

Amit

4 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

PSoc Creator is an IDE (Integrated Development Environment). A remarkable difference to other IDEs is the schematic entry by using pre-configured hardware known as "Components" which are connected (wired) as required. You are already used to making connections in PSoC Designer in the chip view, but in Creator the support is more intuitive and works similar to the well-known CAD-softwares for schematic entry.

   

A point that impressed me much in Creator is the component documentation that is always just a mouse-click away. All the APIs are explained.

   

I would suggest you to get hands on a Pioneer Kit, install Creator 3.1 and start with the example projects for the PSoC4 (there are more than 100) to get used to the IDE. Tested and debugged projects (Yes, there are debugging capabilities for the Pioneer Kit) can be programmed into the Prototype Board which is availlable for $4 only. Check the PSoC4 for the components you need for your applications. When the complexity of your proposed projects increase, you may use the more sophisticated PSoC5 with the very same IDE and a development board for the PSoC5.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thanks Bob,

   

Another thing is the Creator software available online or will it be included in the proto-type board.

   

Regards-

   

Amit

0 Likes
HeLi_263931
Level 8
Level 8
100 likes received 50 likes received 25 likes received

Creator is available online: http://www.cypress.com/psoccreator/

0 Likes
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

A basic comparison of PSOC families -

   

 

   

    

   

          

   

 

   

 

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                              

PSoC 1

PSoC 3

PSoC 4

PSoC 5

8-bit M8C core

8-bit 8051 core (single-cycle)

32-bit ARM Cortex-M0

32-bit ARM Cortex-M3

up to 24 MHz, 4 MIPS

up to 67 MHz, 33 MIPS

up to 48 MHz, 0.9 DMIPS/MHz

up to 67 MHz, 84 MIPS

Flash: 4 KB to 32 KB

Flash: 8 KB to 64 KB

Flash: 16 KB to 32 KB

Flash: 32 KB to 256 KB

SRAM: 256 bytes to 2 KB

SRAM: 3 KB to 8 KB

SRAM: 2 KB to 4 KB

SRAM: 8 KB to 64 KB

8 x 8 MAC

24 bit Digital Filter Block

32 x 32 single cycle

24 bit Digital Filter Block

Switch Cap Filters, BP, LP, HP…DTMF generation

 

 

 

I²C, SPI, UART, One Wire, LIN, FS USB 2.0, Powerline

I²C, SPI, UART, LIN, FS USB 2.0, I²S, CAN

I²C, SPI, UART

I²C, SPI, UART, LIN, FS USB 2.0, I²S

 

 

.

 

1 Delta-Sigma ADC (6 to 14-bit), 131 ksps @ 8-bit, also SAR

1 Delta-Sigma ADC (8 to 20-bit), 192 ksps @12-bit

1 SAR ADC (12-bit), 1 Msps @ 12-bit;

1 Delta-Sigma ADC (8 to 20-bit), 192 ksps @12-bit, 2 SAR ADCs (12-bit) 1 Msps @ 12-bit;

Up to four DACs (6 to 9-bit)

Up to four DACs (8-bit)

Up to two DACs (7 to 8-bit)

Up to four DACs (8-bit)

Up to 64 I/O

Up to 72 I/O

Up to 36 I/O

Up to 72 I/O

Operation: 1.7 V to 5.25 V

Operation: 0.5 V to 5.5 V

Operation: 1.71 V to 5.5 V

Operation: 2.7 V to 5.5 V

Active: 2 mA, Sleep: 3 μA, Hibernate: ?

Active: 1.2 mA, Sleep: 1 μA, Hibernate: 200 nA

Active: 1.6 mA, Sleep: 1.3 μA, Hibernate: 150 nA

Active: 2 mA, Sleep: 2 μA, Hibernate: 300 nA

Requires ICE Cube and FlexPods

 

On-chip SWD, Debug

On-chip JTAG, SWD, SWV, Debug, Trace

 

CY8CKIT-001 Development Kit

CY8CKIT-001 Development Kit

CY8CKIT-040 Pioneer Kit

CY8CKIT-001 Development Kit

CY8CKIT-030 Development Kit

CY8CKIT-042 Pioneer Kit

CY8CKIT-050 Development Kit

 

CY8CKIT-049 Prototype Kit

 

 

 

 

 

   

 

0 Likes