- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
This blog post tells you how to observe memory locations in the debugger watch window. This is useful if you want to group together and view separate memory locations that are linked by functionality such as DAC configuration, DAC routing and DAC trim.
To observe memory in the XDATA space, use the following in the watch window:
*((char*)0x01yyy)
Where YYYY is a 2 byte address. This limits the addressable range for XDATA to 64KB. The char designator restricts it to a single byte, which for most debugging purposes is sufficient.
*Note: There are no spaces in the name.
Other observable memory locations:
The address spaces are limited based on address type through the watch window (Keil limit), and everything must be addressed via the 24 bit address.
XDATA: 0x01YYYY 64k limit
DATA: 0x0000YY 128 byte limit
CODE: 0xFFYYYY 64k limit
PDATA: 0xFE00YY 256 byte limit
Other types: Char is not the only allowable type. For larger values (16 and 32 bit) you can also use int and long:
*((int*)0x01YYYY)
*((long*)0x01YYYY)
Be aware though, Keil is a big endian compiler, so it will interpret memory differently than if you read it out of the memory window. For example:
In the memory map:
0x7000 0x7001 0x7002 0x7003
FE 00 00 1F
The result of the watch window:
Watch window expressions:
You can also create interesting expressions in the watch window:
In the memory map:
0x4690 0x4691
77 02
(int)(*((char*)0x014690)+(*((char*)0x014691)<<8))
This generates the following value -> 0x0277
For PSoC 5 (GCC), there are no memory restrictions for PSoC 5 so the entire register space can be accessed in the debugger.
The same techniques apply for PSoC 5 when setting up watch variables for memory locations, although the compiler is little endian oriented, so the int and long values will look different from PSoC 3 to PSoC 5 for the same value:
In the memory map:
0x7000 0x7001 0x7002 0x7003
FE 00 00 07
The result of the watch window:
Quick Reference (PSoC 3):
XDATA: *((char*)0x01YYYY)
*Limited to 64 KB, no spaces in name
CODE: *((char*)0xFFYYYY)
*Limited to 64 KB, no spaces in name
DATA: *((char*)0x0000YY)
*Limited to 128 B, no spaces in name
Quick Reference (PSoC 5):
ALL MEMORY: *((char*)0xYYYYYYYY)
* no spaces in name