Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hi,

   

After upgrading PSoC Creator to version 3.3 it slowed down significantly. After any edit like adding an existing item, scrolling through a schematic file or source files or even writing a single line of code causes program to hang for about 2-3 seconds. I use Win7 64-bit. I also tried it with Win10, still the same problems. 

   

BR,

   

Necdet

1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Check for non-ascii characters in path or username, avoid files on network. Seems as if re-installation does not work?

   

 

   

Bob

View solution in original post

0 Likes
16 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Check for non-ascii characters in path or username, avoid files on network. Seems as if re-installation does not work?

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Hi, I'm facing the same problem.

   

the early access Creator 3.3 SP1 is better. But still the system is not responding smoothly.

   

I uninstalled all PSOC SW and reinstalled, nothing changed.

   

Metin

0 Likes
Anonymous
Not applicable

Unfortunately reinstallation doesn't work. No files on the network. I will check the path and username but there was no problem in v3.2.

0 Likes
Anonymous
Not applicable

Still no improvements. Sometimes I get the following error when it slows down and the program crashes.

   

Problem Signature:
  Problem Event Name:    APPCRASH
  Application Name:    psoc_creator.exe
  Application Version:    0.0.0.0
  Application Timestamp:    55f3682d
  Fault Module Name:    libclang.dll
  Fault Module Version:    0.0.0.0
  Fault Module Timestamp    555cb825
  Exception Code:    c0000005
  Exception Offset:    00021a27
  OS Version:    6.1.7601.2.1.0.768.3
  Locale ID:    1055
  Additional Information 1:    0a9e
  Additional Information 2:    0a9e372d3b4ad19135b953a78882e789
  Additional Information 3:    0a9e
  Additional Information 4:    0a9e372d3b4ad19135b953a78882e789

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Get help from Cypress directly: At top of this page Design Support->Create Support Case and tell what you already have tried.

   

 

   

Bob

0 Likes
mattl_01
Employee
Employee
100 replies posted 50 replies posted 25 replies posted

For those having performance issues, did you install from CD or directly download from the web?

   

--Matt

0 Likes
Anonymous
Not applicable

Hi Scott,

   

 

   

I did what you said and I cannot see 3.3 installed.

0 Likes
ScottA_91
Employee
Employee
10 solutions authored 100 replies posted 50 replies posted

Necdet,

   

Please contact me directly via email.  kin@cypress.com I'll help you get this resolved.

0 Likes
lock attach
Attachments are accessible only for community members.
ScottA_91
Employee
Employee
10 solutions authored 100 replies posted 50 replies posted

​Necdet and Metin,

   

So during the Creator install, the .Net Optimization Service (NGen) is supposed to run on all of the .Net assembles for Creator.  There is a possibility that it did not run in your cases.  If so, I can help you run the optimization tool by hand to see if that helps.

   

It turns out it is fairly easy to check for the Ngen assemblies.  Open a console Window.  (Hit the Start key and type cmd<enter> or hold shift, right click on a folder and select "Open command window here".)  Enter the following:

   

%windir%\Microsoft.Net\Framework\v4.0.30319\ngen.exe display psoc_creator

   

You should see something like this:

   

   

If you don't see your 3.3 install listed, then please let me know.  The .Net folder may be named differently, so the command may be different.

   

0 Likes

Hi,

   

I have a similar problem. PC_3.3 is very very slow. 

   

I tried this command, but similar it has failed. Can i solve this problem? Please help me

0 Likes
lock attach
Attachments are accessible only for community members.
sugac_1424126
Level 1
Level 1

I am getting the error as

   

Error: The specified assembly is not installed

   

Please find the attachment.

   

I order to achieve the speed in PSoC Creator 3.3 I have reduced the animation of my PC.

   

I have windows configuration of 
4GB RAM,
2.9GHz Intel Pentium (R) Processor
32-bit OS Win7
500GB Hard-drive where C-drive has 70GB free memory.

0 Likes
sugac_1424126
Level 1
Level 1

Hey Guys , Good news.

   

After I got fed up of slow operation, I tried to un-Install the PSoC Creator 3.3, during initialization of Uninstalling process I tried to have a another shot by giving repair...

   

 

   

WOW... ITs perfectly working smooth with out any lag.

   

 

   

@ necdetalpmen_1437776 Try to give repair. I hope your problem will be solved.

0 Likes
Anonymous
Not applicable

Hi,

   

Scott contacted me and we solved the problem. It was something about Turkish characters.

0 Likes
Anonymous
Not applicable

Hi,

   

I'm living same problems. Computer is halting for a while on every modification or action.

   

I'm getting "Error: The specified assembly is not installed" message, when I try the "ngen" command.

   

(To Scott or anyone who knows solution): Please could you share solutions(s). 

   

Especially about Turkish characters.

0 Likes
Anonymous
Not applicable

Same problem here, PSOC Creator 3.3 running so slow almost every operation, especially, when i use block diagrams. I need to know solutions, and as stated before, particularly, about Turkish characters.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

But you all read the advice to contact Scott Atkins per email?

   

 

   

Bob

0 Likes