- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi folks,
(PSoC and Creator newb here...)
I have one of thoise little PSoC 4 4200 based boards. (Not sure what the official name is.) I have built my first example project and am trying to flash it to the device. When I click the "Program" button I get a "Select Debug Targer" popup with the message "Port Acquire Failed."
Digging into Windows Device Manager I see two USB Serial devices. The first is "USB-Serial (Single Channel) Vendor MFG" and the second is simply "USB-Serial Adapter." Both are Cypress.
For "USB-Serial (Single Channel) Vendor MFG" when I drill down and look at events, the Information window shows:
Device USB\VID_04B4&PID_0002&MI_02\6&ab146f9&0&0002 was configured.
Driver Name: oem62.inf
Class Guid: {36FC9E60-C465-11CF-8056-444553540000}
Driver Date: 08/21/2014
Driver Version: 1.2.3.10
Driver Provider: Cypress
Driver Section: CyUsb3.NTamd64
Driver Rank: 0xFF0001
Matching Device Id: USB\VID_04B4&PID_0002&MI_02
Outranked Drivers:
Device Updated: false
The "USB-Serial Adapter" shows
Driver Management has concluded the process to add Service CypressSerial for Device Instance ID USB\VID_04B4&PID_0002&MI_00\6&AB146F9&0&0000 with the following status: 0.