Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer Forum Discussions

NeRe_332166
Level 1
Level 1
First reply posted Welcome! First question asked

I’m having a problem building a project that would build on another PC.

I’ve recently installed PSoC creator on a fresh Windows 10 VM (on a Mac host).

I’ve installed all Windows and PSoC Creator updates and also installed PDL 3.10. I did receive an error when trying to install C++ 2017 redestributable required by PDL 3.10 because I have a newer version installed than the one suggested by the PDL 3.10 installer, but otherwise PDL 3.10 appears to be installed (components in Creator 4.2 are listed as 3.10).

When I clean/build the project I get the error:

image002.png

Here’s the project setup showing the error:

image003.png

I’ve tried uninstalling / reinstalling PDL 3.10 and deleting the ADC component and re-inserting it from the component list in Creator, but still get the same error.

How can I fix this, please?

0 Likes
1 Reply
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

Hi,

Can you please try deleting this downloads (4.2)' folder available at this path :

C:\Users\anks\Documents\PSoC Creator\4.2

Then go to Tools>Find New Components to install the Scan_ADC component or just do update components in PSoC Creator4.2.

Thanks,

Ankita

0 Likes