- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have been having trouble with this optimizing out of variables in several projects and it seems I do not understand when this happens.
In the last case I had a variable defined within scope of a procedure (method) that retrieved info from a serial port buffer and used the value to store a record in SPI flash IC. I thought the variable would only be optimized out if I did not use it.
This is what I am doing:
uint16 level;
level = buf[3]*256 + buf[4];
StoreRecord(.....,level); //I though variable would be retained because I am using it in another function
In this case I had to set up "level" as volatile.
I thought it would only be optimized out if not used, like this...
uint8 level;
Level = buf[3]*256 + buf[4];
//then do nothing else with it
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Well, so based on your code, level is not considered volatile. You'd need something like:
volatile uint16 level;
level = buf[3]*256 + buf[4];
StoreRecord(.....,level);
for it to be marked as volatile. See http://www.keil.com/support/man/docs/c51/c51_le_volatile.htm.The reason Keil is optimizing out your variable is it looks at the assignment and the singular use case and it can either replace the usage with the assignment value, or keep the assignment in a CPU register instead of commiting it back. If you mark the variable volatile as the link above specfies, does it work as expected?
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
Keil
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Well, so based on your code, level is not considered volatile. You'd need something like:
volatile uint16 level;
level = buf[3]*256 + buf[4];
StoreRecord(.....,level);
for it to be marked as volatile. See http://www.keil.com/support/man/docs/c51/c51_le_volatile.htm.The reason Keil is optimizing out your variable is it looks at the assignment and the singular use case and it can either replace the usage with the assignment value, or keep the assignment in a CPU register instead of commiting it back. If you mark the variable volatile as the link above specfies, does it work as expected?