Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

MaBo_3731426
Level 1
Level 1

Hello, I'm following video-lesson 5. After placing the flip-flop and the logical "1" and building the project, I get the following error: "Pin guidance unavailable: Resource limit: Maximum number of Macrocells exceeded (max=0, needed=1).". Can someone help me out?

1 Solution

Je geselecteerde PSoC CY8C4125AXI-483 heeft geen UDB's (zie "Project -> Device Selector") waar de benodigde macrocellen vandaan komen. De schakelaar wordt niet aangeboden in mijn componentenlijst, dus het kan het apparaat hebben veranderd na het bewerken van het topontwerp. Heb je een ontwikkelingskit? Welke ?? CY8CKIT-0xx ???



Bob

View solution in original post

0 Likes
6 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Can you please post your complete project or a shortened version that shows the error so that we all can have a look at all of your settings. To do so, use

Creator->File->Create Workspace Bundle (minimal)

and attach the resulting file.

Bob

0 Likes
lock attach
Attachments are accessible only for community members.

Thanks for replying. Here's the zip-file.

0 Likes

Your selected PSoC CY8C4125AXI-483 has got no UDBs (see in "Project -> Device Selector") where the needed macrocells come from. The toggle ff is not offered in my component list, so it might be that you changed the device after editing the topdesign. Have you got a Development kit? Which one?? CY8CKIT-0xx ???

Bob

0 Likes

I have the psoc 4

Van: bob.marlowe

Verzonden: donderdag 27 september 2018 13:56

Aan: Mark Bolman

Onderwerp: Re: - Maximum number of Macrocells exceeded (max=0, needed=1)."

<http://www.cypress.com> Cypress Semiconductor logo

<https://community.cypress.com/?et=watches.email.thread> Cypress Developer Community

Maximum number of Macrocells exceeded (max=0, needed=1)."

reply from bob.marlowe <https://community.cypress.com/people/bob.marlowe?et=watches.email.thread> in PSoC Software - View the full discussion <https://community.cypress.com/message/170409?et=watches.email.thread#170409>

0 Likes

Je geselecteerde PSoC CY8C4125AXI-483 heeft geen UDB's (zie "Project -> Device Selector") waar de benodigde macrocellen vandaan komen. De schakelaar wordt niet aangeboden in mijn componentenlijst, dus het kan het apparaat hebben veranderd na het bewerken van het topontwerp. Heb je een ontwikkelingskit? Welke ?? CY8CKIT-0xx ???



Bob

0 Likes

You helped me on my way and I found the solution; I had to select the proper device (in my case: CY8C4245AXI-483). Everything works now. Thanks a lot! (P.S. is your last message automatically translated to Dutch?)

0 Likes