Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hello, in designer there is a resource meter/indicator that will show all the used blocks digital / analog etc...but I have noticed in creator that I can add as many components as wanted (even way beyond the capacity of the PSOC) and it does not complain.  Is there a way to tell exactly how much resources you have left/available like you did in designer?
Thanks

1 Solution
Anonymous
Not applicable
0 Likes
9 Replies
Anonymous
Not applicable
0 Likes
Anonymous
Not applicable

Resource meter does not seem to work.  I drop digital blocks in and it does not show up on the resource meter..even after a build.  What is the trick here?  Also, there is no error received when you exceed a block resource.  example...digital blocks available are 1 and I drop in 2 and there is no issue.  why?

0 Likes
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted
        If not used components are being "optimized out" during build process. Only actually used remain and being counted for macrocell, P-term and UDB blocs used, actual usage is given in report file (see *.rpt file in the bottom tab on the left pane), and now in Creator 3.3   
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Resource meter shows usage after a build. Reason are the optimization process odidday1 spoke of. Just dropping a component onto the schematic does not alter the resource meters.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

In Designer the Device Resource Meter reflects when you Drop a block in the sheet and instantly records the block used in real time.  This is far superior compared to what is offered in Creator.  In fact I am finding that Creator is not as robust as Designer.  Another question I will ask is ...Is Designer going to be expanded to include other PSOCs.. like 3, 4, 5?  If it will only support PSOC 1 then will PSOC 1 also include BLE, 8051, MO etc?  thank you

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

"Is Designer going to be expanded to include other PSOCs.. like 3, 4, 5?  If it will only support PSOC 1 then will PSOC 1 also include BLE, 8051, MO etc? "

   

Answer to that question is plainly: "No"

   

PSoC 1 family is very restricted compared to the other family members, so there it is quite easy to calculate the amount of needed resources for a component. Remember that you do not have something like gates or flip-flops or internal routable signals in a PSoC1.

   

You have inherent debug capabilities in the ARM cores which saves you an ICE-Cube, so imho a PSoC4 or 5 will always be my choice.

   

 

   

Bob

   

 

   

"

0 Likes
Anonymous
Not applicable

Thanks Bob for the reply.  I will just focus on PSOC 3, 4, 5 projects going forward.  Much appreciated.

   

Steve

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Steve,

   

if it is not for the pricing at high volume rates, I would not use the PSoC3 but the PSoC5 instead.

   

The reason is: the CPU core which is an 8051 for the PSoC3, a design made in the '80. Compare that with an ARM M3 for speed, ease of use and performance as in the PSoC5.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Got it!!  Thanks again 🙂

0 Likes