hi everyone,
Actually I posted this problem month ago. but still not resolved.
I'm using psoc creator 4.2.0.641 for cy8ckit-044. I'm getting this error when I build and clean for all project :
1. pft.M0000: An internal error occurred in the fitter: (System.UnauthorizedAccessException: Access to the path 'MPU9250.cydsn\codegentemp\bitstream.txt' is denied.).
2. bse.M0105: Unable to open the file for writing. Access to the path 'MPU9250.cydsn\codegentemp\warp_dependencies.txt' is denied.
3. fit.M050:The fitter aborted due to errors, please address all errors and rebuild.
I've tried to de-install the re-install Creator 4.2 but it still doesn't work, and then I install Creator 4.3 and I still have same error.
I even tried to make a new project in Creator 4.2 and 4.3 for basic program (UART lesson 12). But, still getting error when I tried to Generate application.
I'm really desperate.
Pls help me to sort out the error.
Thanks,
Dwi
Solved! Go to Solution.
Hi dwwa_3829216,
Can you please try creating your workspace in a different folder and let me know if you are still facing the same issue? Is building an empty project also throwing the same error?
Actually I posted this problem month ago. but still not resolved.
Can you point us to the thread/discussion so that we can understand more about the issue and not repeat the steps to try and fix the issue?
Thanks and Regards,
Rakshith M B
Hi dwwa_3829216,
Can you please try creating your workspace in a different folder and let me know if you are still facing the same issue? Is building an empty project also throwing the same error?
Actually I posted this problem month ago. but still not resolved.
Can you point us to the thread/discussion so that we can understand more about the issue and not repeat the steps to try and fix the issue?
Thanks and Regards,
Rakshith M B
Thanks for the response RakshithM_16
I've created empty project in different folder.
1. In default folder : Disk(C)>Document> Psoc Creator the result is still error (both creator 4.2 and 4.3).
2. Disk(D) > Psoc Creator the result is successful.*
I also copy my project to same folder as point 2, and it's successful.
*All my project is in Disk(D) but in different folder.
But, another problem that I worry about is sometimes my project never have this error for several days/times and then for another several days/times I got this error again.
this is the thread I mentioned
Best Regards,
Dwi W
Hi dwwa_3829216,
Thank you for providing an update and glad that you are able to build a PSoC Creator project successfully.
But, another problem that I worry about is sometimes my project never have this error for several days/times and then for another several days/times I got this error again.
Can you please let me know if the location is synced online (for example on OneDrive etc)? Is it a shared location? As this is C drive, I do not think it is external to the device. The reason I am asking is that we have come across similar issues when the PSoC Creator projects are stored in shared or external drives.
Thanks and Regards,
Rakshith M B