Hi,
Since having installed the new PSoC 3.1 (SP1) I'm having stability problems with PSoC Creator. The builds (if working) are taking ages and now and then a Visual C++ 'assertion failed' window pops up (see attachment).
Does anyone else recognize this behavior? PSoC 3.0 worked like a charm.
I have a PSoC 4 (CY8C4xxx family). I've updated the KitProg firmware to version 2.11 using the PSoC programmer. Can I go back to using PSoC Creator 3.0 or is this not possible with the new KitProg firmware? (I do have a backup of my project from PSoC Creator 3.0).
I run Windows 7 and still have PSoC 3.0 installed. Any advice would be much appreciated, I have to finish my thesis using PSoC Creator! Thanks..
Caspar
I have not seen such sluggishness or assertion error messages so far. You might create a support case (top right menu, 'MyCases'), maybe Cypress can help you better.
I also don't know whether the new KitProg firmware is compatible with Creator 3.0. It might be worth a try, since Creator 3.1 and 3.0 can co-exist. If it doesn't work, it should be possible to install the older firmware again.
The assertion you posted has to do wth the on-line code checker named "Clang" which flags errors and helps code completion while you are typing. There is a known bug (NO JOKE!) that removes assertions when you add some empty lines to the end of your source.
Bob
Bob is right. From the source code:
http://clang.llvm.org/doxygen/SourceManager_8cpp_source.html
00579 assert(NextLocalOffset + FileSize + 1 > NextLocalOffset &&
00580 NextLocalOffset + FileSize + 1 <= CurrentLoadedOffset &&
00581 "Ran out of source locations!");
00582 // We do a +1 here because we want a SourceLocation that means "the end of the
00583 // file", e.g. for the "no newline at the end of the file" diagnostic.
00584 NextLocalOffset += FileSize + 1;
so, add a couple of lines at the end of your c file.
Thanks! I have succeeded in reverting to PSoC Creator 3.0 (even with the updated KitProg), but I'll also try to make use of the hidden 'feature' in 3.1 and get rid of the assertions.
Thanks Bob... I had the same problem and it is solved now
It is really a strange solution, but it worked 🙂
There is an explanation for that bug.
Creator uses an on-line code checker named "Clang" (a name that could have been invented by Terry Pratchet ) which also provides information on variables, functions and all that which pops up for code completion) There was a bug in interfacing Clang when reading a comment just before end-of-file. This will probably be repaired with Creator 3.2.
Bob
Actually, Cypress support told me to remove the following strings from all files (including ALL auto-generated files):
/* [] END OF FILE */
I confirmed that the only way I could seem to avoid the Clang crash is to follow the Cypress support's recommendation.
Even after replacing all instances of * [] END OF FILE */ from the workspace (find and replace feature), I still get the clang crash. Please see attached picture.
Even after replacing all instances of * [] END OF FILE */ from the workspace (find and replace feature), I still get the clang crash. Please see attached picture.
I am still running into this in 3.2, and was advised of the workaround discussed here. I think it's amazing that this bug was not discovered before the product release, since eveb the auto-generated codes trip this problem
PSoC Creator 3.2 SP1 (3.2.0.6175)
Culture: English (United States)
OS Version: Microsoft Windows NT 6.1.7601 Service Pack 1
CLR Version: 2.0.50727.5485
I work with Parallels Desktop V11 on iMac. I have the same problem in a virtual XP or Win 10.
The same project works well on a virtual XP in VMWare Fusion V8.0 without problems.
Any idea ?
Hey folks,
I apologize for all the problems people have had with this. It is "Fixed" in PSoC Creator 3.3. I put Fixed in quotes because what we have done is to workaround the CLANG defect. You can download 3.3 now from cypress.com/creator. As usual, you don't have to uninstall 3.2 if you are in the middle of something. It can co-exist with 3.2 or 3.1 or 2.X.
There are a bunch of cool new features in 3.3 including a "New Project" wizard that allows you to start from a code example or target a specific kit you have installed. There is also guided pin selection for PSoC 4, an enhanced code example browser, and a resource meter (yay). You can read more at the bottom of cypress.com/creator (the What's New tab). I also attached a copy of the Release Notes.
--Matt
Hi Matt,
>> It is "Fixed" in PSoC Creator 3.3. I put Fixed in quotes because what we have done is to workaround the CLANG defect.
Not really ;-(
The problem exists only with Parallels Desktop. (in my case)
--Reiner
Hey Reiner,
Well, this is bad. By any chance is your project on a network/shared drive? There is another issue which we have not been able to work around. It's a CLANG issue that is apparently a very big deal to fix.
If anyone is using 3.3 and having this problem ("Assertion failed!" in the editor), feel free to email me and the team at psoc_creator_feedback@cypress.com. For other technical support issues, please continue to use cypress.com/support.
--Matt
Hi Matt,
yes, my project is on a network drive. I think, i use VM-Ware at the Moment. Is not a big problem.
Thank you for your efforts.
--Reiner
@Reiner
There have been programming issues reported when using vmware, so take care of that. I use Creator 3.3 on a win7 machine and never had any issues so far. A vista machine sometimes shows some idiosyncrasies but I don't think Creator is to blame.
Bob
PS: Reiner, where are you located in Germany? I live near Bremen.
Hi Bob,
i only have Macs, so i can program PSoC in Win-emulations (Parallels - with occasionally clang-problems. vmware - works fine but not so fast as Parallels). The host-system is XP.
I can live well with this configurations.
Reiner
PS: I live near Wolfsburg. Bremen I know well.
I hope we meet some time in our German forum http://www.psoc-community.de
Hi Reiner -
I was having the same problem with Parallels. Your hint lead me to store the projects in the C:/ drive instead of a location that was shared with the host OS. So far, that has resolved all of the problems I was having with things crashing.
Perhaps you might find similar results.
Michael
Hi Michael,
Thx for this hint. I will test it. But I'm not happy about store my projects in virtual environment;-(
I have test to convert a complete VM Win 10 installation inkl. Creator etc. in a Parallels File. First tests shows no problems (except missing win10 activation in parallels). But it is too early for a final statement.
Reiner
@Michael
I think, i have found the problem with Parallel. It seems, that it is a problem with Parallels Shared Folders. When i map my PSoC WorkDir with ParallelSharedFolder eg \\Mac\myPsocWorkDir i have the clang-problem. But amazing, when i map the same dir directly eg \\IP_fromMyMac\myPsocWorkDir, it works without problems;-) (for several hours)
Maybe it works on your Mac
Reiner