Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
DaEr_349131
Level 5
Level 5
25 likes received 50 sign-ins 5 comments on KBA

Hi,

   

I have trouble finding how to either manually import-export some text-file format and/or programmatically set/get the pin config in a PSoC Creator project.

   

Two use-cases:

   

 - To support several board-designs running the same software, easily be able to maintaing several pin-configuration mappings (kind of like a device-tree on linux)

   

 - When doing PCB Sch&Layout, during pin-swapping, I want to be able to push the netlist back & forth to PSoC Creator to check that it's a viable pin-swap. This is very tedious to do manually by entering the pins in the window shown below.

   

 

   

 

   

Thanks David

0 Likes
1 Solution
JobinT_31
Employee
Employee
50 solutions authored 25 solutions authored 10 solutions authored

Hello David,

   

Currently there is no method to change the pin configuration other than from CYDWR. For every pin change the analog/digit routing algorithm has to be rerun.

   

So one thing you can do is to have multiple project build for different pin configuration.

   

Thanks

   

JOBIN GT

View solution in original post

0 Likes
1 Reply
JobinT_31
Employee
Employee
50 solutions authored 25 solutions authored 10 solutions authored

Hello David,

   

Currently there is no method to change the pin configuration other than from CYDWR. For every pin change the analog/digit routing algorithm has to be rerun.

   

So one thing you can do is to have multiple project build for different pin configuration.

   

Thanks

   

JOBIN GT

0 Likes