Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
EvPa_264126
Level 7
Level 7
500 replies posted 250 replies posted 100 likes received

I tried to reduce the amount of memory by replacing the variables "unsigned int" to "char" (32 -> 😎
But memory consumption has increased only. I would like to know the reason.

0 Likes
5 Replies
kemic_264446
Level 4
Level 4
First like received

I'd start by looking at the generated assembly listing and comparing them, to get an understanding of why the (char) program needs more flash than the (unsigned int) version.

   

My guess would be down to byte alignment and pointer sizes or CPU Instructions. It might take the core CPU more instructions to move 8-Bit signed chars about, than it does unsigned ints. Thus resulting in a larger program.

0 Likes

In fact, is is indeeed that the core CPU requires more instructions to move signed chars then unsigned ints.

   

Here is the compiler output of both versions of test(...) for you to compare:

   

15:.\main.c      **** unsigned int test(unsigned int dat)
  16:.\main.c      **** {return dat+1;}
  27                      .loc 1 16 0
  28                      .cfi_startproc
  29 0000 80B5             push    {r7, lr}
  30                      .cfi_def_cfa_offset 8
  31                      .cfi_offset 7, -8
  32                      .cfi_offset 14, -4
  33 0002 82B0             sub    sp, sp, #8
  34                      .cfi_def_cfa_offset 16
  35 0004 00AF             add    r7, sp, #0
  36                      .cfi_def_cfa_register 7
  37 0006 7860             str    r0, [r7, #4]
  38                      .loc 1 16 0
  39 0008 7B68             ldr    r3, [r7, #4]
  40 000a 0133             add    r3, r3, #1
  41 000c 181C             mov    r0, r3
  42 000e BD46             mov    sp, r7
  43 0010 02B0             add    sp, sp, #8
  44                      @ sp needed
  45 0012 80BD             pop    {r7, pc}
  46                      .cfi_endproc

   


  15:.\main.c      **** char test(char dat)
  16:.\main.c      **** {return dat+1;}
  27                      .loc 1 16 0
  28                      .cfi_startproc
  29 0000 80B5             push    {r7, lr}
  30                      .cfi_def_cfa_offset 8
  31                      .cfi_offset 7, -8
  32                      .cfi_offset 14, -4
  33 0002 82B0             sub    sp, sp, #8
  34                      .cfi_def_cfa_offset 16
  35 0004 00AF             add    r7, sp, #0
  36                      .cfi_def_cfa_register 7
  37 0006 021C             mov    r2, r0
  38 0008 FB1D             add    r3, r7, #7
  39 000a 1A70             strb    r2, [r3]
  40                      .loc 1 16 0
  41 000c FB1D             add    r3, r7, #7
  42 000e 1B78             ldrb    r3, [r3]
  43 0010 0133             add    r3, r3, #1
  44 0012 DBB2             uxtb    r3, r3
  45 0014 181C             mov    r0, r3
  46 0016 BD46             mov    sp, r7
  47 0018 02B0             add    sp, sp, #8
  48                      @ sp needed
  49 001a 80BD             pop    {r7, pc}
  50                      .cfi_endproc

0 Likes
kemic_264446
Level 4
Level 4
First like received

All this means is that the CPU is optimized to work with 16-Bit ints, rather than 8-Bit chars.

   

In my tests it made no difference if the char was signed or unsigned.

0 Likes

Thank you very much for the detailed explanation!

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

I assume you have seen this -

   

 

   

http://www.cypress.com/?rid=91945     AN89610 - PSoC® 4 and PSoC 5LP ARM Cortex Code Optimization

   

 

   

Regards, Dana.

0 Likes