I am Using the Controller CY8C29466-24SXI . In that Just Configuring the Port Pin to Turn ON And OFF the LED . But Controller Not responding its Points to Always HIGH State .
Source Code :
void main(void)
{
M8C_EnableGInt;
PRT2DR = 0;
VLT_CR = VLT_CR_4V5_POR;
while(1)
{
PRT1DR = 0x00;
PRT0DR = 0;
PRT2DR = 0;
}
}
Note : PORT Pins were Configured as Respective Global Out
Kindly Help me if I Miss anything on the Global resource Configurations Parameters
Solved! Go to Solution.
Hello @Praba ,
You will have to configure the port pins individually as output, in the Pinout section. Output can be one of "Open Drain Low", "Pull Up" or "Strong".
Best regards,
Sampath Selvaraj
Hello @Praba ,
You will have to configure the port pins individually as output, in the Pinout section. Output can be one of "Open Drain Low", "Pull Up" or "Strong".
Best regards,
Sampath Selvaraj
Hi Sampath
Thanks for the Comments . Yes Changed the Drive Mode and Working Fine With that . Before Using the Global Resource Out Pin For Configuration of Port Pins .
Can You Guide me how to enable Debugging Option by Using the Mini Programmer / Debugger in the code attached Code for your Reference
Prabakaran
Hi @Praba ,
MiniProg and MiniProg3 cannot be used to debug PSoC1 devices. MiniProg3 supports debugging of PSoC3/4/5 devices.
Having said that, PSoC1 is a very mature product family, and there is little support for the same. Request you to kindly consider PSoC4 for new designs.
Best regards,
Sampath Selvaraj
Hi Sampath
Thanks for the Reply . I am using the PSOC5 . The thing PSOC1 for my old Project Support . So Requested if its Possible for PSOC1 .
Kindly Provide me the Solution - How to Enable Debugging Option in PSOC Creator 4.2 .
Thanks
Prabakaran
Hello @Praba ,
Kindly refer to "Chapter 7 Programming and Debugging" in PSoC Creator User Guide.