- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
"Filter_ADC_VDAC Example Project"
When it is built shows error on line 40 in main(), but project reports as building
successfully ?
OHx51.exe Filter_ADC_VDAC01.omf HEXFILE(Filter_ADC_VDAC01.ihx)
c8051-elf-omf2elf.exe Filter_ADC_VDAC01.omf Filter_ADC_VDAC01.elf
cyhextool -o .\DP8051\DP8051_Keil_951\Debug\Filter_ADC_VDAC01.hex -f .\DP8051\DP8051_Keil_951\Debug\Filter_ADC_VDAC01.ihx -prot .\Generated_Source\PSoC3\protect.hex -id 1E028069 -a EEPROM=90200000:800,PROGRAM=00000000:10000,CONFIG=80000000:2000,PROTECT=90400000:40 -meta 0301 -cunv 00004004 -wonv BC90ACAF -ecc .\Generated_Source\PSoC3\config.hex
Flash used: 10195 of 65536 bytes (15.6 %).
SRAM used: 137 of 8192 bytes (1.7 %).
--------------- Build Succeeded: 01/06/2014 06:35:30 ---------------
Regards, Dana.