Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

I am transferring a PSoC5 project from creatoe 2 to 5LP using creator 3

   

While was trying different hardware arrangment and build the project, I had this error shown up.

   

"The background elaborator has encountered a problem. Out of memory."

   

However, the project just contnue to build without problem. and that error would stayed there until I close and re-open the work space.

   

Anyone had this error?

0 Likes
1 Solution
Anonymous
Not applicable
        That's it "Out of memory"   
The BACKGROUND elaborator or Auto-Complete checking in software   
will have issue some errors.   
But basically harmless, as long as final build will succeed   
You won't care, unless increase the memory.   

View solution in original post

0 Likes
7 Replies
Anonymous
Not applicable

I also noticed that the creator seems to be slower than creator 2 while using more memory.

   

I check once that there were 0 free memory for a couple of times at the beginning while I clean and  building a project

0 Likes
Anonymous
Not applicable
        That's it "Out of memory"   
The BACKGROUND elaborator or Auto-Complete checking in software   
will have issue some errors.   
But basically harmless, as long as final build will succeed   
You won't care, unless increase the memory.   
0 Likes
Anonymous
Not applicable

I amusing 32 bit windows 7 pro with 4G ram already. No more Ram can be added unless change to 64bit windows or modified the kernel.

0 Likes
Anonymous
Not applicable
        I am Vista 32bit and 2.5GB RAM   
have no such a trouble   
How much about Virtual Memory Area?   
I am 3GB max area.   
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I am running Vista and win7 in 64 bit mode on my machines, all with 4GB main memory, virtual memory set to constant 8GB and *NO* memory shortage issues.

   

I would suggest you to have just a try on a different machine.

   

 

   

Bob

Anonymous
Not applicable

 the machine was setup by the IT department, we are not allowed to change or modified anything. Shall check the VM setting tomorrow.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Well, when you have got an IT-Department go to the boys and insist in some analyzation. When they are professionals, they can help you and will fix that bug, I know what I'm talking about, once I ran auch an institution myself.

   

 

   

Bob

0 Likes