- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm working on a PSoC 4 project where I need to use the ADC for one signal. However, I get the following error during the analog placement step of the build: "Net 'Net_575' is connected to an analog mux but is not connected to another component." I have noticed that Net_575 does not exist in my schematic. I also get warnings about the analog terminals on the ADC being unconnected. The build is successful if I connect analog pins to every channel.
I have disabled all the other channels except for the one I want to use. Is there another setting that needs to change in order to only use one ADC channel? I'm using PSoC Creator 3.3 CP3 (3.3.0.9604) and the ADC_SAR_SEQ_P4 component's version is 1.10.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Just set the number of channels for the ADC (on the channels tab) to 1 (one) and reconnect the input pin.
Bob