Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer Forum Discussions

TiMi_264191
Level 3
Level 3
10 sign-ins 25 replies posted 10 replies posted

In Creator 2.1, what is a good way to have a whole project (workspace?) saved to a particular folder?

   

Can I save a copy later in a different folder/location? How?

   

If I create a component, is it available in CREATOR for me to use in a future/different project?

   

If I do not have DEV KIT CD's, how can I (or can I?) load example projects so CREATOR shows them under Examples and Kits on the Start Page?

   

Sometimes I seem to have two projects open at the same time... and if I want to copy some code from main.c(X) to main.c(Y) that is ok... Can I close the workspace on each and all is right with the world? I ask because sometimes I can not find one of the files (easily). By the way, sometimes I get two copies of CREATOR open at the same time in these scenerios.

   

In getting example projects, CREATOR confuses me sometimes when I go to reopen one (that I assumed had been saved) and asks me if I want to write over it....

   

So, what is a good way to keep it all organized? Originals (from you or me), Modified versions, Components (for use in other projects) and Experimental versions (ie saving under a different name).

   

Thanks

   

Tim Miner

Tim Miner
0 Likes
4 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Best is to use

   

File -> Create Workspace Bundle

   

Even a choice of minimal files includes all of your own sources. You may copy the contents of the archive to a new location and adjust the project- and workspace-names to the new needs and (when required) select a new device.

   

 

   

Happy coding

   

Bob

0 Likes
Anonymous
Not applicable

 That did not entirely answer the question. Unless that is the only way to save a work space?

   

The saving process is confusing. Creator often has greyed out menu items.

   

Could someone show the actual steps of opening an example and saving it under a different name?

0 Likes
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Start by opening an project

   

 

   

"File"

   

"New"

   

Pick Project, click "advannced" at bottom

   

Choose "Create New Workspace"

   

 

   

 

   

 

   

0 Likes
Anonymous
Not applicable
        Hello everyone   
PSoC Designer has the cloning process but Creator has not,   
I've been do it like this ...   
1) Copy and Paste workspace root directory by Windows   
2) Change root directory name to new name   
3) Open workspace in new directory   
4) Click Project name in workspace tab and change it (F2 or "Rename")   
5) Same changing on Workspace-name   
That's all, New named project had been created   
You can keep original project and create new your experimental project.   
0 Likes