Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer Forum Discussions

Anonymous
Not applicable

Just installed a fresh copy of Windows 10 on an unused computer. During the installation Adobe SVG won't install. Inside designer  I can't create a new project. If you try to load an existing project, it will just never complete and you get loading in the status bar forever. 

   

So for now windows 10 do not support PSOC designer 5.4 SP1 CP1

   

Is there any plan to support Windows 10  in a near futur?

   

Eric

0 Likes
1 Reply
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Release notes show following compatibility -

   

Windows® XP (SP2 or higher), Vista, Windows 7,
Windows 8, Windows 8.1

   

 

   

File a CASE and ask for the status -

   

 

   

To create a technical or issue case at Cypress -

   

 

   

www.cypress.com

   

“Design Support”

   

“Create a Support Case”

   

 

   

You have to be registered on Cypress web site first.

   

 

   

Regards, Dana.

0 Likes