Designer Install Change

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Would it be possible to change the flow of Designer install so that

   

one click brings user to all necessary input checkoffs, like license,

   

then next click proceeds to install ?

   

 

   

Save users waiting  for multiple steps to occur.

   

 

   

Regards, Dana.

0 Likes
4 Replies
Anonymous
Not applicable

You mean one ingle click and everything is checked annd ready to install?

   

The EULA has to have its own step otherwise some people might complain yo are making them accept a licence.

0 Likes
Anonymous
Not applicable

 I do not have problem with this both the installation of both the designer and the creator takes time, hope it can be done quicker.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

@zeta, one screen is brought up, Eula in a window box, and all

   

checks applied, then off to the races, no more intervention.

   

 

   

Now it unpacks, eula's, then unpacks some more, then asks OK or

   

whatever. This over 5 minutes or more before user can leave system.

   

 

   

One screen.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable
        I just have my computer crashed and install both creator and designer to old machine to continue developemnt, Takes a while with a slow machine. And have to do it when my new faulty machine being fixed - was told would have to rei-install windows and the harddisk would be reformated as wllll. :-(.   
0 Likes