Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

I've looked in the PSoC Creator docs, on forums and other searches and couldn't find information about how to create custom build configurations.

   

I'm familiar with Microsoft Visual Studio​ features to create custom build configurations beyond the standard Debug and Release.  It allows me to define unique conditional compile settings depending on what target I'm trying to build.

   

In particular for the PSoC family it would be nice if I can have individual compile/build settings for the same app if I'm loading into the CY8KIT-042 which doesn't have a bootloader as compared to the CY8KIT-049 which does.  Without loading a separate project.

   

At least for now, does anyone know how to conditionally compile the "Bootloadable" object.  I know how to enable/disable it but I'm trying to load the app it on the 042 and 049 kits correctly.

   

Len

Len
"Engineering is an Art. The Art of Compromise."
0 Likes
1 Solution
cadi_1014291
Level 6
Level 6
25 likes received 10 likes received 10 likes given

From https://community.cypress.com/thread/8394

   

 

   

quote:

   

PSoC Creator 4.1 Update

   

Hello,

   

Here's an update on what to expect with PSoC Creator 4.1, planned to be released in the coming weeks!

   

 

   

Web-Based Content Delivery

   

With this release, you can now obtain updates to devices (including modules), Components, and code examples from the Cypress web page. This will reduce the overall size of PSoC Creator in the future, providing faster installs and updates. The other key benefit of web-based content delivery is that devices, Components, and code examples can be distributed as soon as they are ready, instead of waiting for the next PSoC Creator update.

   

 

   

Pre- and Post-Build User Commands

   

The Build Settings dialog was also updated to provide a User Commands page. This feature allows you to run custom, user-specified, pre-build commands before the compile steps, as well as run custom user-specified, post-build commands after PSoC Creator’s post-build step.

   

 

   

Component Customizer Dialog Updates

   

Cypress has made several small enhancements to the default Configure dialog to improve the user experience with Components. With FM0+ devices moving from instance-based to driver based Components, it is beneficial to present the actual struct members as they are in firmware. These enhancements enable new features in the default GUI that mean more Components can take advantage of the default interface.

   

 

   

New Start Page

   

This is an update to the existing Start Page to enable better, more focused content delivery to users. The static content in the Start Page (left panel) is being refreshed and the live content area (right panel) is being used to show web-based information for “Getting Acquainted” and “New in 4.1”.

   

 

   

PSoC Creator 4.1 and PSoC 6

   

PSoC Creator 4.1 will be a minimum prerequisite and is recommended for all to install in preparation for a PSoC 6 software toolset release that is coming soon.

   

 

   

Maybe Pre- and Post-Build User Commands is what you are looking for.

View solution in original post

0 Likes
3 Replies
cadi_1014291
Level 6
Level 6
25 likes received 10 likes received 10 likes given

From https://community.cypress.com/thread/8394

   

 

   

quote:

   

PSoC Creator 4.1 Update

   

Hello,

   

Here's an update on what to expect with PSoC Creator 4.1, planned to be released in the coming weeks!

   

 

   

Web-Based Content Delivery

   

With this release, you can now obtain updates to devices (including modules), Components, and code examples from the Cypress web page. This will reduce the overall size of PSoC Creator in the future, providing faster installs and updates. The other key benefit of web-based content delivery is that devices, Components, and code examples can be distributed as soon as they are ready, instead of waiting for the next PSoC Creator update.

   

 

   

Pre- and Post-Build User Commands

   

The Build Settings dialog was also updated to provide a User Commands page. This feature allows you to run custom, user-specified, pre-build commands before the compile steps, as well as run custom user-specified, post-build commands after PSoC Creator’s post-build step.

   

 

   

Component Customizer Dialog Updates

   

Cypress has made several small enhancements to the default Configure dialog to improve the user experience with Components. With FM0+ devices moving from instance-based to driver based Components, it is beneficial to present the actual struct members as they are in firmware. These enhancements enable new features in the default GUI that mean more Components can take advantage of the default interface.

   

 

   

New Start Page

   

This is an update to the existing Start Page to enable better, more focused content delivery to users. The static content in the Start Page (left panel) is being refreshed and the live content area (right panel) is being used to show web-based information for “Getting Acquainted” and “New in 4.1”.

   

 

   

PSoC Creator 4.1 and PSoC 6

   

PSoC Creator 4.1 will be a minimum prerequisite and is recommended for all to install in preparation for a PSoC 6 software toolset release that is coming soon.

   

 

   

Maybe Pre- and Post-Build User Commands is what you are looking for.

0 Likes

Carlos,

   

I've seen the new PSoC Creator 4.1 feature set.  I don't think the Pre- and Post- build features will do the trick.

   

Visual Studio IDE also provided custom Pre- and Post- build features. 

   

The feature I'm looking for is more than the two Build configuration of "Debug" and "Release".  In Visual Studio, you can create your own build configuration and give it a new name.   For example,  I could copy the "Debug" configuration and give it a new name such as "Debug with LCD text".  I can then modify this build to have conditional compile settings to enable an LCD display component and conditional "#assert()" to dump debug info.  However, the "Debug" and "Release" builds would not have this compiled in.

   

In another example, I could have "Debug 042-kit" and a "Debug 049-kit".  Each would conditionally compile for the differences between the two kit configurations.  For example, the 042-kit does not need a Bootable component but the 049-kit needs one.

   

Len

Len
"Engineering is an Art. The Art of Compromise."
0 Likes
HuEl_264296
Level 5
Level 5
First like given 25 sign-ins First solution authored

I would be very interested in custom build configurations too.  I'm very happy to see the Pre and Post build steps, but custom configurations would also help.

   

 

   

Hugo

0 Likes