- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
After two years I am just starting again with the PSoC Creator and some things are really bothering me.
My Setup:
- i5-CPU, 16GB RAM, SSD, 64bit Linux Host.
- Win10 Enterprise 64bit in Virtual Machine with 8GB RAM and 4 CPU-cores in Virtualbox.
- PSoC Creator 4.1 (4.1.0.2686)
- CYC8KIT-042-BLE with CY8C4248LQI-BL583
The problem is not the embedded, it is the PSoC Creator!
The Code-completion does not work anymore. I tried to enable different features via Options --> Text Editor --> Inline Diagnostis and Autocomplete. But nothing that I can enable or disable there really changes anything! (Restarted PSoC Creator of course!)
And if that was not already bad enough, the function "Go to Declaration F12" and "Go to Definition Ctrl+F12" is also not working! No error, no message, nothing happens!
I also tried to install the PSoC Creator in a fresh Win7-Virtual machine, with the same results. Right after the installation the F12-function was initially working one time, but after reboot, or when I opened an old project, nothing worked any more.
I was just thinking about ordering the new PSoC-6 with the BLE 5.0 functionality, but not with this performance!
Is there anything I could do to improve the performance?
Has anybody else recognized this behaviour?
Thanks
Andreas
Solved! Go to Solution.
- Labels:
-
PSoC Creator Software
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Why do I have to update all components before I am able to build the project?
Ans:With each version of Creator , new version of certain components gets incorporated.It is not compulsory to update all the components.
Then I didn't install the KEIL-compiler, because I knew I would not use it. But I get an error on each build saying that the path to the binaries is not set!
Ans:You can avoid that by this settings-