Hello everyone

   

I've been finishing this proyect that was of other person who worked with me, but I has a problem when I build it

   

ERROR: .\CortexM0\ARM_GCC_493\Debug\Tarjeta de comunicacion PLC.elf section `.rodata' will not fit in region `rom'
ERROR: section .cyloadablemeta loaded at [00007fc0,00007fff] overlaps section .rodata loaded at [00007ad8,00008147]
ERROR: region `rom' overflowed by 0 bytes
collect2.exe: error: ld returned 1 exit status
The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.

   

 

   

If you can give  instruction for how to solve it, i will appreciate it 

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Here is with the definition error solved

View solution in original post

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

The project archive you supplied cannot be opened, sorry.

   

Use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.

   

Try to compile your project with "Release" settings instead of "Debug"

   

 

   

Bob

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Sorry for the inconvenience, I attached the Zip already
I have already read about the "Release" but the same error.

   

Thank you for you help

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Here is with the definition error solved

0 Likes