Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 FYI,

   

After installing Akamai Netsession in order to download PSoC Creator I noticed (several days later) that the Windows Vista 'NT Kernel & Systems' task was running continuously at 20% to 30% of cpu.  I didn't see an Akamai task running, but I merely uninstalled it because it was the only thing I'd installed recently. 

   

I'm just passing this along in case others are having the same problem.

   

Regards

   

Bill Hayes

0 Likes
1 Reply
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

An interesting thread with some tools to assist -

   

 

   

http://helpdeskgeek.com/windows-7/fix-nt-kernel-system-process-cpu-usage-in-windows-7/

   

 

   

Regards, Dana.

0 Likes