what is operating volatge for PSoC 6 and compare a stand by power between PSoC 6 and PSoC 3. PSoC 6 can support .XML files to make a MATLAB analysis for a camera and sound simulations.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

We are working to make a smart wearable for a intergration of smart home connectivity. Although we make a Smart homes devices using Texas Instrument CC-3200 for low cost to fulfil the needs of all community people to get through IOT by Indian innovation design challenge. On top that we also plan to make smart wearable in that we got a solution from your product that fullfil our needs but we have little confusion between PSoc 6 and PsoC 3 in which PSoC 6 has been developed fully for IOT purpose but for smart wearable battery is main concert so it can be done by PSoC 3 which has high Precision analog value and ultra low power for long standby in various sleep mode. Can accuracy and standy, Power management is same as or much more better than PSoC 3 in PSoC 6. Please justify it.

0 Likes
1 Solution
DheerajK_81
Moderator
Moderator
Moderator
First comment on KBA First comment on blog 5 questions asked

The operating voltage range for PSoC 6 is 1.7V to 3.6V. By default the PSoC 6 MCUs are designed to work at 1.1V (nominal) core voltage generated by an internal LDO regulator.

PSoC 3 and PSoC 6 are powerful MCUs purpose built for different types of application requirements. If you require a large array of analog options then PSoC 3 would be a good choice. If low power is the requirement, then PSoC 6 comes with 6 power modes, security and connectivity options, a best fit for IOT applications.

You can find the power specifications for

- PSoC 6 in Page#24 for various modes here: https://www.cypress.com/file/385921/download

- PSoC 3 in Page#32 for various modes here: https://www.cypress.com/file/127111/download

Regards,

Dheeraj

View solution in original post

0 Likes
1 Reply